<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Classic/Legacy CodeWarrior中的主题 Re: Codewarrior with S12XD use non banked memory.</title>
    <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Codewarrior-with-S12XD-use-non-banked-memory/m-p/148167#M1898</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Not sure why having .copy in 0x8000..0xBFFF would not work, I would think it should if PPAGE is setup before (or the reset value works). Well anyway.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;For the SRecord, look at the bbl file. It supports to map any addresses for the generated SRecords,&lt;/P&gt;&lt;P&gt;see the burner chapter in the build tools manual.&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 22 Oct 2009 21:00:05 GMT</pubDate>
    <dc:creator>CompilerGuru</dc:creator>
    <dc:date>2009-10-22T21:00:05Z</dc:date>
    <item>
      <title>Codewarrior with S12XD use non banked memory.</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Codewarrior-with-S12XD-use-non-banked-memory/m-p/148163#M1894</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;On our project, we have a S12X. The bootloader is in area 0xc000 to 0xffff. And our application code need 20kB the problem is that the non banked flash size&amp;nbsp;in 0x4000 is 16kB. We want to use the area 0x8000 to 0xBFFF as non banked area. Is it possible to do that. We don't want to use pragma in our code. We tried this and it doesn't work. How can we do that?&lt;/P&gt;&lt;P&gt;Can somebody&amp;nbsp;help us?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Oct 2009 22:00:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Codewarrior-with-S12XD-use-non-banked-memory/m-p/148163#M1894</guid>
      <dc:creator>gae037</dc:creator>
      <dc:date>2009-10-21T22:00:10Z</dc:date>
    </item>
    <item>
      <title>Re: Codewarrior with S12XD use non banked memory.</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Codewarrior-with-S12XD-use-non-banked-memory/m-p/148164#M1895</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;gt;We tried this and it doesn't work&lt;/P&gt;&lt;P&gt;What does not work?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Try to use 0xFE8000..0xFEBFFF and make sure PPAGE is (and stays) 0xFE.&lt;/P&gt;&lt;P&gt;When using 0xFE8000 there maybe some linker warnings about cutting 0xFE8000 to 0x8000 which you can safely ignore.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Oct 2009 08:42:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Codewarrior-with-S12XD-use-non-banked-memory/m-p/148164#M1895</guid>
      <dc:creator>CompilerGuru</dc:creator>
      <dc:date>2009-10-22T08:42:26Z</dc:date>
    </item>
    <item>
      <title>Re: Codewarrior with S12XD use non banked memory.</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Codewarrior-with-S12XD-use-non-banked-memory/m-p/148165#M1896</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ok now it works the problem was that the .copy area was not between 0x4000 and 0x7FFF so the varaible initialisation was bad.&lt;/P&gt;&lt;P&gt;I have another question concerning the S19 file generation. On our .map file the adress are in 16 bit (that means without the page index) for exemple we have 0x8000 and not 0xFE8000. But in the S19 file we have 0xFE8000 is it possible to have 16 bit adress in the S19 file (0x8000 instead of 0xFE8000)?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Oct 2009 12:54:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Codewarrior-with-S12XD-use-non-banked-memory/m-p/148165#M1896</guid>
      <dc:creator>gae037</dc:creator>
      <dc:date>2009-10-22T12:54:57Z</dc:date>
    </item>
    <item>
      <title>Re: Codewarrior with S12XD use non banked memory.</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Codewarrior-with-S12XD-use-non-banked-memory/m-p/148166#M1897</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Look in the &lt;SPAN style="font-style: italic"&gt;Build Tool Utilities Manual&lt;/SPAN&gt; (Build_Tools_Utilties.pdf), located in the Help folder of the CodeWarrior Installation. Check out the chapters on the Burner Utility.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Also, enter "SRECCVTSW" on the keyword search (it's text box at upper right on this web page) to find the archive that contains the S-record convertor program. It can change an existing S-record file into different formats, one which might meet your needs.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;---Tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Oct 2009 19:45:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Codewarrior-with-S12XD-use-non-banked-memory/m-p/148166#M1897</guid>
      <dc:creator>J2MEJediMaster</dc:creator>
      <dc:date>2009-10-22T19:45:50Z</dc:date>
    </item>
    <item>
      <title>Re: Codewarrior with S12XD use non banked memory.</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Codewarrior-with-S12XD-use-non-banked-memory/m-p/148167#M1898</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Not sure why having .copy in 0x8000..0xBFFF would not work, I would think it should if PPAGE is setup before (or the reset value works). Well anyway.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;For the SRecord, look at the bbl file. It supports to map any addresses for the generated SRecords,&lt;/P&gt;&lt;P&gt;see the burner chapter in the build tools manual.&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Oct 2009 21:00:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Codewarrior-with-S12XD-use-non-banked-memory/m-p/148167#M1898</guid>
      <dc:creator>CompilerGuru</dc:creator>
      <dc:date>2009-10-22T21:00:05Z</dc:date>
    </item>
  </channel>
</rss>