<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Classic/Legacy CodeWarrior中的主题 Re: CW10 New BSP, PSP</title>
    <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CW10-New-BSP-PSP/m-p/147750#M1883</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Problem is that you cannot open&amp;nbsp;two projects with the same name in a workspace. When you are duplicating a project tree, the project name for the IDE is the same.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am usually using following process when it goes around duplicating and renaming a project under CodeWarrior Eclipse:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; 1- Remove the source project from the workspace (Click right on the project name and select delete.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; This will remove project from workspace, but not delete the folder from the disk.).&lt;/P&gt;&lt;P&gt;&amp;nbsp; 2- Open a Windows Explorer and duplicate the whole project tree. Try to duplicate the project outside of the workspace.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; There are some Pb with some eclipse drop when you are duplicating the project inside of the workspace directory.&lt;/P&gt;&lt;P&gt;&amp;nbsp; 3-Import the duplicated project in the workspace.&lt;/P&gt;&lt;P&gt;&amp;nbsp; 4-Click right on&amp;nbsp;the project name and select Rename&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; 5-Give a meaningful name to the project&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Once this is done, you can open both the original project and the duplicated one in the same Workspace.&lt;/P&gt;&lt;P&gt;Additionally once you are over here you can also move the duplicated project back to&amp;nbsp;in the workspace directory if you prefer to work this way.&lt;/P&gt;&lt;P&gt;Just Remove the project from the workspace, move it over and import it back in&amp;nbsp;the workspace.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Final note you may experience some trouble with the launch configuration files depending on&amp;nbsp;the eclipse version you are using. In worst case you may have to re-create them manually for the duplicated project.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;CrasyCat&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 17 Sep 2010 14:23:36 GMT</pubDate>
    <dc:creator>CrasyCat</dc:creator>
    <dc:date>2010-09-17T14:23:36Z</dc:date>
    <item>
      <title>CW10 New BSP, PSP</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CW10-New-BSP-PSP/m-p/147749#M1882</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm trying to create a new BSP.&amp;nbsp; I had added the bsp_m51jmevb and psp_m51jmevb to my workspace and they have been built.&amp;nbsp; I wish to create a new configuration for my target hardware and I have copied the existing project directories for 51Jm128evb and renamed them to 51Jm128Pcc.&amp;nbsp; (mqx\build\cw10\bsp_m51jmPcc; lib\m51jmPcc.cw10 and config\m51JmPcc&amp;nbsp; Although I don't think config\m51jmPcc is used by CW10).&amp;nbsp; When I try to import the project (as I had done for the 51Jm128evl) I get an error that says "Some projects were hidden because they exist in the workspace directory" and I cannot continue.&amp;nbsp; Selecting some other BSP that is not part of my workspace allows me to continue.&lt;/P&gt;&lt;P&gt;Any thoughts?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Will&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Sep 2010 23:10:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CW10-New-BSP-PSP/m-p/147749#M1882</guid>
      <dc:creator>WHookway</dc:creator>
      <dc:date>2010-09-15T23:10:40Z</dc:date>
    </item>
    <item>
      <title>Re: CW10 New BSP, PSP</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CW10-New-BSP-PSP/m-p/147750#M1883</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Problem is that you cannot open&amp;nbsp;two projects with the same name in a workspace. When you are duplicating a project tree, the project name for the IDE is the same.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am usually using following process when it goes around duplicating and renaming a project under CodeWarrior Eclipse:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; 1- Remove the source project from the workspace (Click right on the project name and select delete.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; This will remove project from workspace, but not delete the folder from the disk.).&lt;/P&gt;&lt;P&gt;&amp;nbsp; 2- Open a Windows Explorer and duplicate the whole project tree. Try to duplicate the project outside of the workspace.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; There are some Pb with some eclipse drop when you are duplicating the project inside of the workspace directory.&lt;/P&gt;&lt;P&gt;&amp;nbsp; 3-Import the duplicated project in the workspace.&lt;/P&gt;&lt;P&gt;&amp;nbsp; 4-Click right on&amp;nbsp;the project name and select Rename&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; 5-Give a meaningful name to the project&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Once this is done, you can open both the original project and the duplicated one in the same Workspace.&lt;/P&gt;&lt;P&gt;Additionally once you are over here you can also move the duplicated project back to&amp;nbsp;in the workspace directory if you prefer to work this way.&lt;/P&gt;&lt;P&gt;Just Remove the project from the workspace, move it over and import it back in&amp;nbsp;the workspace.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Final note you may experience some trouble with the launch configuration files depending on&amp;nbsp;the eclipse version you are using. In worst case you may have to re-create them manually for the duplicated project.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;CrasyCat&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 17 Sep 2010 14:23:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CW10-New-BSP-PSP/m-p/147750#M1883</guid>
      <dc:creator>CrasyCat</dc:creator>
      <dc:date>2010-09-17T14:23:36Z</dc:date>
    </item>
    <item>
      <title>Re: CW10 New BSP, PSP</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CW10-New-BSP-PSP/m-p/147751#M1884</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;CrasyCat,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks, that worked.&amp;nbsp; I am able to build a new project.&amp;nbsp; I used windows explorer to copy the necessary directories.&amp;nbsp; When I imported the project I did not copy the files into the workspace.&amp;nbsp; I fixed the paths and filenames to use the new project directory / file names as required.&amp;nbsp; However, the links maintained in the .project file for all the source files point to the original directory structure&amp;nbsp; - specifically for the mqx/bsp/m51jmevb files.&amp;nbsp; These files were copied when I initially copied the project files.&amp;nbsp; Is there a way within CW to point the "m51jmPcc BSP Files" Folder (which I renamed from the original m51jmevb folder) to the new bsp directory?&amp;nbsp; These are the files that I would most likely need to modify for my new BSP.&amp;nbsp; Each of the files within this folder show them being linked to the original directory.&amp;nbsp; Should I just do a mass edit on the ".project" file to fix these links?&amp;nbsp; Do you recommend that I copy the files into the project on import?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Another question, as a curiosity,&amp;nbsp; where does the "group" get set / defined?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Will&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Sep 2010 20:35:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CW10-New-BSP-PSP/m-p/147751#M1884</guid>
      <dc:creator>WHookway</dc:creator>
      <dc:date>2010-09-22T20:35:29Z</dc:date>
    </item>
    <item>
      <title>Re: CW10 New BSP, PSP</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CW10-New-BSP-PSP/m-p/147752#M1885</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;You can add a linked folder to your project.&lt;/P&gt;&lt;P&gt;Proceed as follows:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; - Right click on the folder name and select &lt;STRONG&gt;File&lt;/STRONG&gt; &amp;gt; &lt;STRONG&gt;New&lt;/STRONG&gt; &amp;gt; &lt;STRONG&gt;Folder&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; - Select the parent folder on the top of the dialog.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; - In the &lt;STRONG&gt;New Folder&lt;/STRONG&gt; dialog click on &lt;STRONG&gt;Advanced &amp;gt;&amp;gt;&lt;/STRONG&gt;.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; - Check &lt;STRONG&gt;Link to folder in the file system&lt;/STRONG&gt;.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; - Browse for the location of the m51jmPcc BSP Files directory (you can use Variables if you do not want to&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; use an absolute path here).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; - Click &lt;STRONG&gt;Finish&lt;/STRONG&gt;.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Your project will just get pointer to the&amp;nbsp;file in the specified&amp;nbsp;directory.&lt;/P&gt;&lt;P&gt;Note that all files located in the specified&amp;nbsp;directory will be added to the project. That means when attempting to do a rebuild from project the content of the directory&amp;nbsp;&amp;nbsp;m51jmPcc BSP Files will be rebuild as well.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Information about groups is stored in file .cproject.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;CrasyCat&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Oct 2010 20:04:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CW10-New-BSP-PSP/m-p/147752#M1885</guid>
      <dc:creator>CrasyCat</dc:creator>
      <dc:date>2010-10-06T20:04:46Z</dc:date>
    </item>
  </channel>
</rss>