<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Classic/Legacy CodeWarrior中的主题 Re: Codewarrior 10 Can't Debug</title>
    <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Codewarrior-10-Can-t-Debug/m-p/147166#M1822</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I've got some more information that may help you help me.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I said I use an USB BDM, well actually it's a demoJM board used like a BDM... I don't put any daugther card and connect to my board using BDM pins... That worked fine for me on win XP, CW 6.1&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;When I first try to debug with this demoJM with Codewarrior v10 on Win 7, I said a screen appears with the image of a blue BDM, and it actually says updating firmware (I assume BDM's firmware)... That happen t0o fast for me and couldn't see well.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Now I have a "real" USB BDM, not the demoJM board... I just plugged it and work fine on win7 Codewarrior v10. The screen with the blue BDM appears again says updating firmware, and when it finished it said updated succesfully.... Then I went back to the demoJM an happend the same as the post above.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I've notice 2 things. There are 2 "CW v10 MCU" &amp;nbsp;fodlers, one on Program Files and the other under Program Files (x86)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;1- The one inside Program Files has a Driver folder wich contains a folder named &amp;nbsp;"osbdm-JM60". I assume those are the drivers for the demoJM board BDM. It's sourprise me that it says OSBDM... it's an OpenSource BDM? Because when I created the project I didn't choose OSBDM, I've chosen P&amp;amp;E USB MULTILINK BDM&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;2-The folder inside Porgram Files (x86) has a folder named "pemicro" wich is the same folder I've got on win XP. I assume those are the drivers for the USB BDM&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I just went to my win XP PC... I've not installed CW 10 there, the demoJM works fine as a BDM... and the fodler&amp;nbsp;"osbdm-JM60" does not exits...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any clue? Now I'll try installing CW 10 on win XP and see if the demoJM works&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;As always thanks!!!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Sep 2010 02:36:57 GMT</pubDate>
    <dc:creator>sebasira</dc:creator>
    <dc:date>2010-09-16T02:36:57Z</dc:date>
    <item>
      <title>Codewarrior 10 Can't Debug</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Codewarrior-10-Can-t-Debug/m-p/147165#M1821</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Well, hello everyone!!!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I manage to get a project to build with this new version of codewarrior. I'm using v10 on a win7 64-bits. I've installed the driver version 10 from P&amp;amp;E. and I'm using a USB BDM connected to a QE32. This worked fine on a winXP PC with Codewarrior v6.1&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;When I click on "debug" the following screen appears:&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;'Launching My_Project_MCF51QE32_Internal_Flash_PnE USB BDM' has encountered a problem.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;ColdFire GDI Protocol Adapter: Can't connect. The Debugger can not connect to the PnE BDC interface or targetted hardware board&lt;/STRONG&gt;.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This also appears on the CONSOLE:&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Info: USB-ML-12 detected - Flash Version 5.83&lt;BR /&gt;Info: USB-ML-12 detected - Flash Version 5.83&lt;BR /&gt;Error: Connect failed.&lt;BR /&gt;Error : The Debugger can not connect to the P&amp;amp;E BDC interface or targetted hardware board.&lt;/STRONG&gt;&lt;BR /&gt;&lt;BR /&gt;&amp;nbsp;I guess it maybe a driver problem. How can I fix it?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;One more thing... when I first ran the debugger an unusual screen appears with a picture of a blue BDM and said something like "updating firmware or software". I've never seen it before and haven't seen it again.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please help... I can`t go further from here if I cannot debug or even download firmware to my hardware&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks Everyone!!!!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Sep 2010 11:07:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Codewarrior-10-Can-t-Debug/m-p/147165#M1821</guid>
      <dc:creator>sebasira</dc:creator>
      <dc:date>2010-09-14T11:07:56Z</dc:date>
    </item>
    <item>
      <title>Re: Codewarrior 10 Can't Debug</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Codewarrior-10-Can-t-Debug/m-p/147166#M1822</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I've got some more information that may help you help me.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I said I use an USB BDM, well actually it's a demoJM board used like a BDM... I don't put any daugther card and connect to my board using BDM pins... That worked fine for me on win XP, CW 6.1&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;When I first try to debug with this demoJM with Codewarrior v10 on Win 7, I said a screen appears with the image of a blue BDM, and it actually says updating firmware (I assume BDM's firmware)... That happen t0o fast for me and couldn't see well.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Now I have a "real" USB BDM, not the demoJM board... I just plugged it and work fine on win7 Codewarrior v10. The screen with the blue BDM appears again says updating firmware, and when it finished it said updated succesfully.... Then I went back to the demoJM an happend the same as the post above.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I've notice 2 things. There are 2 "CW v10 MCU" &amp;nbsp;fodlers, one on Program Files and the other under Program Files (x86)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;1- The one inside Program Files has a Driver folder wich contains a folder named &amp;nbsp;"osbdm-JM60". I assume those are the drivers for the demoJM board BDM. It's sourprise me that it says OSBDM... it's an OpenSource BDM? Because when I created the project I didn't choose OSBDM, I've chosen P&amp;amp;E USB MULTILINK BDM&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;2-The folder inside Porgram Files (x86) has a folder named "pemicro" wich is the same folder I've got on win XP. I assume those are the drivers for the USB BDM&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I just went to my win XP PC... I've not installed CW 10 there, the demoJM works fine as a BDM... and the fodler&amp;nbsp;"osbdm-JM60" does not exits...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any clue? Now I'll try installing CW 10 on win XP and see if the demoJM works&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;As always thanks!!!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Sep 2010 02:36:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Codewarrior-10-Can-t-Debug/m-p/147166#M1822</guid>
      <dc:creator>sebasira</dc:creator>
      <dc:date>2010-09-16T02:36:57Z</dc:date>
    </item>
    <item>
      <title>Re: Codewarrior 10 Can't Debug</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Codewarrior-10-Can-t-Debug/m-p/147167#M1823</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Sebastian,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;It would appear that you have the problem detailed here.&lt;/P&gt;&lt;P&gt;CW10 probably still deliberately breaks this as 6.3 did.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;"osbdm-JM60" refers to the open source BDM made with a JM60&lt;/P&gt;&lt;P&gt;Refer to the community projects section of the fora.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Sep 2010 04:22:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Codewarrior-10-Can-t-Debug/m-p/147167#M1823</guid>
      <dc:creator>peg</dc:creator>
      <dc:date>2010-09-16T04:22:05Z</dc:date>
    </item>
    <item>
      <title>Re: Codewarrior 10 Can't Debug</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Codewarrior-10-Can-t-Debug/m-p/147168#M1824</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It doesn't even work on a win XP PC... That's bad... really bad... I can't continue with my applications!!! Is any way to solve that? I mean, is there a way to use demo JM Board with CW 10?????&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'd really appreciatte any help here!!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best of lucks!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;One more thing: the DEMO JM Board has a P&amp;amp;E Multilinkd BDM embedded, it's not an OSBDM, right?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 19 Sep 2010 08:32:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Codewarrior-10-Can-t-Debug/m-p/147168#M1824</guid>
      <dc:creator>sebasira</dc:creator>
      <dc:date>2010-09-19T08:32:44Z</dc:date>
    </item>
    <item>
      <title>Re: Codewarrior 10 Can't Debug</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Codewarrior-10-Can-t-Debug/m-p/147169#M1825</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;What MCU are you trying to debug with DEMOJM? I think DEMOJM can be used to debug only MCU's it was designed for: S08 JM128 and CFV1 JM128. And nothing else, I think. It is similar with DEMOQE board. I can debug QE128. But if I choose for example QE32 or QE64, it won't connect. CW V6.1 allowed connection to other MCUs, but not more recent CW versions. Do you have&amp;nbsp;problems connecting to original DEMOJM MCU modules?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 19 Sep 2010 16:04:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Codewarrior-10-Can-t-Debug/m-p/147169#M1825</guid>
      <dc:creator>kef</dc:creator>
      <dc:date>2010-09-19T16:04:58Z</dc:date>
    </item>
    <item>
      <title>Re: Codewarrior 10 Can't Debug</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Codewarrior-10-Can-t-Debug/m-p/147170#M1826</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;It seems I forgot to link in what I was talking about. &lt;A href="https://community.freescale.com/message/49272#49272" title="https://community.freescale.com/message/49272#49272"&gt;https://community.freescale.com/message/49272#49272&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The embedded BDM in the Demo JM board is indeed a P&amp;amp;E Multilink.&lt;/P&gt;&lt;P&gt;Supposedly it has less protection fitted to it than the real thing but retains ALL of the functionality in the hardware.&lt;/P&gt;&lt;P&gt;Where the problem comes is that since Codewarrior 6.2 (6.3?) a supplied DLL deliberately hobbles the embedded multilink into only communicating with the type of device that the board is meant to be a demo for.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;There is no technical reason for this!&lt;/P&gt;&lt;P&gt;Neither is there any reason given by Freescale.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The problem seems to be that the demoboards identify themselves as a DEMOQE or whatever.&lt;/P&gt;&lt;P&gt;Later DLL's pick this up and then deliberately do not allow any other device.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;A hack to bypass this is detailed in the linked thread.&lt;/P&gt;&lt;P&gt;I don't know whether this works with CW10. Please let us know.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 19 Sep 2010 18:48:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Codewarrior-10-Can-t-Debug/m-p/147170#M1826</guid>
      <dc:creator>peg</dc:creator>
      <dc:date>2010-09-19T18:48:02Z</dc:date>
    </item>
    <item>
      <title>Re: Codewarrior 10 Can't Debug</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Codewarrior-10-Can-t-Debug/m-p/147171#M1827</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Well Kef, I'm using it to debug a CFV1, it's a QE32... Works fine with CW 6.1 over win XP. So you say that codewarrior versions above v6.1 won't let me connect to other MCU different from JM?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I haven' try with the daugther cards yet.. It's a good test, I'll give it a try and let you know&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 20 Sep 2010 20:58:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Codewarrior-10-Can-t-Debug/m-p/147171#M1827</guid>
      <dc:creator>sebasira</dc:creator>
      <dc:date>2010-09-20T20:58:43Z</dc:date>
    </item>
    <item>
      <title>Re: Codewarrior 10 Can't Debug</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Codewarrior-10-Can-t-Debug/m-p/147172#M1828</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Peg, thanks for the linked thread! I'll take a look a it and see if this solve my problem... Any news I have, I'll let you know!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks! have a nice day&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 20 Sep 2010 21:01:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Codewarrior-10-Can-t-Debug/m-p/147172#M1828</guid>
      <dc:creator>sebasira</dc:creator>
      <dc:date>2010-09-20T21:01:32Z</dc:date>
    </item>
    <item>
      <title>Re: Codewarrior 10 Can't Debug</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Codewarrior-10-Can-t-Debug/m-p/147173#M1829</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Peg... well I read the whole thread about the hack, but there's no folder "prog" under CW 10 installation path. There's new one named "Drivers" but under it there aren't such DLL files...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I found a "prog" folder under other one named "MCU" but those files weren't there, neither.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;What can I do?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Beste Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Sep 2010 03:29:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Codewarrior-10-Can-t-Debug/m-p/147173#M1829</guid>
      <dc:creator>sebasira</dc:creator>
      <dc:date>2010-09-21T03:29:02Z</dc:date>
    </item>
    <item>
      <title>Re: Codewarrior 10 Can't Debug</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Codewarrior-10-Can-t-Debug/m-p/147174#M1830</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sebastian,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I don't generally use Codewarrior, so I don't have CW10 installed nor the time to muck around with it now.&lt;/P&gt;&lt;P&gt;Your options at the moment are:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;1. Use CW6.1.&lt;/P&gt;&lt;P&gt;2. Use a real Multilink&lt;/P&gt;&lt;P&gt;3. Figure it out for yourself, post the method here and become a legend&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Sep 2010 05:03:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Codewarrior-10-Can-t-Debug/m-p/147174#M1830</guid>
      <dc:creator>peg</dc:creator>
      <dc:date>2010-09-21T05:03:24Z</dc:date>
    </item>
    <item>
      <title>Re: Codewarrior 10 Can't Debug</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Codewarrior-10-Can-t-Debug/m-p/147175#M1831</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Well peg, as I need to continue my development kind of&amp;nbsp; "right-now" I decided to try using CW 6.1 over win 7 x64... I'm having some problems and I open a new thread, &lt;A __default_attr="69839" class="jive_macro jive_macro_thread default_title" href="https://community.freescale.com/thread/69839" jivemacro="thread" title="here it is"&gt;here it is&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I think you may help me, I've noticed you had a lot of participation in every thread I mention.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please, unless any of you find a solution to "Using a DEMO BOARD to Debug a MCU different from what the demo board was ment to with CW 10 over win 7 x64" do not reply on this thread... I'll continue in the new one, linked above.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks everyone!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Sep 2010 09:33:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Codewarrior-10-Can-t-Debug/m-p/147175#M1831</guid>
      <dc:creator>sebasira</dc:creator>
      <dc:date>2010-09-22T09:33:40Z</dc:date>
    </item>
  </channel>
</rss>