<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: PCS for MX21 in Classic/Legacy CodeWarrior</title>
    <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/PCS-for-MX21/m-p/140693#M1327</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;BR /&gt;&lt;BLOCKQUOTE&gt;&lt;HR /&gt;hazmatto wrote:&lt;BR /&gt;I am trying to get the Platform Creation Suite v3.01 running on linux for development on the MX21ADS platform.&lt;BR /&gt;After fixing a typo in the installation script on the CD and recreating the installation media, and backgrading our linux development machine to have compatible libraries, we were finally able to install the PCS and the Linux Board Support Package that came with the development kit.&lt;BR /&gt;However, when try and run the Target Wizard, it quits with a message about licensing. We have received a license key from Freescale/Codewarrior, but we can't seem to install the license key. There does not seem to be a license.dat file anywhere or a license manager.&lt;BR /&gt;Are we missing something? Or do we just need to find the correct spot in the directory structure (/opt/Embedix) to create a license.dat file with the key in it?&lt;BR /&gt;&lt;BR /&gt;Thanks.&lt;BR /&gt;-mat&lt;BR /&gt;&lt;HR /&gt;&lt;/BLOCKQUOTE&gt;&lt;BR /&gt;I just noticed that there is a new release of the imx21 bsp (release date 2006 12-12) which probably runs with the LTIB (open-source version of Platform Creation Suite) so I might not have to solve this problem. Downloading it now.&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 20 Dec 2006 04:34:34 GMT</pubDate>
    <dc:creator>hazmatto</dc:creator>
    <dc:date>2006-12-20T04:34:34Z</dc:date>
    <item>
      <title>PCS for MX21</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/PCS-for-MX21/m-p/140692#M1326</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;I am trying to get the Platform Creation Suite v3.01 running on linux for development on the MX21ADS platform.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;After fixing a typo in the installation script on the CD and recreating the installation media, and backgrading our linux development machine to have compatible libraries, we were finally able to install the PCS and the Linux Board Support Package that came with the development kit.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;However, when try and run the Target Wizard, it quits with a message about licensing. We have received a license key from Freescale/Codewarrior, but we can't seem to install the license key. There does not seem to be a license.dat file anywhere or a license manager.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Are we missing something? Or do we just need to find the correct spot in the directory structure (/opt/Embedix) to create a license.dat file with the key in it?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;-mat&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Dec 2006 02:18:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/PCS-for-MX21/m-p/140692#M1326</guid>
      <dc:creator>hazmatto</dc:creator>
      <dc:date>2006-12-20T02:18:35Z</dc:date>
    </item>
    <item>
      <title>Re: PCS for MX21</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/PCS-for-MX21/m-p/140693#M1327</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;BR /&gt;&lt;BLOCKQUOTE&gt;&lt;HR /&gt;hazmatto wrote:&lt;BR /&gt;I am trying to get the Platform Creation Suite v3.01 running on linux for development on the MX21ADS platform.&lt;BR /&gt;After fixing a typo in the installation script on the CD and recreating the installation media, and backgrading our linux development machine to have compatible libraries, we were finally able to install the PCS and the Linux Board Support Package that came with the development kit.&lt;BR /&gt;However, when try and run the Target Wizard, it quits with a message about licensing. We have received a license key from Freescale/Codewarrior, but we can't seem to install the license key. There does not seem to be a license.dat file anywhere or a license manager.&lt;BR /&gt;Are we missing something? Or do we just need to find the correct spot in the directory structure (/opt/Embedix) to create a license.dat file with the key in it?&lt;BR /&gt;&lt;BR /&gt;Thanks.&lt;BR /&gt;-mat&lt;BR /&gt;&lt;HR /&gt;&lt;/BLOCKQUOTE&gt;&lt;BR /&gt;I just noticed that there is a new release of the imx21 bsp (release date 2006 12-12) which probably runs with the LTIB (open-source version of Platform Creation Suite) so I might not have to solve this problem. Downloading it now.&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Dec 2006 04:34:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/PCS-for-MX21/m-p/140693#M1327</guid>
      <dc:creator>hazmatto</dc:creator>
      <dc:date>2006-12-20T04:34:34Z</dc:date>
    </item>
  </channel>
</rss>