<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic pop up when writting code in Classic/Legacy CodeWarrior</title>
    <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/pop-up-when-writting-code/m-p/139799#M1252</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;I have a mystery window pop up when I am writting code. If i type the name&amp;nbsp; of a function e.g&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;read_isc_test_resp(&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;(this calls an already written function)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I get a window pop up when I type the '('/ Ithe window has two parts, the top one has a little 'barbers pole' and the words 'Method:read_isp_test_resp' with&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;{}void&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;underneath&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The lower part has 'No variables avail'&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;When I continue typing, the window changes and displays 'Searching for'&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;This is annoying and also seems to cause a 'CR with no LF' error, which is even more annoying . I have to close the file and open it again for the editor to correct this.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Is there some way of disabling this pop up?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Steve&lt;/SPAN&gt;&lt;BR /&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 12 Jul 2007 17:01:00 GMT</pubDate>
    <dc:creator>stevec</dc:creator>
    <dc:date>2007-07-12T17:01:00Z</dc:date>
    <item>
      <title>pop up when writting code</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/pop-up-when-writting-code/m-p/139799#M1252</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;I have a mystery window pop up when I am writting code. If i type the name&amp;nbsp; of a function e.g&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;read_isc_test_resp(&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;(this calls an already written function)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I get a window pop up when I type the '('/ Ithe window has two parts, the top one has a little 'barbers pole' and the words 'Method:read_isp_test_resp' with&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;{}void&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;underneath&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The lower part has 'No variables avail'&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;When I continue typing, the window changes and displays 'Searching for'&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;This is annoying and also seems to cause a 'CR with no LF' error, which is even more annoying . I have to close the file and open it again for the editor to correct this.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Is there some way of disabling this pop up?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Steve&lt;/SPAN&gt;&lt;BR /&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Jul 2007 17:01:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/pop-up-when-writting-code/m-p/139799#M1252</guid>
      <dc:creator>stevec</dc:creator>
      <dc:date>2007-07-12T17:01:00Z</dc:date>
    </item>
    <item>
      <title>Re: pop up when writting code</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/pop-up-when-writting-code/m-p/139800#M1253</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hello&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Not sure which version of CodeWarrior you are using and which CPU you are targeting.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Anyway it looks like a Code Completion window popping up.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Can you try the following:&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp; - Start the IDE&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp; - Select Edit -&amp;gt;&amp;nbsp;"Preferences"&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&amp;nbsp;- Switch to Code Completion" panel in "Editor" tree&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp; - Uncheck all boxes in that panel.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp; - Close the IDE Preferences dialog clicking on OK&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Does that solve the problem?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;CrasyCat&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Jul 2007 17:50:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/pop-up-when-writting-code/m-p/139800#M1253</guid>
      <dc:creator>CrasyCat</dc:creator>
      <dc:date>2007-07-12T17:50:56Z</dc:date>
    </item>
    <item>
      <title>Re: pop up when writting code</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/pop-up-when-writting-code/m-p/139801#M1254</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Yes it seems to sort it. Thanks very much. Can't understand what was happening but it's gone now. Most grateful.&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Jul 2007 18:19:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/pop-up-when-writting-code/m-p/139801#M1254</guid>
      <dc:creator>stevec</dc:creator>
      <dc:date>2007-07-12T18:19:11Z</dc:date>
    </item>
  </channel>
</rss>