<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>ColdFire/68K Microcontrollers and ProcessorsのトピックRe: Touble when more than 1 PIT is deployed (5282)</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Touble-when-more-than-1-PIT-is-deployed-5282/m-p/207732#M9963</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;gt; MCF_INTC0_IMRH &amp;amp;= ~(isr_mask | MCF_INTC_IMRL_MASKALL) ;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;One small thing I noticed is I don't think you want to use the IMRL's MASKALL on the IMRH...&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;But I doubt that could cause what you are seeing.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;gt; MCF_INTC0_ICR(intC0_ICR) |=&amp;nbsp; (MCF_INTC_ICR_IL(isr_level) | MCF_INTC_ICR_IP(isr_priority));&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I also don't think you want "|=" here...&amp;nbsp; Just "=".&amp;nbsp; (The reset value is 0, so you should be OK anyway.)&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;-- Rich&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 06 Dec 2008 12:25:19 GMT</pubDate>
    <dc:creator>RichTestardi</dc:creator>
    <dc:date>2008-12-06T12:25:19Z</dc:date>
    <item>
      <title>Touble when more than 1 PIT is deployed (5282)</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Touble-when-more-than-1-PIT-is-deployed-5282/m-p/207731#M9962</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;P&gt;Hi,&lt;BR /&gt;&lt;BR /&gt;I have written a PIT0_init()&amp;nbsp; function that generates an ISR upon timeout.&lt;BR /&gt;&lt;BR /&gt;I also have a PIT1_init()&amp;nbsp; function that generates an ISR upon timeout.&lt;BR /&gt;&lt;BR /&gt;When I call PIT0_init&amp;nbsp;() only within the application, everything works as expected (ISR called at regular interval).&lt;BR /&gt;&lt;BR /&gt;Dido when I call PIT1_init() only within the application, everything works as expected.&lt;BR /&gt;&lt;BR /&gt;Nevertheless, when I call both PIT0_init() and PIT1_init(), no ISR are generated anymore.&lt;BR /&gt;&lt;BR /&gt;We can only use one PIT at a time?&lt;BR /&gt;&lt;BR /&gt;Any hints?&lt;BR /&gt;&lt;BR /&gt;S.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;DIV class="msg_source_code"&gt;&lt;DIV class="text_smallest"&gt;Code:&lt;/DIV&gt;&lt;PRE&gt;//FUNCT: Bsp_PIT_err_t PIT0_init (const uint32 timeout_ms){ return pit_init(timeout_ms, 0);}//FUNCT: Bsp_PIT_err_t PIT1_init (const uint32 timeout_ms){ return pit_init(timeout_ms, 1); }//FUNCT: static Bsp_PIT_err_t pit_init(const uint32 timeout_ms, const uint8 pit_num){ const uint16 PRESCALER=0;// [0; 2^16] const uint32 PMR = (timeout_ms * SYSTEM_CLOCK_KHZ/2)&amp;nbsp; - 1; // Modulo [0; 0xFFFF] uint8&amp;nbsp; isr_level&amp;nbsp; = ISR_LEVEL_PIT0; uint8&amp;nbsp; isr_priority=ISR_PRIORITY_PIT0; uint32 isr_mask&amp;nbsp;&amp;nbsp; = MCF_INTC_IMRH_INT_MASK55; uint8&amp;nbsp; intC0_ICR&amp;nbsp; = 55;&amp;nbsp; // Make sure that number is 0, 1 and 2 if(pit_num !=0 &amp;amp;&amp;amp; pit_num != 1 &amp;amp;&amp;amp; pit_num != 2)&amp;nbsp; return BSP_PIT_WRONG_CHNL;&amp;nbsp; // Validate Modulo if(PMR &amp;gt; 0xFFFF)&amp;nbsp; return BSP_PIT_WRONG_MODULO;&amp;nbsp; // Point to right PIT if(pit_num==0) {&amp;nbsp; isr_level&amp;nbsp; = ISR_LEVEL_PIT0;&amp;nbsp; isr_priority=ISR_PRIORITY_PIT0;&amp;nbsp; isr_mask&amp;nbsp;&amp;nbsp; = MCF_INTC_IMRH_INT_MASK55;&amp;nbsp; intC0_ICR&amp;nbsp; = 55; } if(pit_num==1) {&amp;nbsp; isr_level&amp;nbsp; = ISR_LEVEL_PIT1;&amp;nbsp; isr_priority=ISR_PRIORITY_PIT1;&amp;nbsp; isr_mask&amp;nbsp;&amp;nbsp; = MCF_INTC_IMRH_INT_MASK56;&amp;nbsp; intC0_ICR&amp;nbsp; = 56; } if(pit_num==2) {&amp;nbsp; isr_level&amp;nbsp; = ISR_LEVEL_PIT2;&amp;nbsp; isr_priority=ISR_PRIORITY_PIT2;&amp;nbsp; isr_mask&amp;nbsp;&amp;nbsp; = MCF_INTC_IMRH_INT_MASK57;&amp;nbsp; intC0_ICR&amp;nbsp; = 57; }&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Disable interrupts mcf5xxx_irq_disable ();&amp;nbsp;&amp;nbsp; //&amp;nbsp; Sets the level and priority of this interrupt MCF_INTC0_ICR(intC0_ICR) |=&amp;nbsp; (MCF_INTC_ICR_IL(isr_level) | MCF_INTC_ICR_IP(isr_priority)); // Unmask interrupt source&amp;nbsp;&amp;nbsp;&amp;nbsp; MCF_INTC0_IMRH &amp;amp;= ~(isr_mask | MCF_INTC_IMRL_MASKALL) ;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Configure PIT&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Set PRE (prescaler) MCF_PIT_PCSR(pit_num)&amp;nbsp; = (uint16)(MCF_PIT_PCSR_PRE(PRESCALER));&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Modulo count&amp;nbsp; MCF_PIT_PMR(pit_num) = (vuint16)(PMR &amp;amp; 0xFFFF);&amp;nbsp; // Pit Control Status Register MCF_PIT_PCSR(pit_num) |=&amp;nbsp; MCF_PIT_PCSR_OVW |&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; MCF_PIT_PCSR_PIE |&amp;nbsp; // Enable interrupt&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; MCF_PIT_PCSR_PIF |&amp;nbsp; // Reset PIF&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; MCF_PIT_PCSR_RLD |&amp;nbsp; // Copy Modulus in counter when 0 is reached&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; MCF_PIT_PCSR_EN;&amp;nbsp;&amp;nbsp;&amp;nbsp; // EN = 1&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Enable interrupts&amp;nbsp;&amp;nbsp;&amp;nbsp; mcf5xxx_irq_enable ();&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Done&amp;nbsp;&amp;nbsp;&amp;nbsp; return BSP_PIT_NO_ERROR;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;/PRE&gt;&lt;/DIV&gt;&lt;P&gt;&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 06 Dec 2008 06:43:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Touble-when-more-than-1-PIT-is-deployed-5282/m-p/207731#M9962</guid>
      <dc:creator>SVC2</dc:creator>
      <dc:date>2008-12-06T06:43:41Z</dc:date>
    </item>
    <item>
      <title>Re: Touble when more than 1 PIT is deployed (5282)</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Touble-when-more-than-1-PIT-is-deployed-5282/m-p/207732#M9963</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;gt; MCF_INTC0_IMRH &amp;amp;= ~(isr_mask | MCF_INTC_IMRL_MASKALL) ;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;One small thing I noticed is I don't think you want to use the IMRL's MASKALL on the IMRH...&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;But I doubt that could cause what you are seeing.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;gt; MCF_INTC0_ICR(intC0_ICR) |=&amp;nbsp; (MCF_INTC_ICR_IL(isr_level) | MCF_INTC_ICR_IP(isr_priority));&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I also don't think you want "|=" here...&amp;nbsp; Just "=".&amp;nbsp; (The reset value is 0, so you should be OK anyway.)&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;-- Rich&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 06 Dec 2008 12:25:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Touble-when-more-than-1-PIT-is-deployed-5282/m-p/207732#M9963</guid>
      <dc:creator>RichTestardi</dc:creator>
      <dc:date>2008-12-06T12:25:19Z</dc:date>
    </item>
  </channel>
</rss>