<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Memory mapped I/O from Linux device driver in ColdFire/68K Microcontrollers and Processors</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Memory-mapped-I-O-from-Linux-device-driver/m-p/207395#M9937</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;This is the quick and dirty way I did it to force a mapping that worked from just about anywhere.&amp;nbsp; Note that it also disables ints so that you don't accidentally use that mapping taking an irq.&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 06 Jan 2010 05:31:36 GMT</pubDate>
    <dc:creator>jkmahan</dc:creator>
    <dc:date>2010-01-06T05:31:36Z</dc:date>
    <item>
      <title>Memory mapped I/O from Linux device driver</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Memory-mapped-I-O-from-Linux-device-driver/m-p/207393#M9935</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm new to Linux device driver writing. Can anyone offer any advice on the proper way to access memory mapped hardware registers?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm tinkering with stuff using MCF54455EVB. This has a 7-segment LED display. So, from u-boot I can display "12" on it just by doing:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-&amp;gt; mw.l 0x09000014 0x12&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Now I'm trying to do the same thing from a Linux device driver. According to books/online sources this should work:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;#define LED_REG_ADDRESS 0x09000014&lt;BR /&gt;&amp;nbsp; void __iomem *reg;&lt;BR /&gt;&amp;nbsp; request_mem_region(LED_REG_ADDRESS, 4, "LED");&lt;BR /&gt;&amp;nbsp; reg = ioremap_nocache(LED_REG_ADDRESS, 4);&lt;BR /&gt;&amp;nbsp; printk(KERN_INFO "LED phys = %x, virtual = %x\n",&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp; LED_REG_ADDRESS,&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp; (unsigned int)reg);&lt;BR /&gt;&amp;nbsp; writel(0x00000012, reg);&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;I'm assuming that ioremap_nocache should program the MMU to give a translation from kernal allocated virtual address to the actual physical register addess with no cacheing.&amp;nbsp; When it runs it prints the following, but the LED does not change.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;LED phys = 9000014, virtual = e1002014&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;and /proc/iomem shows me that the address has been registered. Have tried all sorts of variations on the above code, but nothing works. Anybody have any ideas?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 14 Aug 2009 15:37:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Memory-mapped-I-O-from-Linux-device-driver/m-p/207393#M9935</guid>
      <dc:creator>jon_fbrj99</dc:creator>
      <dc:date>2009-08-14T15:37:04Z</dc:date>
    </item>
    <item>
      <title>Re: Memory mapped I/O from Linux device driver</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Memory-mapped-I-O-from-Linux-device-driver/m-p/207394#M9936</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I remember having the same problem trying to use ioremap_nocache() per the Linux device drivers books.&amp;nbsp; Finally I searched through the Freescale Coldfire kernel code and found this in arch/m68k/coldfire/mcf5445x-pci.c:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp; &amp;nbsp; /* setup FPGA to route PCI to IRQ3(67), SW7 to IRQ7, SW6 to IRQ4 */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; set_fpga(FPGA_PCI_IRQ_ENABLE, 0x00000000);&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; set_fpga(FPGA_PCI_IRQ_ROUTE, 0x00000039);&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; set_fpga(FPGA_SEVEN_LED, 0x000000FF);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The set_fpga() function is defined as an assembly routine in&amp;nbsp; arch/m68k/coldfire/head.S.&amp;nbsp; It manipulates the Access Control Register ACR0:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /*&lt;BR /&gt;&amp;nbsp; &amp;nbsp;&amp;nbsp; * set_fpga(addr,val)&lt;BR /&gt;&amp;nbsp; &amp;nbsp;&amp;nbsp; *&lt;BR /&gt;&amp;nbsp; &amp;nbsp;&amp;nbsp; * Map in 0x00000000 -&amp;gt; 0x0fffffff and then do the write.&lt;BR /&gt;&amp;nbsp; &amp;nbsp;&amp;nbsp; */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; set_fpga:&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; movew&amp;nbsp;&amp;nbsp; %sr,%d1&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; movew&amp;nbsp;&amp;nbsp; #0x2700,%sr&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; movel&amp;nbsp;&amp;nbsp; ACR0_FPGA, %d0&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; movec&amp;nbsp;&amp;nbsp; %d0, %acr0&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; nop&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; moveal&amp;nbsp; 4(%sp),%a0&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; movel&amp;nbsp;&amp;nbsp; 8(%sp),%a0@&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; movel&amp;nbsp;&amp;nbsp; ACR0_DEFAULT, %d0&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; movec&amp;nbsp;&amp;nbsp; %d0, %acr0&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; nop&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; movew&amp;nbsp;&amp;nbsp; %d1,%sr&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; rts&lt;BR /&gt;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .data&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .align&amp;nbsp; 4&lt;BR /&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;Using this function should allow you write to the 7-seg using the 0x09000014 physical address directly.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Jan 2010 04:32:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Memory-mapped-I-O-from-Linux-device-driver/m-p/207394#M9936</guid>
      <dc:creator>ghp</dc:creator>
      <dc:date>2010-01-06T04:32:33Z</dc:date>
    </item>
    <item>
      <title>Re: Memory mapped I/O from Linux device driver</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Memory-mapped-I-O-from-Linux-device-driver/m-p/207395#M9937</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;This is the quick and dirty way I did it to force a mapping that worked from just about anywhere.&amp;nbsp; Note that it also disables ints so that you don't accidentally use that mapping taking an irq.&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Jan 2010 05:31:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Memory-mapped-I-O-from-Linux-device-driver/m-p/207395#M9937</guid>
      <dc:creator>jkmahan</dc:creator>
      <dc:date>2010-01-06T05:31:36Z</dc:date>
    </item>
    <item>
      <title>Re: Memory mapped I/O from Linux device driver</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Memory-mapped-I-O-from-Linux-device-driver/m-p/207396#M9938</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In order to&amp;nbsp;write a value in a memory mapped register&amp;nbsp;I&amp;nbsp;do the following:&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;(for instance)&lt;/P&gt;&lt;P&gt;#define LED_WRITE&amp;nbsp; 0x90000002&amp;nbsp;&amp;nbsp; /* memory mapped address */&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; static unsigned char ls_leds = 0xFF;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; unsigned char *la_writeLed;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; la_writeLed = ioremap ((volatile unsigned long)LED_WRITE, 4);&amp;nbsp;&amp;nbsp; /* use IOREMAP */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; ...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; ...&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; *(la_writeLed) = ls_leds;&amp;nbsp; /* write the desirable value in the register */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hope this helps!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 09 Jan 2010 00:35:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Memory-mapped-I-O-from-Linux-device-driver/m-p/207396#M9938</guid>
      <dc:creator>raulen</dc:creator>
      <dc:date>2010-01-09T00:35:00Z</dc:date>
    </item>
    <item>
      <title>Re: Memory mapped I/O from Linux device driver</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Memory-mapped-I-O-from-Linux-device-driver/m-p/207397#M9939</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;I can now see why my original did not work. Writing directly via a pointer returned from ioremap (as shown by raulen) works. Writing the same value using writel() does not work. This is because writel is endian swapping the value! So to write 0x12345678 to a 32 bit memory mapped register I can either do *reg = 0x12345678 or writel(0x87654321, reg). Strange but true.&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 Jan 2010 19:48:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Memory-mapped-I-O-from-Linux-device-driver/m-p/207397#M9939</guid>
      <dc:creator>jon_fbrj99</dc:creator>
      <dc:date>2010-01-22T19:48:51Z</dc:date>
    </item>
  </channel>
</rss>