<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>ColdFire/68K Microcontrollers and Processors中的主题 Re: MCF52211 &amp; MCF52223 documentation questions</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF52211-MCF52223-documentation-questions/m-p/207359#M9926</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;gt; &lt;EM&gt;Does the MCF52223 need a 48MHz crystal or an 8MHz crystal ?&lt;/EM&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I believe you can use either.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I have run the part with just the internal 8MHz relaxation oscillator, and it seems to work just fine on USB; however, I would not recommend this except in prototype applications since the USB full speed spec requires a 2500ppm clock tolerance, and the relaxation oscillator has a 20,000ppm tolerance.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;The disadvantage of using&amp;nbsp;an 8MHz crystal is that USB *has* to run at 48MHz, so you have to PLL from 8MHz to 48MHz and set USB_CTRL:CLK_SRC to 3, limiting the CPU speed to the same speed as USB (48MHz); the advantage of using an 8MHz crystal is that you can run the exact same SW (PLL dividers, etc.) as with the relaxation oscillator, with just a change of the CLKMOD0 pin.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;The advantage of using a 48MHz crystal, on the other hand, is you can drive USB directly from the oscillator by setting USB_CTRL:CLK_SRC to 1, and then you can PLL the CPU up to 64MHz or 80MHz, depending on the part (I do this).&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;gt; &lt;EM&gt;What should i connect VDD_USB to ? Just to Vdd ?&lt;/EM&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I connect it to VDD, but I just followed the DEMO board schematic.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;-- Rich&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 05 Dec 2008 00:17:51 GMT</pubDate>
    <dc:creator>RichTestardi</dc:creator>
    <dc:date>2008-12-05T00:17:51Z</dc:date>
    <item>
      <title>MCF52211 &amp; MCF52223 documentation questions</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF52211-MCF52223-documentation-questions/m-p/207358#M9925</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;We are designing a board with an MCF52223 (possibly an MCF52211)&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;DIV&gt;The MCF52223 Reference Manual is very bad.&lt;DIV&gt;I think it is a must to overlay the MCF52211 Reference Manual on it.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Questions remaining:&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;DIV&gt;The MCF52223 Reference Manual states that the reference&amp;nbsp; crystal is 1-16MHz (par 5.2)&lt;DIV&gt;&lt;DIV&gt;&lt;DIV&gt;The MCF52223 Reference Manual uses an 8MHz&amp;nbsp;reference&amp;nbsp; crystal (figure 5.11)&lt;/DIV&gt;The MCF52211 Reference Manual states that the reference&amp;nbsp; crystal is 1-48MHz (par 6.2)&lt;/DIV&gt;&lt;DIV&gt;&lt;DIV&gt;The MCF52211 Reference Manual uses a 48MHz&amp;nbsp;reference&amp;nbsp; crystal (figure 6.12)&lt;/DIV&gt;The MCF52223EVB schematic (that is not provided by FreeScale but by Axiom altough it is a FreeScale product, not an Axiom product) uses an 48MHz crystal...&lt;/DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;EM&gt;Does the MCF52223 need a 48MHz crystal or an 8MHz crystal ?&lt;/EM&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;--------&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;The pin function&amp;nbsp;desriptions of the MCF52223 Reference Manual (par 2) show USB pin function in the quad function selections.&lt;/DIV&gt;&lt;DIV&gt;The pin desriptions of the MCF52223 Reference Manual (par 2.4 and on) show *no* USB pins.&lt;/DIV&gt;&lt;DIV&gt;(Not even USB_DP and VDD_USB).&lt;/DIV&gt;&lt;DIV&gt;The MCF52211 Reference Manual shows removal of the USB function pins in the Revision history (Appendix B.1)&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;EM&gt;What should i connect VDD_USB to ? Just to Vdd ?&lt;/EM&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;EM&gt;Does the MCF52223&amp;nbsp;actually have the quaternary USB pin functions ?&lt;/EM&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;--------&lt;/DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;PTDPAR (0x1000_0070) is not present (Reserved) in the MCF52223 RM ....&lt;/DIV&gt;&lt;DIV&gt;Altough page 2-5 and chapter 21 make me doubt that.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;EM&gt;Do the MCF52223 and/or the MCF52211 have a working PTDPAR ?&lt;/EM&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Header files i found after a long search seem to disagree.&lt;/DIV&gt;&lt;DIV&gt;Not only about PTDPAR but also about bits in it (eg. PWM2/PWM3)&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;(*sigh* why is it a puzzle, *not* documentation?)&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Dec 2008 23:49:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF52211-MCF52223-documentation-questions/m-p/207358#M9925</guid>
      <dc:creator>MrBean</dc:creator>
      <dc:date>2008-12-04T23:49:23Z</dc:date>
    </item>
    <item>
      <title>Re: MCF52211 &amp; MCF52223 documentation questions</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF52211-MCF52223-documentation-questions/m-p/207359#M9926</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;gt; &lt;EM&gt;Does the MCF52223 need a 48MHz crystal or an 8MHz crystal ?&lt;/EM&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I believe you can use either.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I have run the part with just the internal 8MHz relaxation oscillator, and it seems to work just fine on USB; however, I would not recommend this except in prototype applications since the USB full speed spec requires a 2500ppm clock tolerance, and the relaxation oscillator has a 20,000ppm tolerance.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;The disadvantage of using&amp;nbsp;an 8MHz crystal is that USB *has* to run at 48MHz, so you have to PLL from 8MHz to 48MHz and set USB_CTRL:CLK_SRC to 3, limiting the CPU speed to the same speed as USB (48MHz); the advantage of using an 8MHz crystal is that you can run the exact same SW (PLL dividers, etc.) as with the relaxation oscillator, with just a change of the CLKMOD0 pin.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;The advantage of using a 48MHz crystal, on the other hand, is you can drive USB directly from the oscillator by setting USB_CTRL:CLK_SRC to 1, and then you can PLL the CPU up to 64MHz or 80MHz, depending on the part (I do this).&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;gt; &lt;EM&gt;What should i connect VDD_USB to ? Just to Vdd ?&lt;/EM&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I connect it to VDD, but I just followed the DEMO board schematic.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;-- Rich&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Dec 2008 00:17:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF52211-MCF52223-documentation-questions/m-p/207359#M9926</guid>
      <dc:creator>RichTestardi</dc:creator>
      <dc:date>2008-12-05T00:17:51Z</dc:date>
    </item>
    <item>
      <title>Re: MCF52211 &amp; MCF52223 documentation questions</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF52211-MCF52223-documentation-questions/m-p/207360#M9927</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;The MCF52223DS par 2.7 page 33 states that the crystal reference frequency is min 2MHz and max 10MHz.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;48MHz is right out .. (holy handgrenade, anyone ? &lt;IMG alt=":smileywink:" class="emoticon emoticon-smileywink" id="smileywink" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-wink.gif" title="Smiley Wink" /&gt; )&lt;/DIV&gt;&lt;P&gt;&lt;BR /&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The MCF52211DS states the same btw, max 10MHz ....&lt;/P&gt;&lt;BR /&gt;&lt;BR /&gt;PS: I see now that it is not the crystal frequency that is meant here, but the frequency after the predivider.&lt;BR /&gt;&lt;BR /&gt;Message Edited by MrBean on &lt;SPAN class="date_text"&gt;2008-12-04&lt;/SPAN&gt; &lt;SPAN class="time_text"&gt;08:38 PM&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Dec 2008 03:31:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF52211-MCF52223-documentation-questions/m-p/207360#M9927</guid>
      <dc:creator>MrBean</dc:creator>
      <dc:date>2008-12-05T03:31:57Z</dc:date>
    </item>
    <item>
      <title>Re: MCF52211 &amp; MCF52223 documentation questions</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF52211-MCF52223-documentation-questions/m-p/207361#M9928</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&amp;gt; The MCF52223DS par 2.7 page 33 states that the crystal reference freqency is min 2MHz and max 10MHz.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I think that's the limit for the PLL input when driven (indirectly) by the crystal.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;But the PLL gets the input *after* the pre-divider.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;So when you run a 48MHz crystal (like all the DEMO boards do), the pre-divider divides by 6 (which is actually its default setting).&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;This results in 8MHz to the PLL input, which is within spec.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;The diagram I always send folks to is figure 5-1 in MCF52223RM.pdf.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;-- Rich&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Dec 2008 03:39:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF52211-MCF52223-documentation-questions/m-p/207361#M9928</guid>
      <dc:creator>RichTestardi</dc:creator>
      <dc:date>2008-12-05T03:39:21Z</dc:date>
    </item>
    <item>
      <title>Re: MCF52211 &amp; MCF52223 documentation questions</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF52211-MCF52223-documentation-questions/m-p/207362#M9929</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;I will assume for now that this (from MCF52223RM) is utterly&amp;nbsp;wrong:&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;B&gt;&lt;FONT face="Helvetica-Bold" size="5"&gt;&lt;FONT face="Helvetica-Bold" size="5"&gt;&lt;/FONT&gt;&lt;/FONT&gt;&lt;/B&gt;&lt;P align="left"&gt;&lt;B&gt;&lt;FONT face="Helvetica-Bold" size="5"&gt;&lt;FONT face="Helvetica-Bold" size="5"&gt;5.2 Features&lt;/FONT&gt;&lt;/FONT&gt;&lt;/B&gt;&lt;/P&gt;&lt;FONT face="Times New Roman"&gt;&lt;/FONT&gt;&lt;P align="left"&gt;&lt;FONT face="Times New Roman"&gt;Features of the clock module include the following:&lt;/FONT&gt;&lt;/P&gt;&lt;P align="left"&gt;&lt;FONT face="Times New Roman"&gt;• 1- to 16-MHz crystal, ......&lt;/FONT&gt;&lt;/P&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I'll take a 48MHz crystal as it seems to help the usb controller.&lt;/DIV&gt;&lt;DIV&gt;(there is a note added on the bottom of the clock figure MCF52211RM)&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;-----------&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Found Vdd_USB in the 52223DS -&amp;gt; Vdd&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;-----------&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;That leaves the USB alternate pin functions and PTDPAR as remaining questions.&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Dec 2008 03:56:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF52211-MCF52223-documentation-questions/m-p/207362#M9929</guid>
      <dc:creator>MrBean</dc:creator>
      <dc:date>2008-12-05T03:56:25Z</dc:date>
    </item>
  </channel>
</rss>