<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>ColdFire/68K Microcontrollers and ProcessorsのトピックRe: Erasing Secured Flash</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Erasing-Secured-Flash/m-p/206426#M9822</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;To temporarily unsecure the device (until next reset) the backdoor keys can be used. This has to be performed by the program though since the debugger has no access in the secured state.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If you have secured a device and have no way to unsecure it in the program that is loaded (eg by commanding a mass erase) the only way to do it is via EZPORT and commanding a mass erase that way. The debugger (CFFlasher or other methods) will not work since the BDM is not active.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Search the forum for some programs that can be used to unlock FLASH via EZPORT. It is usually necessary to have a second board running the program connected via the EZPORT (much like a SPI connection).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.uTasker.com" rel="nofollow" target="_self"&gt;www.uTasker.com&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 11 Jun 2010 02:34:32 GMT</pubDate>
    <dc:creator>mjbcswitzerland</dc:creator>
    <dc:date>2010-06-11T02:34:32Z</dc:date>
    <item>
      <title>Erasing Secured Flash</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Erasing-Secured-Flash/m-p/206425#M9821</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;P&gt;CPU -&amp;gt; MCF 52235&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I cant erase secured flash. (i write&amp;nbsp;&amp;nbsp;0x00004AC8 @ 0x0414 )...&lt;/P&gt;&lt;P&gt;I have also tried whit CFFlasher&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If i define for instance&amp;nbsp;back-door&amp;nbsp;password, how can I access device in CW?&lt;/P&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 Jun 2010 21:01:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Erasing-Secured-Flash/m-p/206425#M9821</guid>
      <dc:creator>ralu</dc:creator>
      <dc:date>2010-06-10T21:01:56Z</dc:date>
    </item>
    <item>
      <title>Re: Erasing Secured Flash</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Erasing-Secured-Flash/m-p/206426#M9822</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;To temporarily unsecure the device (until next reset) the backdoor keys can be used. This has to be performed by the program though since the debugger has no access in the secured state.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If you have secured a device and have no way to unsecure it in the program that is loaded (eg by commanding a mass erase) the only way to do it is via EZPORT and commanding a mass erase that way. The debugger (CFFlasher or other methods) will not work since the BDM is not active.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Search the forum for some programs that can be used to unlock FLASH via EZPORT. It is usually necessary to have a second board running the program connected via the EZPORT (much like a SPI connection).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.uTasker.com" rel="nofollow" target="_self"&gt;www.uTasker.com&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 Jun 2010 02:34:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Erasing-Secured-Flash/m-p/206426#M9822</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2010-06-11T02:34:32Z</dc:date>
    </item>
    <item>
      <title>Re: Erasing Secured Flash</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Erasing-Secured-Flash/m-p/206427#M9823</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;P&amp;amp;E Micro have an application that will unsecure the flash.&lt;/P&gt;&lt;P&gt;Goto:&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.pemicro.com/products/product_viewDetails.cfm?product_id=163&amp;amp;CFID=2075065&amp;amp;CFTOKEN=c3ae58cc8c32fdfe-45FAE29A-A11E-AE4E-40A39186C41416CD" rel="nofollow" target="_blank"&gt;http://www.pemicro.com/products/product_viewDetails.cfm?product_id=163&amp;amp;CFID=2075065&amp;amp;CFTOKEN=c3ae58cc8c32fdfe-45FAE29A-A11E-AE4E-40A39186C41416CD&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Click on "FAQs, Manual's&amp;nbsp;&amp;amp; Download's"&lt;/P&gt;&lt;P&gt;Then look for &lt;STRONG&gt;&lt;U&gt;UNSECURE CF&lt;/U&gt;&lt;/STRONG&gt; on right side of page.&lt;/P&gt;&lt;P&gt;Assumptions:&lt;/P&gt;&lt;P&gt;You must place the ColdFire device into JTAG mode (usually a jumper setting on the EVB).&lt;/P&gt;&lt;P&gt;Set jumper so PSTCLK goes to pin 6 rather than pin 24 on the BDM header.&lt;/P&gt;&lt;P&gt;Use the P&amp;amp;E USB Multilink hardware.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;David&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Jun 2010 05:20:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Erasing-Secured-Flash/m-p/206427#M9823</guid>
      <dc:creator>DavidS</dc:creator>
      <dc:date>2010-06-16T05:20:24Z</dc:date>
    </item>
  </channel>
</rss>