<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MCF5329 MSCR_FLEXBUS and MSCR_SDRAM Registers, how do they work in SDR mode? in ColdFire/68K Microcontrollers and Processors</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5329-MSCR-FLEXBUS-and-MSCR-SDRAM-Registers-how-do-they-work/m-p/205592#M9717</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The MCF5329 can have its pins set up with different drive strengths.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can anyone help me understand what the MSCR_SDRAM and MSCR_FLEXBUS registers "mean" when using 3.3V SDR? The Reference Manual only seems to document DDR mode.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;This is well documented for all pins EXCEPT the Flexbus and SDRAM controller ones.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Typical non-SDRAM/FlexBus pins can be set up as:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;00 10pF&lt;/LI&gt;&lt;LI&gt;01 20pF&lt;/LI&gt;&lt;LI&gt;10 30pF&lt;/LI&gt;&lt;LI&gt;11 50pF&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;The MSCR_FLEXBUS and MSCR_SDRAM pins are documented as:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;00 Half strength 1.8V Mobile DDR.&lt;/LI&gt;&lt;LI&gt;01 Open drain.&lt;/LI&gt;&lt;LI&gt;10 Full strength 1.8V Mobile DDR.&lt;/LI&gt;&lt;LI&gt;11 2.5V DDR1 or 3.3V CMOS with roughly equal rise and fall delays.&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;That implies the only options for 3.3V SDR chips is the last one.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;But I really need 3.3V SDR with a low drive strength like the MCF5235 supported in the programming of its DSCR_EIM register.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;So what does it mean to set the register to 00, 01 and 10 when the:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;SVdd pins are connected to 3.3v (and not 1.8 or 2.5),&lt;/LI&gt;&lt;LI&gt;The Flexbus is configured for non-DDR, and&lt;/LI&gt;&lt;LI&gt;The SDRAM controller is configured for SDR?&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If I change the values in the above registers while monitoring what is actually happening on the data bus I find that "00" does drive with a lower strength than when set for "11", so it is doing SOMETHING, but I don't know what.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The MCF5329 manual doesn't give any more help on this.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The MCF53277 manual (and MCF5208 ones) are 99% cut-and-paste from each other, except that the MCF53277 additionally states:&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;19.6.1&amp;nbsp;&amp;nbsp;&amp;nbsp; SDR SDRAM Initialization Sequence&lt;BR /&gt;&amp;nbsp;&amp;nbsp; 3. Configure the slew rate for the SDRAM external pins in the pin multiplexing&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; and control module’s MSCR_SDRAM register if needed.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;So that one implies that MSCR_SDRAM can be used in SDR mode. But the documentation of that register in that manual is identical to the one in the MCF5329, and doesn't detail what the settings mean for SDR. That manual forgets to mention changing MSCR_FLEXBUS when changing MSCR_SDRAM - that's an accidental omission.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;All manuals have bad cut-and-paste bugs for MSCR_SDRAM too. They all state "SD_CLK mode select control. These bit fields control the strength of the FlexBus lower data pins." which is the description from the PREVIOUS table.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 07 Jun 2010 15:12:14 GMT</pubDate>
    <dc:creator>TomE</dc:creator>
    <dc:date>2010-06-07T15:12:14Z</dc:date>
    <item>
      <title>MCF5329 MSCR_FLEXBUS and MSCR_SDRAM Registers, how do they work in SDR mode?</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5329-MSCR-FLEXBUS-and-MSCR-SDRAM-Registers-how-do-they-work/m-p/205592#M9717</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The MCF5329 can have its pins set up with different drive strengths.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can anyone help me understand what the MSCR_SDRAM and MSCR_FLEXBUS registers "mean" when using 3.3V SDR? The Reference Manual only seems to document DDR mode.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;This is well documented for all pins EXCEPT the Flexbus and SDRAM controller ones.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Typical non-SDRAM/FlexBus pins can be set up as:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;00 10pF&lt;/LI&gt;&lt;LI&gt;01 20pF&lt;/LI&gt;&lt;LI&gt;10 30pF&lt;/LI&gt;&lt;LI&gt;11 50pF&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;The MSCR_FLEXBUS and MSCR_SDRAM pins are documented as:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;00 Half strength 1.8V Mobile DDR.&lt;/LI&gt;&lt;LI&gt;01 Open drain.&lt;/LI&gt;&lt;LI&gt;10 Full strength 1.8V Mobile DDR.&lt;/LI&gt;&lt;LI&gt;11 2.5V DDR1 or 3.3V CMOS with roughly equal rise and fall delays.&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;That implies the only options for 3.3V SDR chips is the last one.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;But I really need 3.3V SDR with a low drive strength like the MCF5235 supported in the programming of its DSCR_EIM register.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;So what does it mean to set the register to 00, 01 and 10 when the:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;SVdd pins are connected to 3.3v (and not 1.8 or 2.5),&lt;/LI&gt;&lt;LI&gt;The Flexbus is configured for non-DDR, and&lt;/LI&gt;&lt;LI&gt;The SDRAM controller is configured for SDR?&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If I change the values in the above registers while monitoring what is actually happening on the data bus I find that "00" does drive with a lower strength than when set for "11", so it is doing SOMETHING, but I don't know what.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The MCF5329 manual doesn't give any more help on this.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The MCF53277 manual (and MCF5208 ones) are 99% cut-and-paste from each other, except that the MCF53277 additionally states:&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;19.6.1&amp;nbsp;&amp;nbsp;&amp;nbsp; SDR SDRAM Initialization Sequence&lt;BR /&gt;&amp;nbsp;&amp;nbsp; 3. Configure the slew rate for the SDRAM external pins in the pin multiplexing&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; and control module’s MSCR_SDRAM register if needed.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;So that one implies that MSCR_SDRAM can be used in SDR mode. But the documentation of that register in that manual is identical to the one in the MCF5329, and doesn't detail what the settings mean for SDR. That manual forgets to mention changing MSCR_FLEXBUS when changing MSCR_SDRAM - that's an accidental omission.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;All manuals have bad cut-and-paste bugs for MSCR_SDRAM too. They all state "SD_CLK mode select control. These bit fields control the strength of the FlexBus lower data pins." which is the description from the PREVIOUS table.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 07 Jun 2010 15:12:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5329-MSCR-FLEXBUS-and-MSCR-SDRAM-Registers-how-do-they-work/m-p/205592#M9717</guid>
      <dc:creator>TomE</dc:creator>
      <dc:date>2010-06-07T15:12:14Z</dc:date>
    </item>
    <item>
      <title>Re: MCF5329 MSCR_FLEXBUS and MSCR_SDRAM Registers, how do they work in SDR mode?</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5329-MSCR-FLEXBUS-and-MSCR-SDRAM-Registers-how-do-they-work/m-p/205593#M9718</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I received the following complete answer within about 3.5 hours of asking our local distributor. That's and excellent response.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Courier New" size="2"&gt;I think there is some confusion info about both MSCR_SDRAM and&lt;BR /&gt;MSCR_FLEXBUS registers, please check below interpretation info:&lt;BR /&gt;With the MSCR fields (MSCR_x) set to 0b11, the data bus and address bus&lt;BR /&gt;will be configured as "2.5V DDR1 or 3.3V CMOS with roughly equal rise&lt;BR /&gt;and fall delays", the pads are capable of driving a 50pF load. (high&lt;BR /&gt;drive strength )&lt;BR /&gt;With the MSCR fields (MSCR_x) set to 0b10, the pads are capable of&lt;BR /&gt;driving a 30pF load.&lt;BR /&gt;With the MSCR fields (MSCR_x) set to 0b01, the pads are capable of&lt;BR /&gt;driving a 20pF load.&lt;BR /&gt;With the MSCR fields (MSCR_x) set to 0b00, the pads are capable of&lt;BR /&gt;driving a 10pF load. (low drive strength)&lt;BR /&gt;We are considering to add this in manual and sorry for the inconvenience&lt;BR /&gt;this may cause to you.&lt;BR /&gt;And you also could get related info from attached MCF5329 IBIS file.&lt;BR /&gt;I abstracted related info below for your reference:&lt;BR /&gt;************************************************************************&lt;BR /&gt;| &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; Model Selector&lt;BR /&gt;|***********************************************************************&lt;BR /&gt;*&lt;BR /&gt;[Model Selector] pad_rfc&lt;BR /&gt;| 1.8V VDDE&lt;BR /&gt;Pad_rfc_00_1p8 &amp;nbsp;10pF load drive&lt;BR /&gt;Pad_rfc_01_1p8 &amp;nbsp;20pF load drive - open drain&lt;BR /&gt;Pad_rfc_10_1p8 &amp;nbsp;30pF load drive&lt;BR /&gt;Pad_rfc_11_1p8 &amp;nbsp;50pF load drive&lt;BR /&gt;Pad_rfc_in_1p8 &amp;nbsp;Input Buffer&lt;BR /&gt;| 2.5V VDDE&lt;BR /&gt;Pad_rfc_00_2p5 &amp;nbsp;10pF load drive&lt;BR /&gt;Pad_rfc_01_2p5 &amp;nbsp;20pF load drive - open drain&lt;BR /&gt;Pad_rfc_10_2p5 &amp;nbsp;30pF load drive&lt;BR /&gt;Pad_rfc_11_2p5 &amp;nbsp;50pF load drive&lt;BR /&gt;Pad_rfc_in_2p5 &amp;nbsp;Input Buffer&lt;BR /&gt;| 3.3V VDDE&lt;BR /&gt;Pad_rfc_00_3p3 &amp;nbsp;10pF load drive&lt;BR /&gt;Pad_rfc_01_3p3 &amp;nbsp;20pF load drive - open drain&lt;BR /&gt;Pad_rfc_10_3p3 &amp;nbsp;30pF load drive&lt;BR /&gt;Pad_rfc_11_3p3 &amp;nbsp;50pF load drive&lt;BR /&gt;Pad_rfc_in_3p3 &amp;nbsp;Input Buffer&lt;BR /&gt;************************************************************************&lt;/FONT&gt;&lt;FONT face="sans-serif" size="2"&gt;&lt;BR /&gt;&lt;/FONT&gt;&lt;FONT color="red" face="sans-serif" size="2"&gt;Q1 -&lt;/FONT&gt; &lt;FONT color="red" face="Courier New" size="2"&gt;What does it mean to run the ports in "Half strength 1.8V low power/mobile DDR" mode with 3.3V SDRAM?&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="blue" face="sans-serif" size="2"&gt;A1 -&lt;/FONT&gt; &lt;FONT color="blue" face="Courier New" size="2"&gt;"Half strength 1.8V low power/mobile DDR" mode with 3.3V SDRAM means low drive strength.&lt;/FONT&gt;&lt;FONT face="sans-serif" size="2"&gt;&lt;BR /&gt;&lt;/FONT&gt;&lt;FONT color="red" face="sans-serif" size="2"&gt;Q2 -&lt;/FONT&gt; &lt;FONT color="red" face="Courier New" size="2"&gt;What are the actual drive parameters with this setting?&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="blue" face="sans-serif" size="2"&gt;A2 -&lt;/FONT&gt; &lt;FONT color="blue" face="Courier New" size="2"&gt;Low drive strength is 10pF.&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="red" face="sans-serif" size="2"&gt;Q3 -&lt;/FONT&gt; &lt;FONT color="red" face="Courier New" size="2"&gt;Is it reliable? Can it be recommended?&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="blue" face="sans-serif" size="2"&gt;A3 -&lt;/FONT&gt; &lt;FONT color="blue" face="Courier New" size="2"&gt;It is reliable.&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="red" face="sans-serif" size="2"&gt;Q4 -&lt;/FONT&gt; &lt;FONT color="red" face="Courier New" size="2"&gt;Are there other side-effects of this setting?&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="blue" face="sans-serif" size="2"&gt;A4 -&lt;/FONT&gt; &lt;FONT color="blue" face="Courier New" size="2"&gt;No side-effects.&lt;/FONT&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Jun 2010 13:35:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5329-MSCR-FLEXBUS-and-MSCR-SDRAM-Registers-how-do-they-work/m-p/205593#M9718</guid>
      <dc:creator>TomE</dc:creator>
      <dc:date>2010-06-08T13:35:59Z</dc:date>
    </item>
    <item>
      <title>Re: MCF5329 MSCR_FLEXBUS and MSCR_SDRAM Registers, how do they work in SDR mode?</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5329-MSCR-FLEXBUS-and-MSCR-SDRAM-Registers-how-do-they-work/m-p/205594#M9719</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;FONT face="terminal,monaco"&gt;The previous answers from Freescale fixed the SDRAM controller problem, but showed that the Data Sheets don't give any information about the differences between the different modes.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;From the Data Sheet I know we're not exceeding the Drive Capability of the pins when in "High Strength". But we don't have any pins set that way, and the chip defaults to "Second out of Four Strength" out of reset.. We're using "00", "01", and "02" Strengths.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;FONT face="terminal,monaco"&gt;Further questions&lt;/FONT&gt; on "what are the votage and current characteristics" resulted in a simple reply:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Read the IBIS file in the chip page downloadable from Freescale.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This is a data file meant to be read by circuit simulation programs. There are 10,700 lines in it.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;It is possible to get some useful information out of this, but it literally takes HOURS.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Here's a few samples:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Below abstrct info from MCF5329 IBIS shows different "Drive Strength" with different current:&lt;BR /&gt;[Model]&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Pad_rfc_00_2p5 (Drive strength 10pF)&lt;BR /&gt;2.5000&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 25.7801mA&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 15.6642mA&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 36.5627mA&lt;BR /&gt;[Model]&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Pad_rfc_01_2p5 (Drive strength 20pF)&lt;BR /&gt;2.5000&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 37.8790mA&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 23.0194mA&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 53.7138mA&lt;BR /&gt;[Model]&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Pad_rfc_10_2p5 (Drive strength 30pF)&lt;BR /&gt;2.5000&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 56.8199mA&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 34.5260mA&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 80.5814mA&lt;BR /&gt;[Model]&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Pad_rfc_11_2p5 (Drive strength 50pF)&lt;BR /&gt;2.5000&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 94.6989mA&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 57.5453mA&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.1343A&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Normal pins&amp;nbsp; at 3.3V and "01": pad_fc_33_01:&lt;BR /&gt;&amp;nbsp; [Pulldown]&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.4000&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 18.5441mA&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 11.9133mA&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 24.9340mA&lt;BR /&gt;&amp;nbsp; [Pullup]&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.4000&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; -35.3770mA&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; -24.9372mA&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; -46.6793mA&lt;BR /&gt;&lt;BR /&gt;FLEXBUS pins at 3.3V and "00": Pad_rfc_00_3p3:&lt;BR /&gt;&amp;nbsp; [Pulldown]&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.4000&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 9.1752mA&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 5.8891mA&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 12.3481mA&lt;BR /&gt;&amp;nbsp; [Pullup]&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.4000&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; -25.5635mA&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; -17.8931mA&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; -34.0260mA&lt;BR /&gt;&lt;BR /&gt;SDRAM&amp;nbsp; pins&amp;nbsp; at 3.3V and "10": Pad_rfc_10_3p3:&lt;BR /&gt;&amp;nbsp; [Pulldown]&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.4000&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 20.2232mA&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 12.9807mA&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 27.2159mA&lt;BR /&gt;&amp;nbsp; [Pullup]&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.4000&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; -56.3310mA&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; -39.4290mA&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; -74.9783mA&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;SDRAM&amp;nbsp; pins&amp;nbsp; at 3.3V and "11": Pad_rfc_11_3p3:&lt;BR /&gt;&amp;nbsp; [Pulldown]&lt;BR /&gt;&amp;nbsp;&amp;nbsp; 0.1000&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 9.2473mA&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 5.9932mA&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 12.3534mA&lt;BR /&gt;&amp;nbsp;&amp;nbsp; 0.2000&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 17.9396mA&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 11.5904mA&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 24.0214mA&lt;BR /&gt;&amp;nbsp;&amp;nbsp; 0.3000&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 26.0886mA&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 16.8013mA&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 35.0186mA&lt;BR /&gt;&lt;BR /&gt;&amp;nbsp; [Pullup]&lt;BR /&gt;&amp;nbsp;&amp;nbsp; 0.1000&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; -15.6049mA&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; -10.9504mA&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; -20.6701mA&lt;BR /&gt;&amp;nbsp;&amp;nbsp; 0.2000&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; -30.1791mA&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; -21.1629mA&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; -40.0335mA&lt;BR /&gt;&amp;nbsp;&amp;nbsp; 0.3000&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; -43.7467mA&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; -30.6512mA&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; -58.1251mA&lt;BR /&gt;&lt;BR /&gt;&amp;nbsp; [Ramp]&lt;BR /&gt;&amp;nbsp; | variable&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; typ&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; min&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; max&lt;BR /&gt;&amp;nbsp; dV/dt_r&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 1.7328/0.1503n&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 1.4845/0.2742n&amp;nbsp;&amp;nbsp; 1.9554/0.1002n&lt;BR /&gt;&amp;nbsp; dV/dt_f&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 1.5712/0.1272n&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 1.2412/0.2223n&amp;nbsp;&amp;nbsp; 1.8228/88.2325p&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Jun 2010 14:31:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5329-MSCR-FLEXBUS-and-MSCR-SDRAM-Registers-how-do-they-work/m-p/205594#M9719</guid>
      <dc:creator>TomE</dc:creator>
      <dc:date>2010-06-16T14:31:05Z</dc:date>
    </item>
    <item>
      <title>Re: MCF5329 MSCR_FLEXBUS and MSCR_SDRAM Registers, how do they work in SDR mode?</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5329-MSCR-FLEXBUS-and-MSCR-SDRAM-Registers-how-do-they-work/m-p/205595#M9720</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;There doesn't seem to be any way to change the Drive Strength of the Byte Write lines.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;There is a Flexbus drive-strength register that looks like it should change the strength of these,&lt;/P&gt;&lt;P&gt;but it doesn't seem to work when the signals are in SDRAM mode.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Jul 2010 14:49:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5329-MSCR-FLEXBUS-and-MSCR-SDRAM-Registers-how-do-they-work/m-p/205595#M9720</guid>
      <dc:creator>TomE</dc:creator>
      <dc:date>2010-07-06T14:49:57Z</dc:date>
    </item>
  </channel>
</rss>