<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>ColdFire/68K Microcontrollers and Processors中的主题 MCF 5483 Slice Timers: problem with interrupts</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF-5483-Slice-Timers-problem-with-interrupts/m-p/131689#M965</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;I am working with Coldfire 5483 and I want to use both SLT0 and SLT1 slice timers.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- SLT0 is used for generating 10ms tick for my SMX RTOS&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- SLT1 is used for generating a 1ms time pulse&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Both are configured in order to generate an interrupt.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;My problem is that I only get interrupt for the timer with the highest priority.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Is anyone can explain me how to configure these 2 timers and which interrupt level and priority to choose?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 28 Sep 2006 18:03:29 GMT</pubDate>
    <dc:creator>luc</dc:creator>
    <dc:date>2006-09-28T18:03:29Z</dc:date>
    <item>
      <title>MCF 5483 Slice Timers: problem with interrupts</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF-5483-Slice-Timers-problem-with-interrupts/m-p/131689#M965</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;I am working with Coldfire 5483 and I want to use both SLT0 and SLT1 slice timers.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- SLT0 is used for generating 10ms tick for my SMX RTOS&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- SLT1 is used for generating a 1ms time pulse&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Both are configured in order to generate an interrupt.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;My problem is that I only get interrupt for the timer with the highest priority.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Is anyone can explain me how to configure these 2 timers and which interrupt level and priority to choose?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Sep 2006 18:03:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF-5483-Slice-Timers-problem-with-interrupts/m-p/131689#M965</guid>
      <dc:creator>luc</dc:creator>
      <dc:date>2006-09-28T18:03:29Z</dc:date>
    </item>
    <item>
      <title>Re: MCF 5483 Slice Timers: problem with interrupts</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF-5483-Slice-Timers-problem-with-interrupts/m-p/131690#M966</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;I think I found the cause of my problem. I was clearing interrupt of SLT1 by writing 1 to the status bit of SLT0 !!!&lt;BR /&gt;Sorry for this post &lt;IMG alt=":smileyhappy:" class="emoticon emoticon-smileyhappy" id="smileyhappy" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-happy.gif" title="Smiley Happy" /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Sep 2006 20:52:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF-5483-Slice-Timers-problem-with-interrupts/m-p/131690#M966</guid>
      <dc:creator>luc</dc:creator>
      <dc:date>2006-09-28T20:52:51Z</dc:date>
    </item>
  </channel>
</rss>