<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>ColdFire/68K Microcontrollers and ProcessorsのトピックRe: Setting up the Real Time Clock in the Coldfilre MCF52223 micro</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Setting-up-the-Real-Time-Clock-in-the-Coldfilre-MCF52223-micro/m-p/201634#M9312</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi Jim&lt;BR /&gt;&lt;BR /&gt;I believe that the oscillator input is valid.&lt;BR /&gt;&lt;BR /&gt;The M52223 is generally clocked from 48MHz (due to USB) so&lt;BR /&gt;MCF_CLOCK_RTCDR = (48000000-1); seems to be the exact value required.&lt;BR /&gt;&lt;BR /&gt;Regards&lt;BR /&gt;&lt;BR /&gt;Mark&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 12 Mar 2008 04:12:22 GMT</pubDate>
    <dc:creator>mjbcswitzerland</dc:creator>
    <dc:date>2008-03-12T04:12:22Z</dc:date>
    <item>
      <title>Setting up the Real Time Clock in the Coldfilre MCF52223 micro</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Setting-up-the-Real-Time-Clock-in-the-Coldfilre-MCF52223-micro/m-p/201631#M9309</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;SPAN&gt;Is there any&amp;nbsp; code example on setting up the Real Time Clock&amp;nbsp; in the MCF52223. And to be able to read and write to it.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks,&lt;/SPAN&gt;&lt;BR /&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Mar 2008 22:14:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Setting-up-the-Real-Time-Clock-in-the-Coldfilre-MCF52223-micro/m-p/201631#M9309</guid>
      <dc:creator>JimMcP</dc:creator>
      <dc:date>2008-03-10T22:14:12Z</dc:date>
    </item>
    <item>
      <title>Re: Setting up the Real Time Clock in the Coldfilre MCF52223 micro</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Setting-up-the-Real-Time-Clock-in-the-Coldfilre-MCF52223-micro/m-p/201632#M9310</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi Jim&lt;BR /&gt;&lt;BR /&gt;Take a look at the following link which discusses the RTC in the M5223X (I belive it is identical to the RTC in the M52223).&lt;BR /&gt;&lt;BR /&gt;&lt;A href="http://www.utasker.com/forum/index.php?topic=35.0" rel="nofollow" target="_blank"&gt;http://www.utasker.com/forum/index.php?topic=35.0&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;The RTC is fully supported in the uTasker project and also simulated in the uTasker simulator.&lt;BR /&gt;Complete code and a demo is available in the latest service pack - the project also supports the M52223.&lt;BR /&gt;&lt;BR /&gt;Regards&lt;BR /&gt;&lt;BR /&gt;Mark&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Mar 2008 00:58:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Setting-up-the-Real-Time-Clock-in-the-Coldfilre-MCF52223-micro/m-p/201632#M9310</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2008-03-11T00:58:40Z</dc:date>
    </item>
    <item>
      <title>Re: Setting up the Real Time Clock in the Coldfilre MCF52223 micro</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Setting-up-the-Real-Time-Clock-in-the-Coldfilre-MCF52223-micro/m-p/201633#M9311</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;The real time clock frequency setting fot the MCF52223 is it&lt;BR /&gt;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; MCF_CLOCK_RTCDR = 48000000;&lt;BR /&gt;&lt;BR /&gt;OR&lt;BR /&gt;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; MCF_CLOCK_RTCDR = 25000000;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Mar 2008 01:45:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Setting-up-the-Real-Time-Clock-in-the-Coldfilre-MCF52223-micro/m-p/201633#M9311</guid>
      <dc:creator>JimMcP</dc:creator>
      <dc:date>2008-03-12T01:45:36Z</dc:date>
    </item>
    <item>
      <title>Re: Setting up the Real Time Clock in the Coldfilre MCF52223 micro</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Setting-up-the-Real-Time-Clock-in-the-Coldfilre-MCF52223-micro/m-p/201634#M9312</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi Jim&lt;BR /&gt;&lt;BR /&gt;I believe that the oscillator input is valid.&lt;BR /&gt;&lt;BR /&gt;The M52223 is generally clocked from 48MHz (due to USB) so&lt;BR /&gt;MCF_CLOCK_RTCDR = (48000000-1); seems to be the exact value required.&lt;BR /&gt;&lt;BR /&gt;Regards&lt;BR /&gt;&lt;BR /&gt;Mark&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Mar 2008 04:12:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Setting-up-the-Real-Time-Clock-in-the-Coldfilre-MCF52223-micro/m-p/201634#M9312</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2008-03-12T04:12:22Z</dc:date>
    </item>
  </channel>
</rss>