<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MCF51AC256B and MC13201 using SMAC and/or BeeKit in ColdFire/68K Microcontrollers and Processors</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF51AC256B-and-MC13201-using-SMAC-and-or-BeeKit/m-p/201109#M9276</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I feel like this is my own personal blog, this thread is so quiet&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Anyway the good news, I've condensed the SMAC into two files, radio.h and radio.c for the '51AC256B and I am getting closer to a successful compile. Started out with 500 errors and down to only a few dozen now. Do you realize that the transceiver driver files are spread throughout 7 header and source files!!&amp;nbsp; Easy to compress this kind of stuff into one or two files!!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;When I get done, I'll post the code here in-line, so that anyone can use it.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I wish Freescale would provide simple example code for stuff like this!! (hint-like Microchip and others do).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Tim&lt;/P&gt;&lt;P&gt;(Motorola/Freescale user for 20 years)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 25 May 2010 00:58:58 GMT</pubDate>
    <dc:creator>offgrid</dc:creator>
    <dc:date>2010-05-25T00:58:58Z</dc:date>
    <item>
      <title>MCF51AC256B and MC13201 using SMAC and/or BeeKit</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF51AC256B-and-MC13201-using-SMAC-and-or-BeeKit/m-p/201106#M9273</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is there an easy way to run SMAC on the 'AC256 and get it up and running quickly?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am trying to use Beekit, and it only compiles projects for the intended development boards, which I have not acquired, and don't intend to. After having Beekit "Compile and open project" in CW 6.3, it will not allow an "Change MCU/connection" to occur to my target processor.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;So two questions:&lt;/P&gt;&lt;P&gt;1. Is it possible to allow CW to Change MCU to AC256?&lt;/P&gt;&lt;P&gt;2. OR, can I just import a SMAC into my current project, and if so what files are needed?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Many thanks!&lt;/P&gt;&lt;P&gt;Tim&lt;/P&gt;&lt;P&gt;Offgrid Engineering LLC&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 May 2010 03:36:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF51AC256B-and-MC13201-using-SMAC-and-or-BeeKit/m-p/201106#M9273</guid>
      <dc:creator>offgrid</dc:creator>
      <dc:date>2010-05-18T03:36:10Z</dc:date>
    </item>
    <item>
      <title>Re: MCF51AC256B and MC13201 using SMAC and/or BeeKit</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF51AC256B-and-MC13201-using-SMAC-and-or-BeeKit/m-p/201107#M9274</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;STRONG&gt;&lt;EM&gt;I'll reframe the question:&lt;/EM&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;STRONG&gt;Does anyone have a very basic SMAC radio running for Coldfire V1 chip and the MC1319X/1320X transceivers, that they would be willing to share?&lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Or a close relative of that Flexis chip, or ??? Any of the BeeKit projects would work, simple CW, Send and Receive, light some leds, etc.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;My preference would be for all the SMAC radio files to be condensed into 1 or 2 files, since my main motor application is already 32 files (yes the CW free limit)!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for looking!&lt;/P&gt;&lt;P&gt;Tim&lt;/P&gt;&lt;P&gt;&lt;IMG alt=":robothappy:" class="emoticon emoticon-robothappy" id="robothappy" src="http://freescale.i.lithium.com/i/smilies/16x16_robot-happy.gif" title="Robot Happy" /&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 May 2010 00:15:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF51AC256B-and-MC13201-using-SMAC-and-or-BeeKit/m-p/201107#M9274</guid>
      <dc:creator>offgrid</dc:creator>
      <dc:date>2010-05-19T00:15:17Z</dc:date>
    </item>
    <item>
      <title>Re: MCF51AC256B and MC13201 using SMAC and/or BeeKit</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF51AC256B-and-MC13201-using-SMAC-and-or-BeeKit/m-p/201108#M9275</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Here is another idea...&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&lt;BR /&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Has anyone condensed the SMAC code stack into a just a few (1-4) files?&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;For any Freescale processor and for any Freescale tranceiver?&lt;/P&gt;&lt;P&gt;Would they also like to share, even possibly an upload to this forum (if anyone else is interested?)???&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I would think Freescale would want to provide a simple solution for those of us wanting to add SMAC radios to our existing applications. Possible marketing idea??&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Cheers!&lt;/P&gt;&lt;P&gt;Tim&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 May 2010 03:09:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF51AC256B-and-MC13201-using-SMAC-and-or-BeeKit/m-p/201108#M9275</guid>
      <dc:creator>offgrid</dc:creator>
      <dc:date>2010-05-20T03:09:34Z</dc:date>
    </item>
    <item>
      <title>Re: MCF51AC256B and MC13201 using SMAC and/or BeeKit</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF51AC256B-and-MC13201-using-SMAC-and-or-BeeKit/m-p/201109#M9276</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I feel like this is my own personal blog, this thread is so quiet&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Anyway the good news, I've condensed the SMAC into two files, radio.h and radio.c for the '51AC256B and I am getting closer to a successful compile. Started out with 500 errors and down to only a few dozen now. Do you realize that the transceiver driver files are spread throughout 7 header and source files!!&amp;nbsp; Easy to compress this kind of stuff into one or two files!!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;When I get done, I'll post the code here in-line, so that anyone can use it.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I wish Freescale would provide simple example code for stuff like this!! (hint-like Microchip and others do).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Tim&lt;/P&gt;&lt;P&gt;(Motorola/Freescale user for 20 years)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 25 May 2010 00:58:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF51AC256B-and-MC13201-using-SMAC-and-or-BeeKit/m-p/201109#M9276</guid>
      <dc:creator>offgrid</dc:creator>
      <dc:date>2010-05-25T00:58:58Z</dc:date>
    </item>
  </channel>
</rss>