<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>ColdFire/68K Microcontrollers and Processors中的主题 Re: USB on the GO hardware</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/USB-on-the-GO-hardware/m-p/200432#M9153</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Welcome to the forum, Pavelek&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm also considering using OTG feature of MCF51JM or maybe MCF5225x. I'm also going to use standard size B&amp;nbsp;connector for PC connection and standard A connector to connect flash drive. I'm not very familiar with USB, because I have used only FTDI chips.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Yes, PC and flash drive shouldn't be inserted simultaneously. My board won't be powered&amp;nbsp;from USB. I'm going to detect if&amp;nbsp;5V power from PC is present, and if present, then power&amp;nbsp;from type A socket (flash drive) will be immediately removed. I don't&amp;nbsp;expect very much that unpowered flash drive won't disturb PC connection, but at least nothing will smoke.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;ADM869L is high side switch, which switches power&amp;nbsp;to&amp;nbsp;flash drive.&amp;nbsp;You can use any other chip for this, or maybe even simple FET solution. MAX3353 is more useful for 3V powered designs. Flash drive should be powered from 5V and&amp;nbsp;MAX3353 allows to&amp;nbsp;step up voltage&amp;nbsp;to 5V. Second function of MAX3353 is on/off control of device mode pull-up resistor and on/off control of host mode pull-down resistors. Host mode pull-down 15kOhm resistos can be controlled directly from JM I/O pins. You need to wire one 15K end to USBD? pin, another end to JM I/O pin. To disable 15kOhm pull-down&amp;nbsp;set up I/O pin direction to input. To enable 15k&amp;nbsp;pull-down&amp;nbsp;set direction to output and set output pin low. &amp;nbsp;Device mode pull up resistor can be controlled in the similar way if JM is powered from 5V. Or, I think it can be controlled automatically from 5V power from B connector. PC not connected - USB pin not pulled up.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 17 May 2010 12:59:27 GMT</pubDate>
    <dc:creator>kef</dc:creator>
    <dc:date>2010-05-17T12:59:27Z</dc:date>
    <item>
      <title>USB on the GO hardware</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/USB-on-the-GO-hardware/m-p/200431#M9152</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi my name is Israel Pavelek I´m from Argentina and I´m developing a product that need a conection to a pc and to a pendrive they don´t have to be&amp;nbsp;simultaneous, I was first of all thinking in the MCF51JM128 because the aplication do not need a more than a couple of pins for conectt a graphical 128*64 LCD and a serial conection from a other microcontroller that give the information to the LCD, I would like to have both conectors the B for the PC and A for the pendrive to download a couple of data, If there any problem if someone plug the pendrive in the A conecctor and the pc in B coneector at the same time? the other problem is how to connect them, I saw that the USB hardware connections use two chips&amp;nbsp;adm869L&amp;nbsp;and max3353 are they totaly necesary? what are the purpose of them? because a can´t find them in Argentina, besides i´m thinking first of all to develop with a DEMOJM kit.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;A distributor in Argentina offer me the MCF52259 demo kit also, i´m not now working with ethernet.. the USB part it´s the same? I´m talking about the software and hardware.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Thanks&lt;BR /&gt;Israel Pavelek&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 15 May 2010 12:48:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/USB-on-the-GO-hardware/m-p/200431#M9152</guid>
      <dc:creator>ipavelek</dc:creator>
      <dc:date>2010-05-15T12:48:06Z</dc:date>
    </item>
    <item>
      <title>Re: USB on the GO hardware</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/USB-on-the-GO-hardware/m-p/200432#M9153</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Welcome to the forum, Pavelek&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm also considering using OTG feature of MCF51JM or maybe MCF5225x. I'm also going to use standard size B&amp;nbsp;connector for PC connection and standard A connector to connect flash drive. I'm not very familiar with USB, because I have used only FTDI chips.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Yes, PC and flash drive shouldn't be inserted simultaneously. My board won't be powered&amp;nbsp;from USB. I'm going to detect if&amp;nbsp;5V power from PC is present, and if present, then power&amp;nbsp;from type A socket (flash drive) will be immediately removed. I don't&amp;nbsp;expect very much that unpowered flash drive won't disturb PC connection, but at least nothing will smoke.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;ADM869L is high side switch, which switches power&amp;nbsp;to&amp;nbsp;flash drive.&amp;nbsp;You can use any other chip for this, or maybe even simple FET solution. MAX3353 is more useful for 3V powered designs. Flash drive should be powered from 5V and&amp;nbsp;MAX3353 allows to&amp;nbsp;step up voltage&amp;nbsp;to 5V. Second function of MAX3353 is on/off control of device mode pull-up resistor and on/off control of host mode pull-down resistors. Host mode pull-down 15kOhm resistos can be controlled directly from JM I/O pins. You need to wire one 15K end to USBD? pin, another end to JM I/O pin. To disable 15kOhm pull-down&amp;nbsp;set up I/O pin direction to input. To enable 15k&amp;nbsp;pull-down&amp;nbsp;set direction to output and set output pin low. &amp;nbsp;Device mode pull up resistor can be controlled in the similar way if JM is powered from 5V. Or, I think it can be controlled automatically from 5V power from B connector. PC not connected - USB pin not pulled up.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 May 2010 12:59:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/USB-on-the-GO-hardware/m-p/200432#M9153</guid>
      <dc:creator>kef</dc:creator>
      <dc:date>2010-05-17T12:59:27Z</dc:date>
    </item>
    <item>
      <title>USB on the GO, Being Host And Device</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/USB-on-the-GO-hardware/m-p/200433#M9154</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi. my name is Israel Pavelek from Argentina, I would like to have in my proyect the capability of plug a pendrive or plug to the computer, without changing any jumper, so it would be transparent for the user. Let see if I can explain it better. My proyect has an LCD display if the user conects in the A USB port a pendrive, he can be capable of download the image to the pendrive, but if he plug into the mini A-B to the computer connector he would be able to download the image to the computer directily, without changing any jumper, It´s that posible,How can a change from Device to Host, how can i detect these situations? when someone plug a Pendrive or a Mini to pc cable. ? And the critial how to prevent that the user plugs both de pendrive &amp;nbsp;into the A port and the pc into de MIni a-b port?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Israel Pavelek&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 24 Jun 2010 02:36:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/USB-on-the-GO-hardware/m-p/200433#M9154</guid>
      <dc:creator>ipavelek</dc:creator>
      <dc:date>2010-06-24T02:36:00Z</dc:date>
    </item>
  </channel>
</rss>