<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MCF5307 and 16bit flash in ColdFire/68K Microcontrollers and Processors</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5307-and-16bit-flash/m-p/199503#M9078</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello all,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;i am booting colilo from a a 16 bit flash. Code is run correctly, but texts are printed out from the serial uncorrectly, due to the 16-bit word addressing mode:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hello world is printed as HHeelloo&amp;nbsp; .. &amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This becouse char* increment don't point to the next byte but to the same word.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Every help is really appreciated.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;spectrum&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jul 2009 21:11:47 GMT</pubDate>
    <dc:creator>angelo_d</dc:creator>
    <dc:date>2009-07-15T21:11:47Z</dc:date>
    <item>
      <title>MCF5307 and 16bit flash</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5307-and-16bit-flash/m-p/199503#M9078</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello all,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;i am booting colilo from a a 16 bit flash. Code is run correctly, but texts are printed out from the serial uncorrectly, due to the 16-bit word addressing mode:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hello world is printed as HHeelloo&amp;nbsp; .. &amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This becouse char* increment don't point to the next byte but to the same word.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Every help is really appreciated.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;spectrum&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jul 2009 21:11:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5307-and-16bit-flash/m-p/199503#M9078</guid>
      <dc:creator>angelo_d</dc:creator>
      <dc:date>2009-07-15T21:11:47Z</dc:date>
    </item>
    <item>
      <title>Re: MCF5307 and 16bit flash</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5307-and-16bit-flash/m-p/199504#M9079</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello all,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;mm, i finally clarified the mistery: it is related to the flash 2Mx16 SST 29VF3201B i have chosed.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Unfortunately, even if the pinout is exactly as a correspondent size AMD x16 flash, i discovered that SST flash don't suport the x8 mode, or better, don't have the BYTE# signal on pin 47, but it is a NC.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I choosed SST for good pricing, and would avoid to replace it, so i am going to try to modify the colilo bootloader to copy rodata to rom.&lt;/P&gt;&lt;P&gt;Anyway this is just a beginner erro i guess &lt;IMG alt=":smileyhappy:" class="emoticon emoticon-smileyhappy" id="smileyhappy" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-happy.gif" title="Smiley Happy" /&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hope this can help soem other,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;greetings,&lt;/P&gt;&lt;P&gt;angelo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jul 2009 18:59:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5307-and-16bit-flash/m-p/199504#M9079</guid>
      <dc:creator>angelo_d</dc:creator>
      <dc:date>2009-07-16T18:59:37Z</dc:date>
    </item>
  </channel>
</rss>