<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MCF5475CFE PCI Controller in ColdFire/68K Microcontrollers and Processors</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5475CFE-PCI-Controller/m-p/199382#M9066</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;DIV class="postbody"&gt;For a breadboard we are designing, we are using 2 Fire Engine modules mounted on a host board. The final design will be using the PCI bus for communication between Coldfire processors. I would like to connect both Fire Engine MCF5475s to the same PCI bus on the host board, but have encountered two issues.&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/DIV&gt;&lt;DIV class="postbody"&gt;1.&amp;nbsp; The PCI clock for the FE is supplied by the clock on board.&amp;nbsp;&amp;nbsp; I don't see a way to provide an outside clock source, so cannot put both processors on the same PCI clock source.&lt;/DIV&gt;&lt;DIV class="postbody"&gt;2.&amp;nbsp; The PCI_IDSEL line is hardwired to PCI_AD16.&amp;nbsp;&amp;nbsp; (This is used for Type 0 Configuration).&amp;nbsp; I think that this can be overcome by software though, which would be okay for breadboard purposes.&lt;/DIV&gt;&lt;DIV class="postbody"&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV class="postbody"&gt;Any suggestions on how to get around the clock issue?&lt;/DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 05 Nov 2008 01:12:38 GMT</pubDate>
    <dc:creator>mniuser</dc:creator>
    <dc:date>2008-11-05T01:12:38Z</dc:date>
    <item>
      <title>MCF5475CFE PCI Controller</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5475CFE-PCI-Controller/m-p/199382#M9066</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;DIV class="postbody"&gt;For a breadboard we are designing, we are using 2 Fire Engine modules mounted on a host board. The final design will be using the PCI bus for communication between Coldfire processors. I would like to connect both Fire Engine MCF5475s to the same PCI bus on the host board, but have encountered two issues.&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/DIV&gt;&lt;DIV class="postbody"&gt;1.&amp;nbsp; The PCI clock for the FE is supplied by the clock on board.&amp;nbsp;&amp;nbsp; I don't see a way to provide an outside clock source, so cannot put both processors on the same PCI clock source.&lt;/DIV&gt;&lt;DIV class="postbody"&gt;2.&amp;nbsp; The PCI_IDSEL line is hardwired to PCI_AD16.&amp;nbsp;&amp;nbsp; (This is used for Type 0 Configuration).&amp;nbsp; I think that this can be overcome by software though, which would be okay for breadboard purposes.&lt;/DIV&gt;&lt;DIV class="postbody"&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV class="postbody"&gt;Any suggestions on how to get around the clock issue?&lt;/DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Nov 2008 01:12:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5475CFE-PCI-Controller/m-p/199382#M9066</guid>
      <dc:creator>mniuser</dc:creator>
      <dc:date>2008-11-05T01:12:38Z</dc:date>
    </item>
    <item>
      <title>Re: MCF5475CFE PCI Controller</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5475CFE-PCI-Controller/m-p/199383#M9067</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;My comment isn't specifically related to you're question, but since you are using PCI on the fireengines please read the release note (the section on PCI) in the latest BSP.&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Nov 2008 01:36:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5475CFE-PCI-Controller/m-p/199383#M9067</guid>
      <dc:creator>kmahan</dc:creator>
      <dc:date>2008-11-05T01:36:18Z</dc:date>
    </item>
  </channel>
</rss>