<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>ColdFire/68K Microcontrollers and Processors中的主题 Re: MCF52259 Dueling Table Data</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF52259-Dueling-Table-Data/m-p/198741#M9004</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mark --&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Yes, I read that thread, but it only talks about the RAM.&amp;nbsp;&amp;nbsp; MacL says the RTC is backed up at 1.8V, but I need it to run.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have a '59&amp;nbsp;demo board, and a 1.8V - 3.0V variable&amp;nbsp;power supply, guess I'll have to write some code to start the RTC, and find out what happens.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;By the way, how did you measure 3.9uA?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Gary&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jul 2009 09:57:41 GMT</pubDate>
    <dc:creator>GaryOlmstead</dc:creator>
    <dc:date>2009-07-15T09:57:41Z</dc:date>
    <item>
      <title>MCF52259 Dueling Table Data</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF52259-Dueling-Table-Data/m-p/198739#M9002</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi --&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The MCF52259 Data Sheet says (Table 2.1, page 23) that the RAM standby supply voltage (Vstby) must be 1.8V to 3.5V.&amp;nbsp; While Table 2.6 (pg 28( says that Standby voltage Vstby must be 3.0V to 3.5V.&amp;nbsp; I assume this means that 1.8V is OK if you aren't running, but not if you are.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;My interest is not in the RAM, but the RTC, which is also fed from Vstby.&amp;nbsp; Does it work at &amp;lt; 3.0V?&amp;nbsp; The Data Sheet doesn't mention the RTC.&amp;nbsp; The '59 Reference Manual has a whole chapter on the RTC, but doesn't say how it gets its power.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;So, can the RTC keep time at less than 3.0V?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 13 Jul 2009 23:12:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF52259-Dueling-Table-Data/m-p/198739#M9002</guid>
      <dc:creator>GaryOlmstead</dc:creator>
      <dc:date>2009-07-13T23:12:27Z</dc:date>
    </item>
    <item>
      <title>Re: MCF52259 Dueling Table Data</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF52259-Dueling-Table-Data/m-p/198740#M9003</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Gary&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;You should find that this has been discussed in detail here:&lt;/P&gt;&lt;P&gt;&lt;A href="http://forums.freescale.com/freescale/board/message?board.id=CFCOMM&amp;amp;message.id=6407&amp;amp;query.id=118275#M6407" target="_self"&gt;http://forums.freescale.com/freescale/board/message?board.id=CFCOMM&amp;amp;message.id=6407&amp;amp;query.id=118275#M6407&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jul 2009 03:41:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF52259-Dueling-Table-Data/m-p/198740#M9003</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2009-07-15T03:41:52Z</dc:date>
    </item>
    <item>
      <title>Re: MCF52259 Dueling Table Data</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF52259-Dueling-Table-Data/m-p/198741#M9004</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mark --&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Yes, I read that thread, but it only talks about the RAM.&amp;nbsp;&amp;nbsp; MacL says the RTC is backed up at 1.8V, but I need it to run.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have a '59&amp;nbsp;demo board, and a 1.8V - 3.0V variable&amp;nbsp;power supply, guess I'll have to write some code to start the RTC, and find out what happens.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;By the way, how did you measure 3.9uA?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Gary&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jul 2009 09:57:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF52259-Dueling-Table-Data/m-p/198741#M9004</guid>
      <dc:creator>GaryOlmstead</dc:creator>
      <dc:date>2009-07-15T09:57:41Z</dc:date>
    </item>
    <item>
      <title>Re: MCF52259 Dueling Table Data</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF52259-Dueling-Table-Data/m-p/198742#M9005</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Gary&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The tests were with running RTC, which worked down to about 2.0V. Somewhere under 2.0V the oscillator would stop - so the 1.8V limit may be correct but it was difficult to get to this point using a voltage generator (possibly due to small voltage jumps when adjusting the level, which won't happen with a battery being drained to this level).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I measured the Vstby current with a uA meter - no official calibration so tolerance not known. These are therefore ball-park figures and if you need high accuracy it will be necessary to use calibrated equipment in a suitable test environment.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jul 2009 17:29:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF52259-Dueling-Table-Data/m-p/198742#M9005</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2009-07-15T17:29:14Z</dc:date>
    </item>
    <item>
      <title>Re: MCF52259 Dueling Table Data</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF52259-Dueling-Table-Data/m-p/198743#M9006</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mark --&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;OK, I missed the part about the RTC running.&amp;nbsp; Thanks for the clarification.&amp;nbsp; That's really good to know.&amp;nbsp; Although two batteries in series would not have been the end of the world.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;A uA meter... of course, how stupid of me.&amp;nbsp; I may have to invest in one of those.&amp;nbsp; Or rent one, considering how often I need one.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for the info.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Gary&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 17 Jul 2009 01:00:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF52259-Dueling-Table-Data/m-p/198743#M9006</guid>
      <dc:creator>GaryOlmstead</dc:creator>
      <dc:date>2009-07-17T01:00:48Z</dc:date>
    </item>
  </channel>
</rss>