<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Address matters about external flashrom in mpc564 in ColdFire/68K Microcontrollers and Processors</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Address-matters-about-external-flashrom-in-mpc564/m-p/131332#M895</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&lt;P&gt;&lt;FONT size="2"&gt;flash,&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;This is a ColdFire forum, but I've gone ahead and dug up an answer for your MPC564 question.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;The DIP switches select which chip select goes to which memory device (RAM or FLASH), they do not determine the address. You have selected CS0 for external SRAM and CS2 for external Flash.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;The BR and OR registers need to be set to the correct values to allow external memory addressing via the chip selects.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;You&amp;nbsp;can look at the board manual that came with the board. It has recommended BR and OR settings for the EVB in Table 1-2 and can be found at the following Axiom Manufacturing link.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;A href="http://www.axman.com/cgi-bin/support/ProductInfo.pl?id=34" rel="nofollow" target="_blank"&gt;&lt;U&gt;&lt;FONT color="#0000ff" size="2"&gt;&lt;/FONT&gt;&lt;/U&gt;&lt;/A&gt;&lt;A href="http://www.axman.com/cgi-bin/support/ProductInfo.pl?id=34" target="test_blank"&gt;http://www.axman.com/cgi-bin/support/ProductInfo.pl?id=34&lt;/A&gt;&lt;FONT&gt;&lt;/FONT&gt;&lt;P&gt;&lt;/P&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 07 Apr 2006 22:12:51 GMT</pubDate>
    <dc:creator>mnorman</dc:creator>
    <dc:date>2006-04-07T22:12:51Z</dc:date>
    <item>
      <title>Address matters about external flashrom in mpc564</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Address-matters-about-external-flashrom-in-mpc564/m-p/131331#M894</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;DIV&gt;i have some trouble in using mpc564evb&amp;nbsp;.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;in mpc564evb ,i set dip1=ON DIP2=0ff,dip3=0ff and&amp;nbsp; dip4=ON in&lt;BR /&gt;map_sw ,but i don't know what address of external&lt;BR /&gt;flashrom(amd29bdd160gb).if the address is 0x00800000,i have alreadily&lt;BR /&gt;try ,but it have no effect in writing and reading flashrom .if i am&lt;BR /&gt;wrong,can you help findout the address of external flashrom and sram.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Can Someone&amp;nbsp;give me some example about external flashrom in mpc564evb.?&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;my email:&lt;/SPAN&gt;&lt;A class="jive-link-email-small" href="mailto:lingxiangzi@sina.com.cn"&gt;lingxiangzi@sina.com.cn&lt;/A&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Apr 2006 15:44:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Address-matters-about-external-flashrom-in-mpc564/m-p/131331#M894</guid>
      <dc:creator>flash</dc:creator>
      <dc:date>2006-04-04T15:44:38Z</dc:date>
    </item>
    <item>
      <title>Re: Address matters about external flashrom in mpc564</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Address-matters-about-external-flashrom-in-mpc564/m-p/131332#M895</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&lt;P&gt;&lt;FONT size="2"&gt;flash,&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;This is a ColdFire forum, but I've gone ahead and dug up an answer for your MPC564 question.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;The DIP switches select which chip select goes to which memory device (RAM or FLASH), they do not determine the address. You have selected CS0 for external SRAM and CS2 for external Flash.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;The BR and OR registers need to be set to the correct values to allow external memory addressing via the chip selects.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;You&amp;nbsp;can look at the board manual that came with the board. It has recommended BR and OR settings for the EVB in Table 1-2 and can be found at the following Axiom Manufacturing link.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;A href="http://www.axman.com/cgi-bin/support/ProductInfo.pl?id=34" rel="nofollow" target="_blank"&gt;&lt;U&gt;&lt;FONT color="#0000ff" size="2"&gt;&lt;/FONT&gt;&lt;/U&gt;&lt;/A&gt;&lt;A href="http://www.axman.com/cgi-bin/support/ProductInfo.pl?id=34" target="test_blank"&gt;http://www.axman.com/cgi-bin/support/ProductInfo.pl?id=34&lt;/A&gt;&lt;FONT&gt;&lt;/FONT&gt;&lt;P&gt;&lt;/P&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Apr 2006 22:12:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Address-matters-about-external-flashrom-in-mpc564/m-p/131332#M895</guid>
      <dc:creator>mnorman</dc:creator>
      <dc:date>2006-04-07T22:12:51Z</dc:date>
    </item>
  </channel>
</rss>