<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic require example code for UART MCF55233CAL60 in ColdFire/68K Microcontrollers and Processors</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/require-example-code-for-UART-MCF55233CAL60/m-p/196280#M8737</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hi,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;i am new to this microcontroller, if any one has example code for UART for this controller. could please send me. what are the steps to be take care while writing code for UART.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Regards,&lt;/DIV&gt;&lt;DIV&gt;paddy&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 22 Oct 2008 21:10:25 GMT</pubDate>
    <dc:creator>paddy</dc:creator>
    <dc:date>2008-10-22T21:10:25Z</dc:date>
    <item>
      <title>require example code for UART MCF55233CAL60</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/require-example-code-for-UART-MCF55233CAL60/m-p/196280#M8737</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hi,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;i am new to this microcontroller, if any one has example code for UART for this controller. could please send me. what are the steps to be take care while writing code for UART.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Regards,&lt;/DIV&gt;&lt;DIV&gt;paddy&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Oct 2008 21:10:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/require-example-code-for-UART-MCF55233CAL60/m-p/196280#M8737</guid>
      <dc:creator>paddy</dc:creator>
      <dc:date>2008-10-22T21:10:25Z</dc:date>
    </item>
    <item>
      <title>Re: require example code for UART MCF55233CAL60</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/require-example-code-for-UART-MCF55233CAL60/m-p/196281#M8738</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;Hi Paddy&lt;BR /&gt;&lt;BR /&gt;The UARTs can be driven in interrupt or DMA mode, with or without HW/SW flow control so there are various possible code options.&lt;BR /&gt;&lt;BR /&gt;Take a look at the uTasker project since it includes most options for UART (as well as various other peripherals, an OS, a TCP/IP stack and USB). It also allows you to develop and test complete code for the MCF52233 in the uTasker simulator - the simulated device will communicate either via a real COM port or else a virtual loop back device (eg com0com - see the following &lt;A href="http://www.utasker.com/forum/index.php?topic=343.0" rel="nofollow" target="_blank"&gt;http://www.utasker.com/forum/index.php?topic=343.0&lt;/A&gt; ).&lt;BR /&gt;&lt;BR /&gt;See the web site below and its forum at &lt;A href="http://www.uTasker.com/forum" rel="nofollow" target="_blank"&gt;www.uTasker.com/forum&lt;/A&gt; as well as on-line demo at &lt;A href="http://demo.utasker.com" rel="nofollow" target="_blank"&gt;demo.utasker.com&lt;/A&gt; (where you can configure its UART :smileywink: ).&lt;BR /&gt;&lt;BR /&gt;Regards&lt;BR /&gt;&lt;BR /&gt;Mark&lt;BR /&gt;&lt;BR /&gt;&lt;A href="http://www.uTasker.com" rel="nofollow" target="_blank"&gt;www.uTasker.com&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Oct 2008 23:08:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/require-example-code-for-UART-MCF55233CAL60/m-p/196281#M8738</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2008-10-22T23:08:32Z</dc:date>
    </item>
    <item>
      <title>Re: require example code for UART MCF55233CAL60</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/require-example-code-for-UART-MCF55233CAL60/m-p/196282#M8739</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;The Coldfire Niche Light project, available free on the MCF52235 page of the Freescale site contains several sample builds, including serial port code. It also has an ethernet TCP/IP stack, but there are builds in the project that strip out various sections of the code giving simpler projects with less bulk to them.&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Oct 2008 23:17:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/require-example-code-for-UART-MCF55233CAL60/m-p/196282#M8739</guid>
      <dc:creator>daverj</dc:creator>
      <dc:date>2008-10-22T23:17:27Z</dc:date>
    </item>
  </channel>
</rss>