<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>ColdFire/68K Microcontrollers and Processors中的主题 MCF5213 port pull-ups</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5213-port-pull-ups/m-p/131212#M866</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&amp;nbsp;In the users manual for the MCF5213 there is no mention of pull-up resistors for port TC pins (PTC[0] thru PTC[3]). However, if these four are lines are defined as general purpose inputs these&amp;nbsp;pins are acting as if there are approximately 30k pull-up resistors internally.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;Are there internal pull-ups on port TC?&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 26 Sep 2006 01:53:40 GMT</pubDate>
    <dc:creator>life_user</dc:creator>
    <dc:date>2006-09-26T01:53:40Z</dc:date>
    <item>
      <title>MCF5213 port pull-ups</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5213-port-pull-ups/m-p/131212#M866</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&amp;nbsp;In the users manual for the MCF5213 there is no mention of pull-up resistors for port TC pins (PTC[0] thru PTC[3]). However, if these four are lines are defined as general purpose inputs these&amp;nbsp;pins are acting as if there are approximately 30k pull-up resistors internally.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;Are there internal pull-ups on port TC?&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Sep 2006 01:53:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5213-port-pull-ups/m-p/131212#M866</guid>
      <dc:creator>life_user</dc:creator>
      <dc:date>2006-09-26T01:53:40Z</dc:date>
    </item>
    <item>
      <title>Re: MCF5213 port pull-ups</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5213-port-pull-ups/m-p/131213#M867</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;I think there's pull-up on Port TC, because in the MCF5213EC datasheet, Table 3 P18 Pull-up/pull-down column says, "2 All signals have a pull-up in GPIO mode".&lt;BR /&gt;In table 26, there's a parameter (Iapu) which specify the Weak Internal Pull Up Device Current, tested at VIL Max.&lt;BR /&gt;&lt;BR /&gt;Emmanuel&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Sep 2006 15:11:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5213-port-pull-ups/m-p/131213#M867</guid>
      <dc:creator>Nouchi</dc:creator>
      <dc:date>2006-09-26T15:11:15Z</dc:date>
    </item>
  </channel>
</rss>