<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: M52233DEMO - Communication error in ColdFire/68K Microcontrollers and Processors</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/M52233DEMO-Communication-error/m-p/195407#M8632</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hi,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&amp;nbsp; Check out the free ColdFire_LITE_TCPIP software stack available from Freescale at &lt;A href="http://www.freescale.com/coldfire" rel="nofollow" target="_blank"&gt;www.freescale.com/coldfire&lt;/A&gt;.&amp;nbsp; This TCP/IP stack&amp;nbsp;is provided free of charge, and in&amp;nbsp;source code that can be built using CodeWarrior for ColdFire v6.4.&amp;nbsp;&amp;nbsp; This is a great place to start for the MCF5223x family of MCUs with in 10/100BaseT Ethernet Interface with built in MAC &amp;amp; Phy.&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&amp;nbsp; There is also a ROM monitor called dBUG available&amp;nbsp;at no charge in source code from Freescale.&amp;nbsp;&amp;nbsp; Look for M5223EVB_DBUG.ZIP&amp;nbsp;using the search engine on the Freescale site.&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; There are also operating systems available for this&amp;nbsp;MCU family, including uTasker (&lt;A href="http://www.uTasker.com" rel="nofollow" target="_blank"&gt;www.uTasker.com&lt;/A&gt;), among&amp;nbsp;others.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;Thanks,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Rick&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 26 Feb 2008 10:47:56 GMT</pubDate>
    <dc:creator>RickN</dc:creator>
    <dc:date>2008-02-26T10:47:56Z</dc:date>
    <item>
      <title>M52233DEMO - Communication error</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/M52233DEMO-Communication-error/m-p/195406#M8631</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Hi all,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm new to freescale coldfire MCF5223x family. I buy an used M52233DEMO board and I cannot connect with this board.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I have the codewarrior 7.0 for CF, and in new project wizard, ColdFire evaluation boards-&amp;gt;M52233DEMO-&amp;gt;P&amp;amp;E USB Multilink --&amp;gt; with Processor Expert--&amp;gt; Full optimizations.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The chip in the board is a PCF52235LCAF60. I didn´t find this chip int the Processor expert CPU beans, only the 52233CAF60.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;.... I build the project, and when i click in the run, the program display (memory write failure&amp;nbsp; expected value0x20007ffxc, actual value0x00) using INTERNAL_RAM configuration&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;....and with the INTERNAL_ROM the program display (could not set PC to entry point)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;How could I connect to this board? With other programs , or other settings.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks for the help&lt;/SPAN&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 Feb 2008 11:28:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/M52233DEMO-Communication-error/m-p/195406#M8631</guid>
      <dc:creator>alvarobs</dc:creator>
      <dc:date>2008-02-25T11:28:48Z</dc:date>
    </item>
    <item>
      <title>Re: M52233DEMO - Communication error</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/M52233DEMO-Communication-error/m-p/195407#M8632</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hi,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&amp;nbsp; Check out the free ColdFire_LITE_TCPIP software stack available from Freescale at &lt;A href="http://www.freescale.com/coldfire" rel="nofollow" target="_blank"&gt;www.freescale.com/coldfire&lt;/A&gt;.&amp;nbsp; This TCP/IP stack&amp;nbsp;is provided free of charge, and in&amp;nbsp;source code that can be built using CodeWarrior for ColdFire v6.4.&amp;nbsp;&amp;nbsp; This is a great place to start for the MCF5223x family of MCUs with in 10/100BaseT Ethernet Interface with built in MAC &amp;amp; Phy.&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&amp;nbsp; There is also a ROM monitor called dBUG available&amp;nbsp;at no charge in source code from Freescale.&amp;nbsp;&amp;nbsp; Look for M5223EVB_DBUG.ZIP&amp;nbsp;using the search engine on the Freescale site.&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; There are also operating systems available for this&amp;nbsp;MCU family, including uTasker (&lt;A href="http://www.uTasker.com" rel="nofollow" target="_blank"&gt;www.uTasker.com&lt;/A&gt;), among&amp;nbsp;others.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;Thanks,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Rick&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Feb 2008 10:47:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/M52233DEMO-Communication-error/m-p/195407#M8632</guid>
      <dc:creator>RickN</dc:creator>
      <dc:date>2008-02-26T10:47:56Z</dc:date>
    </item>
  </channel>
</rss>