<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>ColdFire/68K Microcontrollers and Processors中的主题 Reset failure when battery backed</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Reset-failure-when-battery-backed/m-p/194917#M8603</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We are using a MCF52259 micro ccontroller with a rechargable battery connected to the VSTBY pin to maintain the Real Time Clock when the system is powered down.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;With the battery connected, when the unit is turned on the system fails to start (RSTO is held low). In this fault condition if the battery supply is disconnected even temporarily the system will start running normally. The battery voltage to the VSTBY pin is currently 3.1V - well within the specified operating range of 1.8 - 3.5V.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If the unit is powered up with the battery supply disconnected (VSTBY connected to VCC) the system works correctly.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have searched the forums and the processor User Manual and nothing sheds any light on this issue.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Richard.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 05 Jan 2012 22:38:27 GMT</pubDate>
    <dc:creator>rParker</dc:creator>
    <dc:date>2012-01-05T22:38:27Z</dc:date>
    <item>
      <title>Reset failure when battery backed</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Reset-failure-when-battery-backed/m-p/194917#M8603</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We are using a MCF52259 micro ccontroller with a rechargable battery connected to the VSTBY pin to maintain the Real Time Clock when the system is powered down.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;With the battery connected, when the unit is turned on the system fails to start (RSTO is held low). In this fault condition if the battery supply is disconnected even temporarily the system will start running normally. The battery voltage to the VSTBY pin is currently 3.1V - well within the specified operating range of 1.8 - 3.5V.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If the unit is powered up with the battery supply disconnected (VSTBY connected to VCC) the system works correctly.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have searched the forums and the processor User Manual and nothing sheds any light on this issue.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Richard.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 Jan 2012 22:38:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Reset-failure-when-battery-backed/m-p/194917#M8603</guid>
      <dc:creator>rParker</dc:creator>
      <dc:date>2012-01-05T22:38:27Z</dc:date>
    </item>
    <item>
      <title>Re: Reset failure when battery backed</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Reset-failure-when-battery-backed/m-p/194918#M8604</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Check this post:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.freescale.com/message/92208#92208" title="https://community.freescale.com/message/92208#92208"&gt;https://community.freescale.com/message/92208#92208&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;"ebee" found he had problems when the battery was "high" (3.6V).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Check your reset circuitry. When is reset released relative to the 3.3V coming up?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Tom&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 08 Jan 2012 13:32:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Reset-failure-when-battery-backed/m-p/194918#M8604</guid>
      <dc:creator>TomE</dc:creator>
      <dc:date>2012-01-08T13:32:56Z</dc:date>
    </item>
  </channel>
</rss>