<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>ColdFire/68K Microcontrollers and Processorsのトピックproblem with MSL</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/problem-with-MSL/m-p/193069#M8460</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; I'm having trouble with my project where I ported the FreeRTOS OS on a MCF52221.&lt;/P&gt;&lt;P&gt;I need to use the standard sprintf functio, nut if I use a standard complete MSL (C_4i_CF_StdABI_MSL.a) the project goes in Cpu_Interrupt because of some error accours.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The solution i fount out is to use the small MSL library (C_4i_CF_StdABI_SZ_MSL.a) as the guide saidformy processor. This means that a lot of functions like ato() atof() don't work. Another thing is that sprintf function has not complete functionality, like 0 padding.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;What I'm asking is: is there some option to use a complete MSL liibrary with MCF52221 or is mandatory to use the small one?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 23 Jun 2009 16:20:36 GMT</pubDate>
    <dc:creator>LPs1978</dc:creator>
    <dc:date>2009-06-23T16:20:36Z</dc:date>
    <item>
      <title>problem with MSL</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/problem-with-MSL/m-p/193069#M8460</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; I'm having trouble with my project where I ported the FreeRTOS OS on a MCF52221.&lt;/P&gt;&lt;P&gt;I need to use the standard sprintf functio, nut if I use a standard complete MSL (C_4i_CF_StdABI_MSL.a) the project goes in Cpu_Interrupt because of some error accours.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The solution i fount out is to use the small MSL library (C_4i_CF_StdABI_SZ_MSL.a) as the guide saidformy processor. This means that a lot of functions like ato() atof() don't work. Another thing is that sprintf function has not complete functionality, like 0 padding.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;What I'm asking is: is there some option to use a complete MSL liibrary with MCF52221 or is mandatory to use the small one?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Jun 2009 16:20:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/problem-with-MSL/m-p/193069#M8460</guid>
      <dc:creator>LPs1978</dc:creator>
      <dc:date>2009-06-23T16:20:36Z</dc:date>
    </item>
    <item>
      <title>Re: problem with MSL</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/problem-with-MSL/m-p/193070#M8461</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Maybe this thread can be helpful...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="http://forums.freescale.com/freescale/board/message?board.id=CWCFCOMM&amp;amp;message.id=2281&amp;amp;query.id=4110#M2281" target="_blank"&gt;http://forums.freescale.com/freescale/board/message?board.id=CWCFCOMM&amp;amp;message.id=2281&amp;amp;query.id=4110#M2281&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Jun 2009 17:37:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/problem-with-MSL/m-p/193070#M8461</guid>
      <dc:creator>vier_kuifjes</dc:creator>
      <dc:date>2009-06-23T17:37:13Z</dc:date>
    </item>
    <item>
      <title>Re: problem with MSL</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/problem-with-MSL/m-p/193071#M8462</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I helpful, I read it before to post my question.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;What I need is to know if the problem that I have with standard MSL library is a "standard problem" or is somethoing in my appplication that make sthe sprintf working wrong.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Jun 2009 19:27:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/problem-with-MSL/m-p/193071#M8462</guid>
      <dc:creator>LPs1978</dc:creator>
      <dc:date>2009-06-23T19:27:39Z</dc:date>
    </item>
  </channel>
</rss>