<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>ColdFire/68K Microcontrollers and ProcessorsのトピックRe: Problem with flashing U-Boot onto MCF5485evb</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Problem-with-flashing-U-Boot-onto-MCF5485evb/m-p/191867#M8371</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;There are a couple of things to check.&amp;nbsp; The first thing is to make sure the uboot you are using is built for 5485EVB and not the 5475EVB.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Then make sure that you have the baud rate in minicom set to 115200, and that you are using the top serial port on the 5485EVB.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;You can also check to make sure the serial cable that you are using is good.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;- Coray&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 25 Jun 2009 22:27:10 GMT</pubDate>
    <dc:creator>fsl_linux_spt</dc:creator>
    <dc:date>2009-06-25T22:27:10Z</dc:date>
    <item>
      <title>Problem with flashing U-Boot onto MCF5485evb</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Problem-with-flashing-U-Boot-onto-MCF5485evb/m-p/191863#M8367</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am trying to install Linux onto MCF5485EVB. My host system is CentOS. I have installed LTIB onto the host system. I have also installed CF Flasher(from Freescale site) and BDM drivers(from P&amp;amp;E Micro site). I have installed the drivers and CF flasher onto my host system using WINE. I am using LPT BDM interface for connecting host and target system.&lt;/P&gt;&lt;P&gt;When I try to program using CF flasher it gives me an error message saying "Could not initialize BDM device" .&lt;/P&gt;&lt;P&gt;What do I do? Any suggestions?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you for your help..&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Jun 2009 04:53:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Problem-with-flashing-U-Boot-onto-MCF5485evb/m-p/191863#M8367</guid>
      <dc:creator>rgirme</dc:creator>
      <dc:date>2009-06-19T04:53:06Z</dc:date>
    </item>
    <item>
      <title>Re: Problem with flashing U-Boot onto MCF5485evb</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Problem-with-flashing-U-Boot-onto-MCF5485evb/m-p/191864#M8368</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;CF Flasher has&amp;nbsp;not been tested on wine.&amp;nbsp;&amp;nbsp;You will need to&amp;nbsp;run it from a windows box.&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Jun 2009 00:54:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Problem-with-flashing-U-Boot-onto-MCF5485evb/m-p/191864#M8368</guid>
      <dc:creator>fsl_linux_spt</dc:creator>
      <dc:date>2009-06-23T00:54:40Z</dc:date>
    </item>
    <item>
      <title>Re: Problem with flashing U-Boot onto MCF5485evb</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Problem-with-flashing-U-Boot-onto-MCF5485evb/m-p/191865#M8369</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;EM&gt;Hi,&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am trying to install Linux onto MCF5485EVB.&lt;/P&gt;&lt;P&gt;I need CF flasher for writing the bootloader onto MCF5485. So you suggest that I should run CF flasher and write the bootloader onto the processor using host system as Windows OS?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Jun 2009 02:38:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Problem-with-flashing-U-Boot-onto-MCF5485evb/m-p/191865#M8369</guid>
      <dc:creator>rgirme</dc:creator>
      <dc:date>2009-06-23T02:38:31Z</dc:date>
    </item>
    <item>
      <title>Re: Problem with flashing U-Boot onto MCF5485evb</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Problem-with-flashing-U-Boot-onto-MCF5485evb/m-p/191866#M8370</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have flashed the processor with u-boot using CF flasher and Windows XP as host system. But when I start minicom, the u-boot does not show up.&lt;/P&gt;&lt;P&gt;What could be the problem?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Jun 2009 03:05:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Problem-with-flashing-U-Boot-onto-MCF5485evb/m-p/191866#M8370</guid>
      <dc:creator>rgirme</dc:creator>
      <dc:date>2009-06-24T03:05:50Z</dc:date>
    </item>
    <item>
      <title>Re: Problem with flashing U-Boot onto MCF5485evb</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Problem-with-flashing-U-Boot-onto-MCF5485evb/m-p/191867#M8371</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;There are a couple of things to check.&amp;nbsp; The first thing is to make sure the uboot you are using is built for 5485EVB and not the 5475EVB.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Then make sure that you have the baud rate in minicom set to 115200, and that you are using the top serial port on the 5485EVB.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;You can also check to make sure the serial cable that you are using is good.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;- Coray&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 Jun 2009 22:27:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Problem-with-flashing-U-Boot-onto-MCF5485evb/m-p/191867#M8371</guid>
      <dc:creator>fsl_linux_spt</dc:creator>
      <dc:date>2009-06-25T22:27:10Z</dc:date>
    </item>
  </channel>
</rss>