<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>ColdFire/68K Microcontrollers and Processors中的主题 Re: MCF5225X Tower - serial communication</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5225X-Tower-serial-communication/m-p/191199#M8312</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The UART on the serial card should work normally as long as the UART is set to UART1 (UB port configuration and not QS configuration).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 20 Mar 2011 19:43:20 GMT</pubDate>
    <dc:creator>mjbcswitzerland</dc:creator>
    <dc:date>2011-03-20T19:43:20Z</dc:date>
    <item>
      <title>MCF5225X Tower - serial communication</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5225X-Tower-serial-communication/m-p/191196#M8309</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I've just started the Tower kit and I am trying to run the "Hello" project from MQX. The problem is that I can connect to tower, I can flash the program, but I get nothing on Terminal window (using a straight cable from my computer to RS232 connector - which is placed on the below board). I'm not sure if everything is set up, because independently on which project I run, I can not see anything in terminal window.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Some help, please ?&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 Mar 2011 15:27:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5225X-Tower-serial-communication/m-p/191196#M8309</guid>
      <dc:creator>Paleantrop</dc:creator>
      <dc:date>2011-03-15T15:27:01Z</dc:date>
    </item>
    <item>
      <title>Re: MCF5225X Tower - serial communication</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5225X-Tower-serial-communication/m-p/191197#M8310</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Put an oscilloscope on what you think is the transmit data pin. You should see the board trying to transmit.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If you don't have a CRO, slow the baud rate down as much as you can and put a LED on it.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Then put the CRO on the RX pin and see if the terminal program transmits on there. Compare the bit widths.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Make sure you don't have two driven pins connected together (TX connected to TX etc).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Make sure the terminal program is configured with no flow control. It may be set to want the other signals (CTS, DTR and the like).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Does the Tower board provide these signals? Are they not-connected, driven from the chip or driven from pullup resistors?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The DB9 connector has three pins you care about. The other ones are there to cause trouble.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Try shorting TX to RX on the cable and see if the terminal program with display what you type (testing it and the cable by using a loopback).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Tom&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 18 Mar 2011 18:57:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5225X-Tower-serial-communication/m-p/191197#M8310</guid>
      <dc:creator>TomE</dc:creator>
      <dc:date>2011-03-18T18:57:29Z</dc:date>
    </item>
    <item>
      <title>Re: MCF5225X Tower - serial communication</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5225X-Tower-serial-communication/m-p/191198#M8311</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for your answer Tom. Meanwhile I have connected to RS232 connector from the Controller Board and I've been able to use it.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 18 Mar 2011 19:03:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5225X-Tower-serial-communication/m-p/191198#M8311</guid>
      <dc:creator>Paleantrop</dc:creator>
      <dc:date>2011-03-18T19:03:26Z</dc:date>
    </item>
    <item>
      <title>Re: MCF5225X Tower - serial communication</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5225X-Tower-serial-communication/m-p/191199#M8312</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The UART on the serial card should work normally as long as the UART is set to UART1 (UB port configuration and not QS configuration).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 20 Mar 2011 19:43:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5225X-Tower-serial-communication/m-p/191199#M8312</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2011-03-20T19:43:20Z</dc:date>
    </item>
  </channel>
</rss>