<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: M5485EVB &amp; ltib-mcf547x_8x-20070107 in ColdFire/68K Microcontrollers and Processors</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/M5485EVB-ltib-mcf547x-8x-20070107/m-p/190982#M8288</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi,&lt;BR /&gt;&lt;BR /&gt;Since my question of yesterday, I have fund some things.&lt;BR /&gt;If I understand well :&lt;BR /&gt;VFS is the virtual filesystem which give to system the methods to use real filesystem.&lt;BR /&gt;In my case, real filesystem must be in RAM.&lt;BR /&gt;&lt;BR /&gt;So, which filesystem must I use ?&lt;BR /&gt;cramfs is on RAM, but I have read somewhere that root can't be mount in cramfs. it's right ?&lt;BR /&gt;&lt;BR /&gt;With 2.4 kernel that I have used, filesystem is already include in file "image.bin" which seems to be a concatenation of linux kernel "linux.bin" and filesystem "romfs.img"...&lt;BR /&gt;In 2.6 kernel, I have only "vmlinux.bin" and filesystem "cramfs.big" or "routfs.jffs2" or others ...&lt;BR /&gt;How can I install my filesystem (and where) and link it to VFS.&lt;BR /&gt;&lt;BR /&gt;Thanks,&lt;BR /&gt;Pierrick&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 20 Feb 2008 15:28:20 GMT</pubDate>
    <dc:creator>pierrick</dc:creator>
    <dc:date>2008-02-20T15:28:20Z</dc:date>
    <item>
      <title>M5485EVB &amp; ltib-mcf547x_8x-20070107</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/M5485EVB-ltib-mcf547x-8x-20070107/m-p/190981#M8287</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Hi, (sorry for my bad english)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I work on&amp;nbsp; evaluation board M5485evb.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I want to install the Linux BSP that is on freescale website (ltib-mcf547x_8x-20070107).&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I have made many tests, but it doesn't work ... always crashing on :&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;"Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(1,0)"&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;DIV class="msg_source_code"&gt;&lt;DIV class="text_smallest"&gt;Code:&lt;/DIV&gt;&lt;PRE&gt;colilo&amp;gt;g 2000
Linux version 2.6.10 (pierrick@localhost) (gcc version 4.1.1 (CodeSourcery Sou
ery G++ 4.1-30)) #18 Mon Feb 18 18:17:30 CET 2008
starting up linux rev 0.2: startmem 0xc029c000, size 61MB
Built 1 zonelists
Kernel command line: root=/dev/ram
PID hash table entries: 512 (order: 9, 8192 bytes)
RTC driver is not initialized yet, returning 1970.
Console: colour dummy device 80x25
Dentry cache hash table entries: 16384 (order: 3, 65536 bytes)
Inode-cache hash table entries: 8192 (order: 2, 32768 bytes)
Memory: 62352k/65536k available (1976k kernel code, 1016k data, 96k init)
Mount-cache hash table entries: 1024 (order: 0, 8192 bytes)
NET: Registered protocol family 16
Linux/m68k PCI BIOS32 revision 0.05
ColdFire PCI Host Bridge (Rev. 0) detected
PCI: Probing PCI hardware
ColdFire internal SEC driver version 0.11
MCF547x/8x SEC device driver installed
SCSI subsystem initialized
NET: Registered protocol family 23
Initialize Multi-channel DMA API Alpha v0.3 (2004-04-26)
JFFS2 version 2.2. (C) 2001-2003 Red Hat, Inc.
Initializing Cryptographic API
rtc: RV5C387 RTC driver successfully loaded
ColdFire watchdog driver is loaded.
MCF547x/8x DSPI device driver installed
Coldfire DSPI driver is loaded
ColdFire internal UART serial driver version 1.00
ttyS0 at 0xe0008600 (irq = 99) is a builtin ColdFire UART
ttyS1 at 0xe0008700 (irq = 98) is a builtin ColdFire UART
ttyS2 at 0xe0008800 (irq = 97) is a builtin ColdFire UART
ttyS3 at 0xe0008900 (irq = 96) is a builtin ColdFire UART
io scheduler noop registered
io scheduler anticipatory registered
io scheduler deadline registered
io scheduler cfq registered
RAMDISK driver initialized: 16 RAM disks of 8192K size 1024 blocksize
loop: loaded (max 8 devices)
ColdFire internal FEC driver version 0.11
elevator: using anticipatory as default io scheduler
Unlock all sector for Intel on Fire Engine...
physmap flash device: 1000000 at f0000000
phys_mapped_flash: Found 1 x16 devices at 0x0 in 16-bit bank
 Intel/Sharp Extended Query Table at 0x0031
Using buffer write method
cfi_cmdset_0001: Erase suspend on write enabled
RedBoot partition parsing not available
Using physmap partition definition
Creating 2 MTD partitions on "phys_mapped_flash":
0x00000000-0x00040000 : "Colilo (256K)"
0x00040000-0x00200000 : "user (other Flash memory) 2Mb-256K"
mice: PS/2 mouse device common for all mice
i2c /dev entries driver
i2c-algo-mcf.o: I2C ColdFire algorithm module is loaded.
NET: Registered protocol family 2
IP: routing cache hash table of 1024 buckets, 8Kbytes
TCP: Hash tables configured (established 8192 bind 16384)
Initializing IPsec netlink socket
NET: Registered protocol family 1
NET: Registered protocol family 17
NET: Registered protocol family 15
IrCOMM protocol (Dag Brattli)
Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(1,0)&lt;/PRE&gt;&lt;/DIV&gt;&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;&lt;/DIV&gt;&lt;SPAN&gt;A time, I don't need special config, but only a Linux which run only in RAM.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;My last config attempt is on attached file...&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;So, could you help me please...&lt;/SPAN&gt;&lt;BR /&gt;&lt;UL&gt;&lt;LI&gt;what is exactly this "vfs" problem ?&lt;/LI&gt;&lt;LI&gt;could you give me a working config please ?&lt;/LI&gt;&lt;/UL&gt;&lt;SPAN&gt;thanks,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Pierrick&lt;/SPAN&gt;&lt;BR /&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.freescale.com%2Ffiles%2Fcommunity_files%2FCFCOMM%2Fmsg3986_linux_config.txt" rel="noopener noreferrer" target="_blank"&gt;linux_config.txt&lt;/A&gt;&lt;DIV class="message-edit-history"&gt;&lt;SPAN class="edit-author"&gt;Message Edited by t.dowe on&lt;/SPAN&gt; &lt;SPAN class="local-date"&gt;2009-09-04&lt;/SPAN&gt; &lt;SPAN class="local-time"&gt;02:40 PM&lt;/SPAN&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Oct 2020 09:42:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/M5485EVB-ltib-mcf547x-8x-20070107/m-p/190981#M8287</guid>
      <dc:creator>pierrick</dc:creator>
      <dc:date>2020-10-29T09:42:40Z</dc:date>
    </item>
    <item>
      <title>Re: M5485EVB &amp; ltib-mcf547x_8x-20070107</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/M5485EVB-ltib-mcf547x-8x-20070107/m-p/190982#M8288</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi,&lt;BR /&gt;&lt;BR /&gt;Since my question of yesterday, I have fund some things.&lt;BR /&gt;If I understand well :&lt;BR /&gt;VFS is the virtual filesystem which give to system the methods to use real filesystem.&lt;BR /&gt;In my case, real filesystem must be in RAM.&lt;BR /&gt;&lt;BR /&gt;So, which filesystem must I use ?&lt;BR /&gt;cramfs is on RAM, but I have read somewhere that root can't be mount in cramfs. it's right ?&lt;BR /&gt;&lt;BR /&gt;With 2.4 kernel that I have used, filesystem is already include in file "image.bin" which seems to be a concatenation of linux kernel "linux.bin" and filesystem "romfs.img"...&lt;BR /&gt;In 2.6 kernel, I have only "vmlinux.bin" and filesystem "cramfs.big" or "routfs.jffs2" or others ...&lt;BR /&gt;How can I install my filesystem (and where) and link it to VFS.&lt;BR /&gt;&lt;BR /&gt;Thanks,&lt;BR /&gt;Pierrick&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Feb 2008 15:28:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/M5485EVB-ltib-mcf547x-8x-20070107/m-p/190982#M8288</guid>
      <dc:creator>pierrick</dc:creator>
      <dc:date>2008-02-20T15:28:20Z</dc:date>
    </item>
  </channel>
</rss>