<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Kernel debug through BDM in M5484Lite EVB in ColdFire/68K Microcontrollers and Processors</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Kernel-debug-through-BDM-in-M5484Lite-EVB/m-p/190917#M8283</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;I am using Eclipse instead Codewarrior. Anyway, it would be enough to be able to debug the kernel through the gdb command line using the P&amp;amp;E BDM.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Could you resume the procedure you did with the P&amp;amp;E USB BDM?&amp;nbsp; It must be similar with the new LTIB.&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 07 Oct 2008 17:57:39 GMT</pubDate>
    <dc:creator>raulen</dc:creator>
    <dc:date>2008-10-07T17:57:39Z</dc:date>
    <item>
      <title>Kernel debug through BDM in M5484Lite EVB</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Kernel-debug-through-BDM-in-M5484Lite-EVB/m-p/190915#M8281</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hi everybody!&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;I need some help to be able to run my system.&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;I am using a MCF5484 Lite evaluation board and I am going to use Linux as the operating system. I had&amp;nbsp;&amp;nbsp; luck and could use the LTIB tool for this processor, that enables me to obtain easily the linux kernel image (kernel 2.6.25). I launched the system from U-Boot and I checked that all was OK.&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;I took the toolchain for this processor from Codesourcery (Sourcery G++ Lite 4.2.-25). Through the gdbserver and using Eclipse I can debug applications. But I also need to debug the kernel to add new drivers and other features. Using the Codesourcery Toolchain and by means of a P&amp;amp;E BDM device it should&amp;nbsp; be posible to debug the Linux kernel. I have two of these BDM devices: ParallelPortCable and USBMultilink, but I am not sucessful.&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;Does anyone have experience debugging the Linux kernel with this P&amp;amp;E BDM?&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;Any help will be welcome&lt;BR /&gt;Thanks in advance.&lt;BR /&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Oct 2008 14:05:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Kernel-debug-through-BDM-in-M5484Lite-EVB/m-p/190915#M8281</guid>
      <dc:creator>raulen</dc:creator>
      <dc:date>2008-10-03T14:05:59Z</dc:date>
    </item>
    <item>
      <title>Re: Kernel debug through BDM in M5484Lite EVB</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Kernel-debug-through-BDM-in-M5484Lite-EVB/m-p/190916#M8282</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;I've used P&amp;amp;E's USB BDM for some kernel debugging of the previous LTIB release (2.6.10) but it wasn't pretty. Basically, I used an older version of CodeWarrior to break the kernel where I wanted to and then step from there.&lt;BR /&gt;&lt;BR /&gt;I think the latest CodeWarrior has module debug capabilities so that might work for you. Or wait until someone ports the kgdb for MCF547x/8x.&lt;BR /&gt;&lt;BR /&gt;Best,&lt;BR /&gt;Andreas&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Oct 2008 13:01:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Kernel-debug-through-BDM-in-M5484Lite-EVB/m-p/190916#M8282</guid>
      <dc:creator>aeg</dc:creator>
      <dc:date>2008-10-07T13:01:49Z</dc:date>
    </item>
    <item>
      <title>Re: Kernel debug through BDM in M5484Lite EVB</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Kernel-debug-through-BDM-in-M5484Lite-EVB/m-p/190917#M8283</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;I am using Eclipse instead Codewarrior. Anyway, it would be enough to be able to debug the kernel through the gdb command line using the P&amp;amp;E BDM.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Could you resume the procedure you did with the P&amp;amp;E USB BDM?&amp;nbsp; It must be similar with the new LTIB.&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Oct 2008 17:57:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Kernel-debug-through-BDM-in-M5484Lite-EVB/m-p/190917#M8283</guid>
      <dc:creator>raulen</dc:creator>
      <dc:date>2008-10-07T17:57:39Z</dc:date>
    </item>
  </channel>
</rss>