<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Invalid interrupts on mcf5484 serial 0 in ColdFire/68K Microcontrollers and Processors</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Invalid-interrupts-on-mcf5484-serial-0/m-p/190518#M8258</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Reference manual (13.2.1.6 Interrupt Control Registers 1–63 (ICRn)) says :&lt;BR /&gt;"It is software’s responsibility to program the ICRn registers with unique and non-overlapping level and priority definitions. Failure to program the ICRn registers in this matter can result in undefined behavior. "&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Well, I had programmed the ICR registers for the four serial lines with the same value (040 (octal)) and those invalid interrupts were the results &lt;IMG alt=":smileysad:" class="emoticon emoticon-smileysad" id="smileysad" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-sad.gif" title="Smiley Sad" /&gt;.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 17 Apr 2010 12:24:30 GMT</pubDate>
    <dc:creator>phdm</dc:creator>
    <dc:date>2010-04-17T12:24:30Z</dc:date>
    <item>
      <title>Invalid interrupts on mcf5484 serial 0</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Invalid-interrupts-on-mcf5484-serial-0/m-p/190517#M8257</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We have made a board similar to MCF5484Lite one and use uClinux-dist (with added addresses for the mcf5484 serial lines and with slt0 as tick timer) on it.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Whenever we emit simultaneously on serial lines 1 &amp;amp; 2 (PSC1 &amp;amp; PSC2), we get invalid interrupts for PSC0.&amp;nbsp; This happens after about ten seconds of sending at 4800 bps on PSC1 and at 38400 on PSC2.&amp;nbsp; PSC0 is not used (TXRDY is masked,&lt;/P&gt;&lt;P&gt;IRQ99 is masked in IMRH and transmitter is disabled in PSC0, and still we receive interrupts on IRQ99, interrupts that we cannot stop, so our system becomes unusable.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Does that seem familiar to someone ?&amp;nbsp; Is that a known problem of the MCF5484 ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 10 Apr 2010 04:55:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Invalid-interrupts-on-mcf5484-serial-0/m-p/190517#M8257</guid>
      <dc:creator>phdm</dc:creator>
      <dc:date>2010-04-10T04:55:48Z</dc:date>
    </item>
    <item>
      <title>Re: Invalid interrupts on mcf5484 serial 0</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Invalid-interrupts-on-mcf5484-serial-0/m-p/190518#M8258</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Reference manual (13.2.1.6 Interrupt Control Registers 1–63 (ICRn)) says :&lt;BR /&gt;"It is software’s responsibility to program the ICRn registers with unique and non-overlapping level and priority definitions. Failure to program the ICRn registers in this matter can result in undefined behavior. "&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Well, I had programmed the ICR registers for the four serial lines with the same value (040 (octal)) and those invalid interrupts were the results &lt;IMG alt=":smileysad:" class="emoticon emoticon-smileysad" id="smileysad" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-sad.gif" title="Smiley Sad" /&gt;.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 17 Apr 2010 12:24:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Invalid-interrupts-on-mcf5484-serial-0/m-p/190518#M8258</guid>
      <dc:creator>phdm</dc:creator>
      <dc:date>2010-04-17T12:24:30Z</dc:date>
    </item>
  </channel>
</rss>