<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>ColdFire/68K Microcontrollers and Processors中的主题 Controlling 15&amp;quot; LCD</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Controlling-15-quot-LCD/m-p/189394#M8170</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN class="medium_text"&gt;&lt;SPAN&gt;Hello&lt;BR /&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;SPAN&gt;Is it possible to control a 15-inch LCD with a ColdFire?. Do not know if I can do, is to buy a monitor and remove, to begin testing. Many thanks.&lt;BR /&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;SPAN&gt;Regards&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 07 Apr 2010 07:42:37 GMT</pubDate>
    <dc:creator>Pakito</dc:creator>
    <dc:date>2010-04-07T07:42:37Z</dc:date>
    <item>
      <title>Controlling 15" LCD</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Controlling-15-quot-LCD/m-p/189394#M8170</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN class="medium_text"&gt;&lt;SPAN&gt;Hello&lt;BR /&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;SPAN&gt;Is it possible to control a 15-inch LCD with a ColdFire?. Do not know if I can do, is to buy a monitor and remove, to begin testing. Many thanks.&lt;BR /&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;SPAN&gt;Regards&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Apr 2010 07:42:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Controlling-15-quot-LCD/m-p/189394#M8170</guid>
      <dc:creator>Pakito</dc:creator>
      <dc:date>2010-04-07T07:42:37Z</dc:date>
    </item>
    <item>
      <title>Re: Controlling 15" LCD</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Controlling-15-quot-LCD/m-p/189395#M8171</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, it is possible. To do that, you are going to need a graphics controller. Epson and Fujitsu are two prominent manufacturers of embedded graphics controllers. Have a look at their products. Normally, you'd interface to a TFT panel with a digital RGB interface. But there are graphics controllers with video DAC built-in, so you can interface to a standard analog VGA input.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Apr 2010 12:48:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Controlling-15-quot-LCD/m-p/189395#M8171</guid>
      <dc:creator>scifi</dc:creator>
      <dc:date>2010-04-07T12:48:07Z</dc:date>
    </item>
    <item>
      <title>Re: Controlling 15" LCD</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Controlling-15-quot-LCD/m-p/189396#M8172</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It depends what you're trying to do - VGA / SVGA RGB output, PAL/NTSC composite video, or control an LCD module directly at the hardware level.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Check out the Maxim MAX7456 for PAL/NTSC composite video on-screen-displays, they do similar chips for VGA/RGB too.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 08 Apr 2010 17:16:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Controlling-15-quot-LCD/m-p/189396#M8172</guid>
      <dc:creator>FridgeFreezer</dc:creator>
      <dc:date>2010-04-08T17:16:15Z</dc:date>
    </item>
  </channel>
</rss>