<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>ColdFire/68K Microcontrollers and Processors中的主题 Re: ucLibc missing from ltib-cflinux-20111026</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/ucLibc-missing-from-ltib-cflinux-20111026/m-p/189160#M8125</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Looking into this more, it seems that the support for uClibc in ltib-cflinux-20111026 might have been removed for a reason. looking into the ltib spec file for the uclibc, it looks like they build uclibc as a static library then fake out libc.so to use this STATIC library.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;ltib-cflinux-20111026/dist/lfs-5.1/uclibc/uclibc.spec&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The line&lt;/P&gt;&lt;P&gt;perl -i.orig -p -e 's,/lib/libc.so.0,../../lib/libc.so.0,; s,/usr/lib/uclibc_nonshared.a,./uclibc_nonshared.a,' libc.so&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Seems to be replacing paths to the libs so with the uclibc static library.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This would defeat the purpose of uclibc (smaller image size). I guess the tlib developers realized this and did not completely remove it from the configuration.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Anyone know where I can get a toolchain for coldfire that supports uclibc?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 12 Dec 2011 23:30:07 GMT</pubDate>
    <dc:creator>zinger</dc:creator>
    <dc:date>2011-12-12T23:30:07Z</dc:date>
    <item>
      <title>ucLibc missing from ltib-cflinux-20111026</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/ucLibc-missing-from-ltib-cflinux-20111026/m-p/189159#M8124</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Looks like uClibc-r18301.tar.bz2 is missing in the iso&amp;nbsp;CFLINUX_20111031_ltib.iso&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;./ltib --preconfig ./config/platform/cflinux/m54455evb-flash.defconfig -m scdeploy -p uclibc&lt;/P&gt;&lt;P&gt;Fails with error:&lt;/P&gt;&lt;P&gt;error: File /home/[me]/freescale/ltib-cflinux-20111026/rpm/SOURCES/uClibc-r18301.tar.bz2: No such file or directory&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;this file is nowhere on the iso image either, and does not seem to be a standard release.&lt;/P&gt;&lt;P&gt;Any idea where this file is?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Dec 2011 22:23:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/ucLibc-missing-from-ltib-cflinux-20111026/m-p/189159#M8124</guid>
      <dc:creator>zinger</dc:creator>
      <dc:date>2011-12-09T22:23:52Z</dc:date>
    </item>
    <item>
      <title>Re: ucLibc missing from ltib-cflinux-20111026</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/ucLibc-missing-from-ltib-cflinux-20111026/m-p/189160#M8125</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Looking into this more, it seems that the support for uClibc in ltib-cflinux-20111026 might have been removed for a reason. looking into the ltib spec file for the uclibc, it looks like they build uclibc as a static library then fake out libc.so to use this STATIC library.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;ltib-cflinux-20111026/dist/lfs-5.1/uclibc/uclibc.spec&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The line&lt;/P&gt;&lt;P&gt;perl -i.orig -p -e 's,/lib/libc.so.0,../../lib/libc.so.0,; s,/usr/lib/uclibc_nonshared.a,./uclibc_nonshared.a,' libc.so&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Seems to be replacing paths to the libs so with the uclibc static library.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This would defeat the purpose of uclibc (smaller image size). I guess the tlib developers realized this and did not completely remove it from the configuration.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Anyone know where I can get a toolchain for coldfire that supports uclibc?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Dec 2011 23:30:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/ucLibc-missing-from-ltib-cflinux-20111026/m-p/189160#M8125</guid>
      <dc:creator>zinger</dc:creator>
      <dc:date>2011-12-12T23:30:07Z</dc:date>
    </item>
  </channel>
</rss>