<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>ColdFire/68K Microcontrollers and Processors中的主题 Re: edma on dspi is so ineffective</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/edma-on-dspi-is-so-ineffective/m-p/186225#M7816</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;thank the reply, when I try the spi, set the pcs to sck delay to 5us,then i got byte to byte delay 5us,how could get fast byte transfer and remain pcs to sck delay. can someone help me out?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 29 Nov 2011 09:59:34 GMT</pubDate>
    <dc:creator>yan211</dc:creator>
    <dc:date>2011-11-29T09:59:34Z</dc:date>
    <item>
      <title>edma on dspi is so ineffective</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/edma-on-dspi-is-so-ineffective/m-p/186223#M7814</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp;I am working on the powerfull mcf54415,In my eyes ,the edma can get all out of the chip,but when i dive into the spi code, i was comfused. the edma did nothing ,but make thing conplicate.it just transfer 16 byte a time, then in the enoq interrupt ,it trigger rx edma channel to get the rx byte to dma buffer, then copy to user buffer,SO what the use of edma.&lt;/P&gt;&lt;P&gt;&amp;nbsp; Can any one give a explain? Can i make the dma to transfer 1MB a time with just a interrupt?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 25 Nov 2011 20:52:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/edma-on-dspi-is-so-ineffective/m-p/186223#M7814</guid>
      <dc:creator>yan211</dc:creator>
      <dc:date>2011-11-25T20:52:17Z</dc:date>
    </item>
    <item>
      <title>Re: edma on dspi is so ineffective</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/edma-on-dspi-is-so-ineffective/m-p/186224#M7815</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;That was what I thought as well. If you have to copy it to the registers, whats the point?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 26 Nov 2011 13:05:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/edma-on-dspi-is-so-ineffective/m-p/186224#M7815</guid>
      <dc:creator>JimDon</dc:creator>
      <dc:date>2011-11-26T13:05:22Z</dc:date>
    </item>
    <item>
      <title>Re: edma on dspi is so ineffective</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/edma-on-dspi-is-so-ineffective/m-p/186225#M7816</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;thank the reply, when I try the spi, set the pcs to sck delay to 5us,then i got byte to byte delay 5us,how could get fast byte transfer and remain pcs to sck delay. can someone help me out?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 29 Nov 2011 09:59:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/edma-on-dspi-is-so-ineffective/m-p/186225#M7816</guid>
      <dc:creator>yan211</dc:creator>
      <dc:date>2011-11-29T09:59:34Z</dc:date>
    </item>
    <item>
      <title>Re: edma on dspi is so ineffective</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/edma-on-dspi-is-so-ineffective/m-p/186226#M7817</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;too fast to ask! now i try to use different CTAR, got the expect!!so versatile the dspi&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 29 Nov 2011 10:24:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/edma-on-dspi-is-so-ineffective/m-p/186226#M7817</guid>
      <dc:creator>yan211</dc:creator>
      <dc:date>2011-11-29T10:24:55Z</dc:date>
    </item>
  </channel>
</rss>