<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>ColdFire/68K Microcontrollers and ProcessorsのトピックRe: MCF5475 - code execution from flash</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5475-code-execution-from-flash/m-p/186183#M7813</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi,&lt;BR /&gt;&lt;BR /&gt;sorry, I am neither an expert for MCF547x nor Intel P33 - in my own board with MCF5373L and Intel P30 flash I finally left out the connection of WAIT to /TA because I did not find a way to use it properly.&lt;BR /&gt;&lt;BR /&gt;I hope there are others who can give more detailed advice for this specific configuration.&lt;BR /&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Wolfgang&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 07 Feb 2008 16:58:00 GMT</pubDate>
    <dc:creator>w_wegner</dc:creator>
    <dc:date>2008-02-07T16:58:00Z</dc:date>
    <item>
      <title>MCF5475 - code execution from flash</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5475-code-execution-from-flash/m-p/186180#M7810</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hi,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I am able to debug from flash, but i am not able to run the code stand alone. Do i have to change any settings to run the code directly from flash on reset. I am using Intel P33 flash. Using FB_CS0 for flash. Address range for flash is from 0xee000000 to 0xefffffff. Could someone help me out.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Jaimy&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Feb 2008 18:28:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5475-code-execution-from-flash/m-p/186180#M7810</guid>
      <dc:creator>Jaimy</dc:creator>
      <dc:date>2008-02-05T18:28:55Z</dc:date>
    </item>
    <item>
      <title>Re: MCF5475 - code execution from flash</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5475-code-execution-from-flash/m-p/186181#M7811</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi,&lt;BR /&gt;&lt;BR /&gt;I am not sure if this applies to MCF547x/8x, too, but some questions:&lt;BR /&gt;- do you use BDM for debugging? If so, do you have a pullup on BKPT on your processor board? It is needed at least for MCF5373, although I did not find a reference in the data sheet&lt;BR /&gt;- also, on my MCF5373 board, i needed a pullup resistor on my console serial port RX line for U-Boot - I am not sure if this is a driver or hardware thing, but for my design U-Boot would not start up without this pullup or a level converter attached.&lt;BR /&gt;&lt;BR /&gt;(The same might apply to /TA, if this signal is present on MCF547x, too)&lt;BR /&gt;&lt;BR /&gt;HTH,&lt;BR /&gt;Wolfgang&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Feb 2008 20:05:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5475-code-execution-from-flash/m-p/186181#M7811</guid>
      <dc:creator>w_wegner</dc:creator>
      <dc:date>2008-02-06T20:05:18Z</dc:date>
    </item>
    <item>
      <title>Re: MCF5475 - code execution from flash</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5475-code-execution-from-flash/m-p/186182#M7812</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hi,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;BKPT is used and is pulled high. I have given serial port lines to rs232 level converter. /TA line is also used in BDM and is pulled high.&lt;/DIV&gt;&lt;DIV&gt;But one doubt is /TA line is also connected to WAIT of flash. But WAIT is only used in synchronous mode. On reset only asynchronous read mode is used. While debugging in initialisation file, /TA line is made GPIO. Only then i am able to access flash. But this is not possible in stand alone. On reset /TA is not GPIO.&lt;/DIV&gt;&lt;DIV&gt;Even when i am shorting /TA high, flash is accessible in debug mode without making it GPIO&amp;nbsp;but not in stand alone. There is no way&amp;nbsp;to disconnect WAIT from&amp;nbsp;/TA in board. &amp;nbsp;Attaching the interface diagram i have used. R/W, CLK, WP#, CS#, OE#&amp;nbsp;, /TA are all pulled high. &amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Is it possible to use same flash for asynchronous as well as synchronous mode with one set of connections?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;jaimy&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Feb 2008 12:50:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5475-code-execution-from-flash/m-p/186182#M7812</guid>
      <dc:creator>Jaimy</dc:creator>
      <dc:date>2008-02-07T12:50:59Z</dc:date>
    </item>
    <item>
      <title>Re: MCF5475 - code execution from flash</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5475-code-execution-from-flash/m-p/186183#M7813</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi,&lt;BR /&gt;&lt;BR /&gt;sorry, I am neither an expert for MCF547x nor Intel P33 - in my own board with MCF5373L and Intel P30 flash I finally left out the connection of WAIT to /TA because I did not find a way to use it properly.&lt;BR /&gt;&lt;BR /&gt;I hope there are others who can give more detailed advice for this specific configuration.&lt;BR /&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Wolfgang&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Feb 2008 16:58:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5475-code-execution-from-flash/m-p/186183#M7813</guid>
      <dc:creator>w_wegner</dc:creator>
      <dc:date>2008-02-07T16:58:00Z</dc:date>
    </item>
  </channel>
</rss>