<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>ColdFire/68K Microcontrollers and Processors中的主题 Re: Coldfire V1 &amp; V2</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Coldfire-V1-V2/m-p/186002#M7783</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Download every development board schematic you can find and see how things are connected. there. Copy them slavishly.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;1.5.2 Integrated Debug Module&lt;/P&gt;&lt;P&gt;The device includes a new debug signal, ALLPST. This signal is the logical AND&lt;/P&gt;&lt;P&gt;of the processor status (PST[3:0]) signals and is useful for detecting when the&lt;/P&gt;&lt;P&gt;processor is in a halted state (PST[3:0] = 1111).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Does your debugger need DDATA[3:0] and PST[3:0]? Does it need ALLPST as well or instead?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Note "33.4.6 Freescale-Recommended BDM Pinout" shows 23 of the 26 pins connected. You have 13. That my be what you want, but check. Your debugger manual might clear this up.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I don't like your power-on circuitry. THe chip has "low voltage detect" forcing reset, but it doesn't trigger until 2.15V, and the CPU isn't rated to run at under 3.0V. I think you need an external reset generator on RSTI, so it mightn't survive or recover from a brownout.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Why are you adding pulldowns on all those pins? You don't need to pull any pin you can program as an output and force high or low.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Tom&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 07 Aug 2012 21:25:46 GMT</pubDate>
    <dc:creator>TomE</dc:creator>
    <dc:date>2012-08-07T21:25:46Z</dc:date>
    <item>
      <title>Coldfire V1 &amp; V2</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Coldfire-V1-V2/m-p/186001#M7782</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everybody,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am going to start two projects; one with Coldfire V1 (MCF51MM128CLK) and one with Coldfire V2(MCF52252AF80)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have attached two schematics.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Could someone tell me if there is any error between the controller and debugger connector?&lt;/P&gt;&lt;P&gt;Also I am not sure where the ALLPST pin of coldfire V2 should be connected.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Nikos&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 Aug 2012 01:43:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Coldfire-V1-V2/m-p/186001#M7782</guid>
      <dc:creator>Eric_t</dc:creator>
      <dc:date>2012-08-06T01:43:48Z</dc:date>
    </item>
    <item>
      <title>Re: Coldfire V1 &amp; V2</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Coldfire-V1-V2/m-p/186002#M7783</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Download every development board schematic you can find and see how things are connected. there. Copy them slavishly.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;1.5.2 Integrated Debug Module&lt;/P&gt;&lt;P&gt;The device includes a new debug signal, ALLPST. This signal is the logical AND&lt;/P&gt;&lt;P&gt;of the processor status (PST[3:0]) signals and is useful for detecting when the&lt;/P&gt;&lt;P&gt;processor is in a halted state (PST[3:0] = 1111).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Does your debugger need DDATA[3:0] and PST[3:0]? Does it need ALLPST as well or instead?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Note "33.4.6 Freescale-Recommended BDM Pinout" shows 23 of the 26 pins connected. You have 13. That my be what you want, but check. Your debugger manual might clear this up.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I don't like your power-on circuitry. THe chip has "low voltage detect" forcing reset, but it doesn't trigger until 2.15V, and the CPU isn't rated to run at under 3.0V. I think you need an external reset generator on RSTI, so it mightn't survive or recover from a brownout.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Why are you adding pulldowns on all those pins? You don't need to pull any pin you can program as an output and force high or low.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Tom&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Aug 2012 21:25:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Coldfire-V1-V2/m-p/186002#M7783</guid>
      <dc:creator>TomE</dc:creator>
      <dc:date>2012-08-07T21:25:46Z</dc:date>
    </item>
  </channel>
</rss>