<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MCF5329 with USB low-speed in ColdFire/68K Microcontrollers and Processors</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5329-with-USB-low-speed/m-p/185933#M7775</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;21.3.3.14 Port Status and Control Registers (PORTSCn)&lt;/P&gt;&lt;P&gt;...&lt;/P&gt;&lt;P&gt;- Port speed. This read-only register field indicates the speed the port operates. This bit is not defined in the EHCI&lt;BR /&gt;specification.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;What is that showing?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;- Line status. Reflects current logical levels of the USB DP (bit 11) and DM (bit 10) signal lines.&lt;/P&gt;&lt;P&gt;- High speed port. Indicates if the host/device connected is in high speed mode.&lt;BR /&gt;&amp;nbsp; Note: This bit is redundant with the PSPD bit field.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;What are they showing?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;You probably have to reset the port to get it to switch (if it doesn't do that on its own).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Check section "21.5.5.6.2 Discovery"&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 25 Feb 2011 14:57:05 GMT</pubDate>
    <dc:creator>TomE</dc:creator>
    <dc:date>2011-02-25T14:57:05Z</dc:date>
    <item>
      <title>MCF5329 with USB low-speed</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5329-with-USB-low-speed/m-p/185932#M7774</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello!&lt;/P&gt;&lt;P&gt;I'm trying to implement an USB-stack of my own. The (nearly) the complete handling seems to work on full-speed, but if i switch to low-speed (through d-minus pullup instead of d-plus pullup through external max3353e), nothing is working (no packets are send properly). is there a register in the mcf5329 to tell the internal transceiver that it should run on low-speed mode now? Somehow i don't see that kind of configuration.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance!!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 24 Feb 2011 20:52:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5329-with-USB-low-speed/m-p/185932#M7774</guid>
      <dc:creator>Rost</dc:creator>
      <dc:date>2011-02-24T20:52:40Z</dc:date>
    </item>
    <item>
      <title>Re: MCF5329 with USB low-speed</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5329-with-USB-low-speed/m-p/185933#M7775</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;21.3.3.14 Port Status and Control Registers (PORTSCn)&lt;/P&gt;&lt;P&gt;...&lt;/P&gt;&lt;P&gt;- Port speed. This read-only register field indicates the speed the port operates. This bit is not defined in the EHCI&lt;BR /&gt;specification.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;What is that showing?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;- Line status. Reflects current logical levels of the USB DP (bit 11) and DM (bit 10) signal lines.&lt;/P&gt;&lt;P&gt;- High speed port. Indicates if the host/device connected is in high speed mode.&lt;BR /&gt;&amp;nbsp; Note: This bit is redundant with the PSPD bit field.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;What are they showing?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;You probably have to reset the port to get it to switch (if it doesn't do that on its own).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Check section "21.5.5.6.2 Discovery"&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 25 Feb 2011 14:57:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5329-with-USB-low-speed/m-p/185933#M7775</guid>
      <dc:creator>TomE</dc:creator>
      <dc:date>2011-02-25T14:57:05Z</dc:date>
    </item>
  </channel>
</rss>