<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>ColdFire/68K Microcontrollers and ProcessorsのトピックCompact Flash (ATA) Hot Swap on MCF5445x - CPU freeze</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Compact-Flash-ATA-Hot-Swap-on-MCF5445x-CPU-freeze/m-p/184577#M7674</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a 54454 design using a Compact Flash card attached directly to the ATA lines. When the CF card is inserted when the board is powered up (i.e. hot swapped), approximately 1/3 of the time the CPU will freeze (and eventually resets due to the watchdog). If the board is reset&amp;nbsp;with the card in place, the CF card works perfectly. Has anyone else seen any issues with this?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;The wiring is fairly straight forward and follows the various appnotes I've found on the subject. Basically a direct connection from the CF card holder, to the corresponding pin on the 54454 ATA bus, with pullups/downs where appropriate.&lt;/LI&gt;&lt;LI&gt;I&amp;nbsp;have eliminated software being the issue. I can completely reduce the code running on the CPU to almost nothing (including no&amp;nbsp;ATA interaction of any kind) and the probloem still occurs.&lt;/LI&gt;&lt;LI&gt;The only thing that seems to do the trick is killing power to the CF card, which obviously isn't terribly useful.&lt;/LI&gt;&lt;LI&gt;If the watchdog is disabled, the CPU becomes completely frozen. There are no exceptions, no bus faults, nothing at all.&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;Any ideas? Has anyone else successfully designed a CF interface on the 54454? If so, can you hot wap the card? Anyone perhaps have similar experiences with normal ATA devices (i.e. hot swapable HDs)?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Chris&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Keywords: MCF54454, MCF54455,&amp;nbsp;MCF5445x, 54454, 54455, 5445x, ATA, Compact Flash, CF, hot swap&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 20 Mar 2010 02:44:34 GMT</pubDate>
    <dc:creator>cmaryan</dc:creator>
    <dc:date>2010-03-20T02:44:34Z</dc:date>
    <item>
      <title>Compact Flash (ATA) Hot Swap on MCF5445x - CPU freeze</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Compact-Flash-ATA-Hot-Swap-on-MCF5445x-CPU-freeze/m-p/184577#M7674</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a 54454 design using a Compact Flash card attached directly to the ATA lines. When the CF card is inserted when the board is powered up (i.e. hot swapped), approximately 1/3 of the time the CPU will freeze (and eventually resets due to the watchdog). If the board is reset&amp;nbsp;with the card in place, the CF card works perfectly. Has anyone else seen any issues with this?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;The wiring is fairly straight forward and follows the various appnotes I've found on the subject. Basically a direct connection from the CF card holder, to the corresponding pin on the 54454 ATA bus, with pullups/downs where appropriate.&lt;/LI&gt;&lt;LI&gt;I&amp;nbsp;have eliminated software being the issue. I can completely reduce the code running on the CPU to almost nothing (including no&amp;nbsp;ATA interaction of any kind) and the probloem still occurs.&lt;/LI&gt;&lt;LI&gt;The only thing that seems to do the trick is killing power to the CF card, which obviously isn't terribly useful.&lt;/LI&gt;&lt;LI&gt;If the watchdog is disabled, the CPU becomes completely frozen. There are no exceptions, no bus faults, nothing at all.&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;Any ideas? Has anyone else successfully designed a CF interface on the 54454? If so, can you hot wap the card? Anyone perhaps have similar experiences with normal ATA devices (i.e. hot swapable HDs)?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Chris&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Keywords: MCF54454, MCF54455,&amp;nbsp;MCF5445x, 54454, 54455, 5445x, ATA, Compact Flash, CF, hot swap&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 20 Mar 2010 02:44:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Compact-Flash-ATA-Hot-Swap-on-MCF5445x-CPU-freeze/m-p/184577#M7674</guid>
      <dc:creator>cmaryan</dc:creator>
      <dc:date>2010-03-20T02:44:34Z</dc:date>
    </item>
    <item>
      <title>Re: Compact Flash (ATA) Hot Swap on MCF5445x - CPU freeze</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Compact-Flash-ATA-Hot-Swap-on-MCF5445x-CPU-freeze/m-p/184578#M7675</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;This is probably power system issue. On this page is same notes about hot swap of MMC/SC cards and apropriate power lines decupling. &lt;A href="http://elm-chan.org/docs/mmc/mmc_e.html" rel="nofollow" target="_blank"&gt;http://elm-chan.org/docs/mmc/mmc_e.html&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Andrija&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 22 Mar 2010 18:04:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Compact-Flash-ATA-Hot-Swap-on-MCF5445x-CPU-freeze/m-p/184578#M7675</guid>
      <dc:creator>aersek</dc:creator>
      <dc:date>2010-03-22T18:04:09Z</dc:date>
    </item>
    <item>
      <title>Re: Compact Flash (ATA) Hot Swap on MCF5445x - CPU freeze</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Compact-Flash-ATA-Hot-Swap-on-MCF5445x-CPU-freeze/m-p/184579#M7676</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please provide me the schematic of CF to ATA converter if you have sucessfully sorted out the problem. I require this for my design.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;regards&lt;/P&gt;&lt;P&gt;Ammar&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 19 Jun 2011 02:24:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Compact-Flash-ATA-Hot-Swap-on-MCF5445x-CPU-freeze/m-p/184579#M7676</guid>
      <dc:creator>AmmarAhmedSiddi</dc:creator>
      <dc:date>2011-06-19T02:24:15Z</dc:date>
    </item>
  </channel>
</rss>