<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MCF5212 - Problem writing flash via EZPort in ColdFire/68K Microcontrollers and Processors</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5212-Problem-writing-flash-via-EZPort/m-p/183521#M7590</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;I've done some further trials to narrow down my problem.&lt;BR /&gt;&lt;BR /&gt;It turns out that if I erase sector zero and then reset the ColdFire, I lose the ability to further write to flash&lt;BR /&gt;via the EZPort interface.&lt;BR /&gt;&lt;BR /&gt;If I erase and then re-program the flash without resetting in between, everything is OK. I can still write&lt;BR /&gt;to flash.&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 30 Jan 2008 07:37:18 GMT</pubDate>
    <dc:creator>jim_wygralak</dc:creator>
    <dc:date>2008-01-30T07:37:18Z</dc:date>
    <item>
      <title>MCF5212 - Problem writing flash via EZPort</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5212-Problem-writing-flash-via-EZPort/m-p/183520#M7589</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;I am attempting to develop a system for programming the ColdFire flash via the EZPort.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The problem I've run into is that if the ColdFire doesn't already have a runable image in flash, I can not&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;write to it, or erase it.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;If I program it via the BDM port, I can then read, erase, and write the upper unused blocks using the EZPort,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;all I want. As soon as I erase the low blocks that contain the programmed image, I lose the ability to further&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;write or erase any of the flash memory. I can still read from it, however.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I don't understand why erasing flash should prevent me from programming it further. This also prevents me&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;from using EZPort to program fresh chips.&lt;/SPAN&gt;&lt;BR /&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 29 Jan 2008 06:27:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5212-Problem-writing-flash-via-EZPort/m-p/183520#M7589</guid>
      <dc:creator>jim_wygralak</dc:creator>
      <dc:date>2008-01-29T06:27:58Z</dc:date>
    </item>
    <item>
      <title>Re: MCF5212 - Problem writing flash via EZPort</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5212-Problem-writing-flash-via-EZPort/m-p/183521#M7590</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;I've done some further trials to narrow down my problem.&lt;BR /&gt;&lt;BR /&gt;It turns out that if I erase sector zero and then reset the ColdFire, I lose the ability to further write to flash&lt;BR /&gt;via the EZPort interface.&lt;BR /&gt;&lt;BR /&gt;If I erase and then re-program the flash without resetting in between, everything is OK. I can still write&lt;BR /&gt;to flash.&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 Jan 2008 07:37:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5212-Problem-writing-flash-via-EZPort/m-p/183521#M7590</guid>
      <dc:creator>jim_wygralak</dc:creator>
      <dc:date>2008-01-30T07:37:18Z</dc:date>
    </item>
    <item>
      <title>Re: MCF5212 - Problem writing flash via EZPort</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5212-Problem-writing-flash-via-EZPort/m-p/183522#M7591</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am facing similar problems with writing to the chip after erase cycle.&lt;/P&gt;&lt;P&gt;Following your advice I perform PP right after BE command without living EzPort mode. It helped, I have no Write Error flag anymore. But I still has no data retention, FLASH stays blank. Have you had similar problem?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 08 Jul 2010 02:00:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5212-Problem-writing-flash-via-EZPort/m-p/183522#M7591</guid>
      <dc:creator>Jetoleg</dc:creator>
      <dc:date>2010-07-08T02:00:20Z</dc:date>
    </item>
  </channel>
</rss>