<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic M54455EVB Coldfire development kit - can't find much information in ColdFire/68K Microcontrollers and Processors</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/M54455EVB-Coldfire-development-kit-can-t-find-much-information/m-p/180503#M7333</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm starting to play with a MCF5445x development kit, in order to get familiar with the V4 Coldfire parts. This box comes loaded up with an embedded Linux that you can start from a terminal hooked to one of the serial ports, and through one of the ethernet ports you can run a small web server.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Digging through the information that came with the kit, on the Freescale web pages, and on this forum I 'm not really finding much information. There are a few application notes that pretty much deal with specific hardware issues with the kit, but I can't find any code examples or tutorials. I have the kit up and running, and in Codewarrior can "see the hardware" via the built in USB multilink.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there some place that I've missed that has the source code for what is running in the box, or some example code, so that I can modify or enhance the native code using the delivered Codewarrior? For a moment I thought that the intent of the kit was just for embedded Linux development, but then I asked myself, "if that was the case, why deliver Codewarrior with it?" Any ideas will be appreciated.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you in advance. Regards, Allan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 12 May 2009 20:28:58 GMT</pubDate>
    <dc:creator>MountRitter</dc:creator>
    <dc:date>2009-05-12T20:28:58Z</dc:date>
    <item>
      <title>M54455EVB Coldfire development kit - can't find much information</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/M54455EVB-Coldfire-development-kit-can-t-find-much-information/m-p/180503#M7333</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm starting to play with a MCF5445x development kit, in order to get familiar with the V4 Coldfire parts. This box comes loaded up with an embedded Linux that you can start from a terminal hooked to one of the serial ports, and through one of the ethernet ports you can run a small web server.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Digging through the information that came with the kit, on the Freescale web pages, and on this forum I 'm not really finding much information. There are a few application notes that pretty much deal with specific hardware issues with the kit, but I can't find any code examples or tutorials. I have the kit up and running, and in Codewarrior can "see the hardware" via the built in USB multilink.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there some place that I've missed that has the source code for what is running in the box, or some example code, so that I can modify or enhance the native code using the delivered Codewarrior? For a moment I thought that the intent of the kit was just for embedded Linux development, but then I asked myself, "if that was the case, why deliver Codewarrior with it?" Any ideas will be appreciated.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you in advance. Regards, Allan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 May 2009 20:28:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/M54455EVB-Coldfire-development-kit-can-t-find-much-information/m-p/180503#M7333</guid>
      <dc:creator>MountRitter</dc:creator>
      <dc:date>2009-05-12T20:28:58Z</dc:date>
    </item>
    <item>
      <title>Re: M54455EVB Coldfire development kit - can't find much information</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/M54455EVB-Coldfire-development-kit-can-t-find-much-information/m-p/180504#M7334</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I don't know if you could find the information that you request. I have the same problem, I can't find useful information about ColdFire V4 MCF5445. I hope that anybody can help me to find information about how to use well&amp;nbsp;the plattform. Also I don't know if I can work with a Linux distribution as Ubuntu or other ones. Please I need help.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 Jun 2010 08:36:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/M54455EVB-Coldfire-development-kit-can-t-find-much-information/m-p/180504#M7334</guid>
      <dc:creator>nestor_pb</dc:creator>
      <dc:date>2010-06-11T08:36:21Z</dc:date>
    </item>
    <item>
      <title>Re: M54455EVB Coldfire development kit - can't find much information</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/M54455EVB-Coldfire-development-kit-can-t-find-much-information/m-p/180505#M7335</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Guys,&lt;/P&gt;&lt;P&gt;The FSLMQX RTOS supports MCF54455 (and EVB specifically) if you want to use CodeWarrior on PC.&lt;/P&gt;&lt;P&gt;You can download and get info at &lt;A href="http://www.freescale.com/mqx" rel="nofollow" target="_blank"&gt;http://www.freescale.com/mqx&lt;/A&gt; .&lt;/P&gt;&lt;P&gt;Always install CodeWarrior first.....then FSLMQX.&lt;/P&gt;&lt;P&gt;As FYI...CodeWarrior will build a simple "Hello World" project for the M54455EVB and can be a good starting point for your application.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;David&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Jun 2010 05:10:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/M54455EVB-Coldfire-development-kit-can-t-find-much-information/m-p/180505#M7335</guid>
      <dc:creator>DavidS</dc:creator>
      <dc:date>2010-06-16T05:10:55Z</dc:date>
    </item>
  </channel>
</rss>