<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Disable PST/DDATA signals on MCF5274 in ColdFire/68K Microcontrollers and Processors</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Disable-PST-DDATA-signals-on-MCF5274/m-p/179667#M7262</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;PDDPAR and DDRDD registers to output GPIO. Should do what you want.&lt;/P&gt;&lt;P&gt;(didnt check the 527x manual, i'm only used to 521xx-525xx)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 12 May 2009 23:47:26 GMT</pubDate>
    <dc:creator>MrBean</dc:creator>
    <dc:date>2009-05-12T23:47:26Z</dc:date>
    <item>
      <title>Disable PST/DDATA signals on MCF5274</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Disable-PST-DDATA-signals-on-MCF5274/m-p/179666#M7261</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am trying to disable the PST and DDATA BDM signals on an MCF5274. This is to reduce emissions.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The manual states that setting the PSTEN bit in CCR to '0' will disable these signals. The problem is that it does not work for me. This bit is always '0' no matter what I write to it and the signals are still active.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there something special I have to do in order to read and write this bit? (The CPU is in supervisor mode).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Anders&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 08 May 2009 22:36:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Disable-PST-DDATA-signals-on-MCF5274/m-p/179666#M7261</guid>
      <dc:creator>anej</dc:creator>
      <dc:date>2009-05-08T22:36:58Z</dc:date>
    </item>
    <item>
      <title>Re: Disable PST/DDATA signals on MCF5274</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Disable-PST-DDATA-signals-on-MCF5274/m-p/179667#M7262</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;PDDPAR and DDRDD registers to output GPIO. Should do what you want.&lt;/P&gt;&lt;P&gt;(didnt check the 527x manual, i'm only used to 521xx-525xx)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 May 2009 23:47:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Disable-PST-DDATA-signals-on-MCF5274/m-p/179667#M7262</guid>
      <dc:creator>MrBean</dc:creator>
      <dc:date>2009-05-12T23:47:26Z</dc:date>
    </item>
    <item>
      <title>Re: Disable PST/DDATA signals on MCF5274</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Disable-PST-DDATA-signals-on-MCF5274/m-p/179668#M7263</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;This is not possible on MCF5274/MCF5275. The pins in question are not configurable as GPIO. The only way to disable the pins is using the CCR register but I can not get it to work as expected.&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 May 2009 20:41:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Disable-PST-DDATA-signals-on-MCF5274/m-p/179668#M7263</guid>
      <dc:creator>anej</dc:creator>
      <dc:date>2009-05-13T20:41:00Z</dc:date>
    </item>
    <item>
      <title>Re: Disable PST/DDATA signals on MCF5274</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Disable-PST-DDATA-signals-on-MCF5274/m-p/179669#M7264</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You can't disable the PST signals on this part using that register&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If your concern is EMI, switch to JTAG mode as a workaround (JTAGEN)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 May 2009 01:43:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Disable-PST-DDATA-signals-on-MCF5274/m-p/179669#M7264</guid>
      <dc:creator>PaoloRenzo</dc:creator>
      <dc:date>2009-05-14T01:43:28Z</dc:date>
    </item>
    <item>
      <title>Re: Disable PST/DDATA signals on MCF5274</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Disable-PST-DDATA-signals-on-MCF5274/m-p/179670#M7265</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp;register should be something like this&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 May 2009 01:57:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Disable-PST-DDATA-signals-on-MCF5274/m-p/179670#M7265</guid>
      <dc:creator>PaoloRenzo</dc:creator>
      <dc:date>2009-05-14T01:57:32Z</dc:date>
    </item>
    <item>
      <title>Re: Disable PST/DDATA signals on MCF5274</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Disable-PST-DDATA-signals-on-MCF5274/m-p/179671#M7266</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Where can I find the manual or errata that shows this?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;/Anders&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 May 2009 13:46:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Disable-PST-DDATA-signals-on-MCF5274/m-p/179671#M7266</guid>
      <dc:creator>anej</dc:creator>
      <dc:date>2009-05-14T13:46:44Z</dc:date>
    </item>
    <item>
      <title>Re: Disable PST/DDATA signals on MCF5274</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Disable-PST-DDATA-signals-on-MCF5274/m-p/179672#M7267</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Will update errata manual.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Sorry for the inconveniences this might caused to you&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 May 2009 21:30:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Disable-PST-DDATA-signals-on-MCF5274/m-p/179672#M7267</guid>
      <dc:creator>PaoloRenzo</dc:creator>
      <dc:date>2009-05-14T21:30:18Z</dc:date>
    </item>
    <item>
      <title>Re: Disable PST/DDATA signals on MCF5274</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Disable-PST-DDATA-signals-on-MCF5274/m-p/179673#M7268</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN class="j-post-author"&gt;&lt;STRONG&gt;&lt;A href="https://community.nxp.com/people/PaoloRenzo"&gt;PaoloRenzo&lt;/A&gt;&lt;/STRONG&gt;&lt;/SPAN&gt; wrote (4 years ago):&lt;/P&gt;&lt;P&gt;&amp;gt; Will update errata manual.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can't see any updated manuals or errata for that chip.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm having similar problems with the MCF5235. I can't set the PSTEN pin in the CCR, so I'm suspecting it might have the same problems as the MCF5274.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does anyone know?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 Jul 2013 04:30:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Disable-PST-DDATA-signals-on-MCF5274/m-p/179673#M7268</guid>
      <dc:creator>TomE</dc:creator>
      <dc:date>2013-07-15T04:30:04Z</dc:date>
    </item>
  </channel>
</rss>