<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>ColdFire/68K Microcontrollers and ProcessorsのトピックRe: Confused about internal pull-ups/pull-downs on 5223x family</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Confused-about-internal-pull-ups-pull-downs-on-5223x-family/m-p/178748#M7190</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;P class="MsoNormal"&gt;You are correct in all statements. There are a couple of things to think about though:&lt;BR /&gt;1) These are very weak pull devices - basically very small current sources equivalent to about 50K ohm. This is important for signals like RSTIN, which typ you want a nice edge on.&lt;BR /&gt;2) Redundancy, while external resistors are not required, it is suggest that at least for a critical signals - RSTIN, RCON, etc they be use for redundancy, if external fails you have the internal. etc.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 12 Jan 2008 04:40:22 GMT</pubDate>
    <dc:creator>DrSeuss</dc:creator>
    <dc:date>2008-01-12T04:40:22Z</dc:date>
    <item>
      <title>Confused about internal pull-ups/pull-downs on 5223x family</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Confused-about-internal-pull-ups-pull-downs-on-5223x-family/m-p/178747#M7189</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;I've read the MCF52235 ColdFire Integrated Microcontroller Reference Manual from cover to cover and I'm still a bit foggy&amp;nbsp;about the meaning of the "pull-up/pull-down" column in Table 2-1.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;The column heading&amp;nbsp;cites Note 2, which says "all signals have a pull-up in gpio mode." I assume this to mean that the device unconditionally activates an internal pull-up for any multi-function pin that is operating as a gpio, but the internal pull-up is not activated for other modes unless there is an entry&amp;nbsp;in the column&amp;nbsp;that indicates otherwise. Is this correct?&lt;/DIV&gt;&lt;DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;All pins that have a gpio function are configured to operate in gpio mode upon reset, and thus all of these pins are pulled up by the internal pull-ups by default. Are the pull-ups active when reset is asserted, or only upon release of reset?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Some pins (e.g., IRQ2) indicate "pull-up" in the column and cite Note 6, which says "for primary and gpio functions only." I assume this to mean that the device activates an internal pull-up, but&amp;nbsp;only&amp;nbsp;when the pin is operating as either gpio or primary function, and in all other cases the pin has no internal pull-up. Correct?&lt;/DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;The RSTI pin indicates "pull-up" and cites Note 9, which says "RSTI has an internal pull-up resistor, ..." Based on this, I assume that the TEST and JTAG_EN&amp;nbsp;pins, which indicate "pull-down," have internal pull-downs, and thus it is not necessary to tie&amp;nbsp;them to ground or supply external pull-downs. Correct?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Similarly, RCON indicates "pull-up," which is assumed to mean that it has an internal pull-up, and thus this pin may be left disconnected to permanently disable the ezport. Correct?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 Jan 2008 02:30:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Confused-about-internal-pull-ups-pull-downs-on-5223x-family/m-p/178747#M7189</guid>
      <dc:creator>lambtron</dc:creator>
      <dc:date>2008-01-11T02:30:46Z</dc:date>
    </item>
    <item>
      <title>Re: Confused about internal pull-ups/pull-downs on 5223x family</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Confused-about-internal-pull-ups-pull-downs-on-5223x-family/m-p/178748#M7190</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;P class="MsoNormal"&gt;You are correct in all statements. There are a couple of things to think about though:&lt;BR /&gt;1) These are very weak pull devices - basically very small current sources equivalent to about 50K ohm. This is important for signals like RSTIN, which typ you want a nice edge on.&lt;BR /&gt;2) Redundancy, while external resistors are not required, it is suggest that at least for a critical signals - RSTIN, RCON, etc they be use for redundancy, if external fails you have the internal. etc.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 12 Jan 2008 04:40:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Confused-about-internal-pull-ups-pull-downs-on-5223x-family/m-p/178748#M7190</guid>
      <dc:creator>DrSeuss</dc:creator>
      <dc:date>2008-01-12T04:40:22Z</dc:date>
    </item>
  </channel>
</rss>