<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>ColdFire/68K Microcontrollers and ProcessorsのトピックMCF5211/5213 Watchdog Reset</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5211-5213-Watchdog-Reset/m-p/130048#M719</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;I would like to have&amp;nbsp;a "hard" reset whenever the watchdog times out.&lt;/DIV&gt;&lt;DIV&gt;There is a CWRI bit in the CWCR that is supposed to be used for selecting interrupt or reset whenever the watchdog times out.&amp;nbsp; If I then look into the bit descriptions of the CWRI bit I find that selecting 0 for interrupt on timeout is OK but selecting 1 states the following: "Reserved. If a one is written undetermined behaviour will result.&amp;nbsp; Note: If a core reset is required, the watchdog interrupt should set the soft reset bit in the interrupt controller."&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Has anyone had any success with this approach or is there another way to get the reset of the micro upon watchdog timeout??&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Thanks,&lt;/DIV&gt;&lt;DIV&gt;NM&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 10 Apr 2007 01:43:13 GMT</pubDate>
    <dc:creator>foreigner</dc:creator>
    <dc:date>2007-04-10T01:43:13Z</dc:date>
    <item>
      <title>MCF5211/5213 Watchdog Reset</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5211-5213-Watchdog-Reset/m-p/130048#M719</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;I would like to have&amp;nbsp;a "hard" reset whenever the watchdog times out.&lt;/DIV&gt;&lt;DIV&gt;There is a CWRI bit in the CWCR that is supposed to be used for selecting interrupt or reset whenever the watchdog times out.&amp;nbsp; If I then look into the bit descriptions of the CWRI bit I find that selecting 0 for interrupt on timeout is OK but selecting 1 states the following: "Reserved. If a one is written undetermined behaviour will result.&amp;nbsp; Note: If a core reset is required, the watchdog interrupt should set the soft reset bit in the interrupt controller."&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Has anyone had any success with this approach or is there another way to get the reset of the micro upon watchdog timeout??&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Thanks,&lt;/DIV&gt;&lt;DIV&gt;NM&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Apr 2007 01:43:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5211-5213-Watchdog-Reset/m-p/130048#M719</guid>
      <dc:creator>foreigner</dc:creator>
      <dc:date>2007-04-10T01:43:13Z</dc:date>
    </item>
    <item>
      <title>Re: MCF5211/5213 Watchdog Reset</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5211-5213-Watchdog-Reset/m-p/130049#M720</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;Hi&lt;BR /&gt;&lt;BR /&gt;I think this is a documentation error. Earlier ColdFire processors could be reset by the Core Watchdog Timer, but this is not available for later processors.&lt;BR /&gt;&lt;BR /&gt;An alternative is to force a reset by writing to the Reset Control Register (RCR) in the Reset Controller Module. You could do this from the interrupt handler of the CWT.&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;Cheers&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;Simon&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Apr 2007 16:42:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5211-5213-Watchdog-Reset/m-p/130049#M720</guid>
      <dc:creator>SimonMarsden_de</dc:creator>
      <dc:date>2007-04-11T16:42:26Z</dc:date>
    </item>
    <item>
      <title>Re: MCF5211/5213 Watchdog Reset</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5211-5213-Watchdog-Reset/m-p/130050#M721</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Thanks for the info Simon!&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I can do it that way, I'm just not sure how well this would work if the program somehow "got lost".&amp;nbsp; Will it still get the correct vector for the interrupt and so on?&amp;nbsp; I know this is not anything that commonly happens but that's kind of the idea for a watchdog right?&lt;/DIV&gt;&lt;DIV&gt;I guess an external watchdog is always an option.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Thanks,&lt;/DIV&gt;&lt;DIV&gt;Nick&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Apr 2007 19:13:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5211-5213-Watchdog-Reset/m-p/130050#M721</guid>
      <dc:creator>foreigner</dc:creator>
      <dc:date>2007-04-11T19:13:49Z</dc:date>
    </item>
  </channel>
</rss>