<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>ColdFire/68K Microcontrollers and ProcessorsのトピックRe: 5329EVB, LTIB and Kernel panics?</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/5329EVB-LTIB-and-Kernel-panics/m-p/178718#M7188</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;BR /&gt;&amp;gt; I'm not familiar with the utility you suggested, can you flesh this out a bit?&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;m68k-uclinux-objdump is part of the gnu toolchain.&amp;nbsp; Documentation&lt;BR /&gt;on the standard objdump should help you understand most of the&lt;BR /&gt;options.&amp;nbsp; I believe "man objdump" should work.&lt;BR /&gt;&lt;BR /&gt;&amp;gt; Where is the utility located?&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;It's located in the toolchain.&amp;nbsp; For this bsp the toolchain installs at:&lt;BR /&gt;/opt/freescale/usr/local/gcc-4.2.47-uclibc-0.9.47/m68k-uclinux/bin/&lt;BR /&gt;&lt;BR /&gt;&amp;gt; I'm assuming I'm running this against my kernel image on my host, yes?&amp;nbsp; And that&lt;BR /&gt;&amp;gt; would be image.bin for me, not vmlinux, since I'm building a romfs flash image?&lt;BR /&gt;&lt;BR /&gt;Yes, you would run objdump against your built kernel on the host.&amp;nbsp; The&lt;BR /&gt;image.bin is just the kernel binary+romfs.img cat'd together.&amp;nbsp; Since the&lt;BR /&gt;problem is causing the kernel to crash you can look at the elf kernel that&lt;BR /&gt;is still on your host and get an idea of where it's failing.&amp;nbsp; Using the objdump&lt;BR /&gt;command you can see the kernel assembly code as it lays out in memory&lt;BR /&gt;starting at location 0x40020000 (this part of the image never changes, the&lt;BR /&gt;kernel will always be at this memory location).&amp;nbsp; There is a copy of the&lt;BR /&gt;kernel elf file located at &amp;lt;ltib&amp;gt;/rootfs/boot/vmlinux after a build.&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 11 Jan 2008 05:26:12 GMT</pubDate>
    <dc:creator>mwaddel</dc:creator>
    <dc:date>2008-01-11T05:26:12Z</dc:date>
    <item>
      <title>5329EVB, LTIB and Kernel panics?</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/5329EVB-LTIB-and-Kernel-panics/m-p/178713#M7183</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Anyone else getting spurious kernel panics with the 5329 and the latest LTIB?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;By 'spurious',&amp;nbsp; I mean that the board is just sitting there with the busybox prompt, I'm off doing something else, and I come back and the board has locked with a kernel panic.&amp;nbsp; Networking is turned off in LTIB as far as I can tell, and I'm not running any user programs.&amp;nbsp;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;This has happened 4-6 times with several different kernel configurations, including one that was based on the LTIB defaults minus microwindows, mp3play and play.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;John&lt;/SPAN&gt;&lt;BR /&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 Jan 2008 01:48:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/5329EVB-LTIB-and-Kernel-panics/m-p/178713#M7183</guid>
      <dc:creator>jpa</dc:creator>
      <dc:date>2008-01-11T01:48:46Z</dc:date>
    </item>
    <item>
      <title>Re: 5329EVB, LTIB and Kernel panics?</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/5329EVB-LTIB-and-Kernel-panics/m-p/178714#M7184</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;I didn't see behavior like that during development and I did leave it&lt;BR /&gt;running overnight on many occasions.&amp;nbsp; Any clues from the kernel&lt;BR /&gt;panic dump as to which area is causing the crash?&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;You can use "m68k-uclinux-objdump -d vmlinux | less" and search&lt;BR /&gt;through the disassembled kernel for the sequence that's causing&lt;BR /&gt;the problem.&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 Jan 2008 02:29:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/5329EVB-LTIB-and-Kernel-panics/m-p/178714#M7184</guid>
      <dc:creator>mwaddel</dc:creator>
      <dc:date>2008-01-11T02:29:37Z</dc:date>
    </item>
    <item>
      <title>Re: 5329EVB, LTIB and Kernel panics?</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/5329EVB-LTIB-and-Kernel-panics/m-p/178715#M7185</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;The board was kind enough to cooperate and repeat itself...&lt;BR /&gt;&lt;BR /&gt;# *** ILLEGAL INSTRUCTION ***&amp;nbsp;&amp;nbsp; FORMAT=4&lt;BR /&gt;Current process id is 0&lt;BR /&gt;BAD KERNEL TRAP: 00000000&lt;BR /&gt;PC: [&amp;lt;4001fcf4&amp;gt;]&lt;BR /&gt;SR: 2200&amp;nbsp; SP: 40208ed8&amp;nbsp; a2: 406a2360&lt;BR /&gt;d0: 00000000&amp;nbsp;&amp;nbsp;&amp;nbsp; d1: 00000100&amp;nbsp;&amp;nbsp;&amp;nbsp; d2: 00000000&amp;nbsp;&amp;nbsp;&amp;nbsp; d3: 00000000&lt;BR /&gt;d4: 00000068&amp;nbsp;&amp;nbsp;&amp;nbsp; d5: 02000000&amp;nbsp;&amp;nbsp;&amp;nbsp; a0: fc030000&amp;nbsp;&amp;nbsp;&amp;nbsp; a1: 401f284a&lt;BR /&gt;Process swapper (pid: 0, stackpage=401f384a)&lt;BR /&gt;Stack from 40208f0c:&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 40002000 40103d22 00000000 00000000 00000068 00000000 00000000 00000000&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 4069a640 4004224c 40042ce2 40027fa8 40208ff8 406a202a fc030000 4004227c&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 00000068 406a2000 00000068 4069a640 00000000 401f6108 40042336 00000068&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 4069a640 00000000 00000000 401ae4b0 402196fb 400ceab4 40020992 00000068&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 00000000 40023b3a 00000068 40208f9c 4021a820 00000000 00000000 00000000&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 00000000 40208008 401f284a 401ae4b0 00000000 ffffffff 00000000 41a02000&lt;BR /&gt;Call Trace:&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; [&amp;lt;40020a84&amp;gt;] [&amp;lt;40020bb4&amp;gt;] [&amp;lt;400200e2&amp;gt;]&lt;BR /&gt;Kernel panic - not syncing: Aiee, killing interrupt handler!&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 Jan 2008 03:20:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/5329EVB-LTIB-and-Kernel-panics/m-p/178715#M7185</guid>
      <dc:creator>jpa</dc:creator>
      <dc:date>2008-01-11T03:20:34Z</dc:date>
    </item>
    <item>
      <title>Re: 5329EVB, LTIB and Kernel panics?</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/5329EVB-LTIB-and-Kernel-panics/m-p/178716#M7186</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Well, if my kernel addresses are the same as your's then it's crashing in&lt;BR /&gt;the _exit routine.&amp;nbsp; Looks like it's trying to jump back to the bootloader area&lt;BR /&gt;(0x4001fcf4), all the kernel code is in 0x40020000+.&amp;nbsp; Something could be&lt;BR /&gt;corrupting the stack or stepping on a register???&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 Jan 2008 04:02:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/5329EVB-LTIB-and-Kernel-panics/m-p/178716#M7186</guid>
      <dc:creator>mwaddel</dc:creator>
      <dc:date>2008-01-11T04:02:48Z</dc:date>
    </item>
    <item>
      <title>Re: 5329EVB, LTIB and Kernel panics?</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/5329EVB-LTIB-and-Kernel-panics/m-p/178717#M7187</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;I'm not familiar with the utility you suggested, can you flesh this out a bit?&amp;nbsp; Where is the utility located?&amp;nbsp; I'm assuming I'm running this against my kernel image on my host, yes?&amp;nbsp; And that would be image.bin for me, not vmlinux, since I'm building a romfs flash image?&lt;BR /&gt;&lt;BR /&gt;For what it's worth, I'm beginning to wonder if the kernel panic isn't related to my problems with USB hubs.&amp;nbsp; It's too early to tell, but the board seems suspiciously stable now that I've unplugged the hub so I can try other things.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;At the time of the panic, it was just sitting at a busybox prompt.&amp;nbsp; Would it be helpful to see a list of active processes from ps ?&lt;BR /&gt;&lt;BR /&gt;John&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 Jan 2008 04:29:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/5329EVB-LTIB-and-Kernel-panics/m-p/178717#M7187</guid>
      <dc:creator>jpa</dc:creator>
      <dc:date>2008-01-11T04:29:18Z</dc:date>
    </item>
    <item>
      <title>Re: 5329EVB, LTIB and Kernel panics?</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/5329EVB-LTIB-and-Kernel-panics/m-p/178718#M7188</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;BR /&gt;&amp;gt; I'm not familiar with the utility you suggested, can you flesh this out a bit?&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;m68k-uclinux-objdump is part of the gnu toolchain.&amp;nbsp; Documentation&lt;BR /&gt;on the standard objdump should help you understand most of the&lt;BR /&gt;options.&amp;nbsp; I believe "man objdump" should work.&lt;BR /&gt;&lt;BR /&gt;&amp;gt; Where is the utility located?&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;It's located in the toolchain.&amp;nbsp; For this bsp the toolchain installs at:&lt;BR /&gt;/opt/freescale/usr/local/gcc-4.2.47-uclibc-0.9.47/m68k-uclinux/bin/&lt;BR /&gt;&lt;BR /&gt;&amp;gt; I'm assuming I'm running this against my kernel image on my host, yes?&amp;nbsp; And that&lt;BR /&gt;&amp;gt; would be image.bin for me, not vmlinux, since I'm building a romfs flash image?&lt;BR /&gt;&lt;BR /&gt;Yes, you would run objdump against your built kernel on the host.&amp;nbsp; The&lt;BR /&gt;image.bin is just the kernel binary+romfs.img cat'd together.&amp;nbsp; Since the&lt;BR /&gt;problem is causing the kernel to crash you can look at the elf kernel that&lt;BR /&gt;is still on your host and get an idea of where it's failing.&amp;nbsp; Using the objdump&lt;BR /&gt;command you can see the kernel assembly code as it lays out in memory&lt;BR /&gt;starting at location 0x40020000 (this part of the image never changes, the&lt;BR /&gt;kernel will always be at this memory location).&amp;nbsp; There is a copy of the&lt;BR /&gt;kernel elf file located at &amp;lt;ltib&amp;gt;/rootfs/boot/vmlinux after a build.&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 Jan 2008 05:26:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/5329EVB-LTIB-and-Kernel-panics/m-p/178718#M7188</guid>
      <dc:creator>mwaddel</dc:creator>
      <dc:date>2008-01-11T05:26:12Z</dc:date>
    </item>
  </channel>
</rss>