<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>ColdFire/68K Microcontrollers and Processors中的主题 Re: M52259 Can it flash itself</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/M52259-Can-it-flash-itself/m-p/178400#M7149</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Also take a look at the uTasker proejct for the Coldfire V2 (including M5225X) &lt;A href="http://www.utasker.com/kirin3.html" rel="nofollow" target="_self"&gt;http://www.utasker.com/kirin3.html&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;It includes loading via Ethernet (FTP, HTTP POST and TFTP), USB and UART, with optional encryption support:&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.utasker.com/docs/uTasker/uTaskerBoot_003.PDF" rel="nofollow" target="_self"&gt;http://www.utasker.com/docs/uTasker/uTaskerBoot_003.PDF&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.utasker.com/docs/M5223X/uTaskerV1.3_Kirin3_demo.PDF" rel="nofollow" target="_self"&gt;http://www.utasker.com/docs/M5223X/uTaskerV1.3_Kirin3_demo.PDF&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.utasker.com/docs/uTasker/uTaskerSerialLoader.PDF" rel="nofollow" target="_self"&gt;http://www.utasker.com/docs/uTasker/uTaskerSerialLoader.PDF&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 24 Feb 2010 06:45:24 GMT</pubDate>
    <dc:creator>mjbcswitzerland</dc:creator>
    <dc:date>2010-02-24T06:45:24Z</dc:date>
    <item>
      <title>M52259 Can it flash itself</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/M52259-Can-it-flash-itself/m-p/178398#M7147</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am currently working with M52259demo board and I have a question.&lt;/P&gt;&lt;P&gt;Can M52259 flash itself?&lt;/P&gt;&lt;P&gt;If I loading new program via Ethernet or USB, can I update the program to flash?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Feb 2010 16:52:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/M52259-Can-it-flash-itself/m-p/178398#M7147</guid>
      <dc:creator>epl</dc:creator>
      <dc:date>2010-02-23T16:52:42Z</dc:date>
    </item>
    <item>
      <title>Re: M52259 Can it flash itself</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/M52259-Can-it-flash-itself/m-p/178399#M7148</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;HR /&gt;epl wrote:&lt;BR /&gt;&lt;P&gt;Can M52259 flash itself?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;HR /&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;Yes, it can.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;HR /&gt;epl wrote:&lt;BR /&gt;&lt;P&gt;If I loading new program via Ethernet or USB, can I update the program to flash?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;HR /&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;Of course you can, provided the firmware implements such functionality.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Feb 2010 17:27:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/M52259-Can-it-flash-itself/m-p/178399#M7148</guid>
      <dc:creator>scifi</dc:creator>
      <dc:date>2010-02-23T17:27:11Z</dc:date>
    </item>
    <item>
      <title>Re: M52259 Can it flash itself</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/M52259-Can-it-flash-itself/m-p/178400#M7149</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Also take a look at the uTasker proejct for the Coldfire V2 (including M5225X) &lt;A href="http://www.utasker.com/kirin3.html" rel="nofollow" target="_self"&gt;http://www.utasker.com/kirin3.html&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;It includes loading via Ethernet (FTP, HTTP POST and TFTP), USB and UART, with optional encryption support:&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.utasker.com/docs/uTasker/uTaskerBoot_003.PDF" rel="nofollow" target="_self"&gt;http://www.utasker.com/docs/uTasker/uTaskerBoot_003.PDF&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.utasker.com/docs/M5223X/uTaskerV1.3_Kirin3_demo.PDF" rel="nofollow" target="_self"&gt;http://www.utasker.com/docs/M5223X/uTaskerV1.3_Kirin3_demo.PDF&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.utasker.com/docs/uTasker/uTaskerSerialLoader.PDF" rel="nofollow" target="_self"&gt;http://www.utasker.com/docs/uTasker/uTaskerSerialLoader.PDF&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Feb 2010 06:45:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/M52259-Can-it-flash-itself/m-p/178400#M7149</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2010-02-24T06:45:24Z</dc:date>
    </item>
    <item>
      <title>Re: M52259 Can it flash itself</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/M52259-Can-it-flash-itself/m-p/178401#M7150</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using MQX on a 52259 board and have developped the required software to update the MQX image running in internal flash flash from MQX itself, using only C code.&lt;/P&gt;&lt;P&gt;The new image is download through FTP or serial line while the system is running&lt;/P&gt;&lt;P&gt;Tthen a command is run to update : the flash image is updated and the board is restarted; this takes only 3 seconds.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I post some tips on that in the thread named "Building a relocatable C program that can be run out of SRAM in MQX"&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.freescale.com/message/73480#73480" title="https://community.freescale.com/message/73480#73480"&gt;https://community.freescale.com/message/73480#73480&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I guess the tips also apply to non MQX software.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Mar 2011 07:38:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/M52259-Can-it-flash-itself/m-p/178401#M7150</guid>
      <dc:creator>trailman</dc:creator>
      <dc:date>2011-03-02T07:38:32Z</dc:date>
    </item>
    <item>
      <title>Re: M52259 Can it flash itself</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/M52259-Can-it-flash-itself/m-p/178402#M7151</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;U-Boot also has support for this, but it may be overkill for your project:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.denx.de/wiki/U-Boot" rel="nofollow" target="_blank"&gt;http://www.denx.de/wiki/U-Boot&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;It is also a lot of work to port to your CPU and your development board (then your working board) if someone hasn't done so already. There's support for "MCF5227x" in there.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Tom&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Mar 2011 07:40:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/M52259-Can-it-flash-itself/m-p/178402#M7151</guid>
      <dc:creator>TomE</dc:creator>
      <dc:date>2011-03-03T07:40:03Z</dc:date>
    </item>
    <item>
      <title>Re: M52259 Can it flash itself</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/M52259-Can-it-flash-itself/m-p/178403#M7152</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using the MCF52255 in a project, and I need to be able to save and change a few calibration constants in flash from time to time. Is there an easy way to do this, or would I have to hack boot loader code?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Your help would be appreciated.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Apr 2012 21:33:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/M52259-Can-it-flash-itself/m-p/178403#M7152</guid>
      <dc:creator>trusc</dc:creator>
      <dc:date>2012-04-18T21:33:14Z</dc:date>
    </item>
    <item>
      <title>Re: M52259 Can it flash itself</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/M52259-Can-it-flash-itself/m-p/178404#M7153</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;What you need is a "Flash Driver". That's a module that knows how to erase and write to the FLASH in your particular chip.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If U-Boot can write to the FLASH in that chip, then there should be a small number of files that you should be able to reuse to do the same thing.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Doesn't CodeWarrior or the Processor Expert come with this, or come with code samples that do this?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;We wrote our own (for external Spansion FLASH on an MCF5329) but that doesn't mean you should have to.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Tom&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Apr 2012 11:30:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/M52259-Can-it-flash-itself/m-p/178404#M7153</guid>
      <dc:creator>TomE</dc:creator>
      <dc:date>2012-04-19T11:30:22Z</dc:date>
    </item>
    <item>
      <title>Re: M52259 Can it flash itself</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/M52259-Can-it-flash-itself/m-p/178405#M7154</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Tom&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for pointing me in the right direction. I'll look into that.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Chris&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Apr 2012 13:08:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/M52259-Can-it-flash-itself/m-p/178405#M7154</guid>
      <dc:creator>trusc</dc:creator>
      <dc:date>2012-04-19T13:08:53Z</dc:date>
    </item>
  </channel>
</rss>