<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>ColdFire/68K Microcontrollers and ProcessorsのトピックRe: CF51JM not reliable at full PLL speed</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/CF51JM-not-reliable-at-full-PLL-speed/m-p/177477#M7044</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Well FWIW, I use that part at 48Mhz with no issues.&lt;/P&gt;&lt;P&gt;The clock fail is to detect manufacuring issues.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;PRE&gt;/* * Enable the 12Mhz xtal oscillator and use the PLL * to crank it up to 48MHz. */void InitCLOCK12MHZ(void){ long counter = 0; // See chapter 7 of MCF51JMRM.pdf  // to completely understand this. // First start the 12 MHz XTAL oscillator up. // Set BDIV=0 RANGE=1,HGO=1,EREFS=1,ERCLKEN=1 MCGC2 = 0x36;    // Wait for the osc to start up. while(MCGSC_OSCINIT == 0 &amp;amp;&amp;amp; counter++ &amp;lt; 10000)   ; if(counter &amp;gt; 10000) {  OSCILLATOR_Fail = 1;  return; } // Select the external ref clock (the 12 MHz oscillator). // set RDIV to divide by 8 - 12/8 = 1.5 MHz to feed the PLL // CLKS=10 RDIV=3 See 7.3.1 // Also, enable the internal 32k ref clock so RTC can use it. MCGC1 = 0x98 | MCGC1_IRCLKEN_MASK ;  // Wait for bit 3 to set and bit 2 to reset to indicate // external reference is selected. while((MCGSC &amp;amp; 0xC) != 0x8)  ;  // Select the PLL with a x32 multiplier to give 48MHz // PLLS=1  VDIV=8 (x32) 1.5x32=48 See Table  7.3.6 MCGC3 = 0x48;  // Wait for the PLL to be selected while(MCGSC_PLLST == 0 )  ;  // Wait for the PLL to lock. while(MCGSC_LOCK == 0)  ;  // Clear bits 6 &amp;amp; 7 to 0 to select the PLL output as the CPU clock. MCGC1 &amp;amp;= ~0xC0;  }&lt;/PRE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 29 Oct 2020 09:26:28 GMT</pubDate>
    <dc:creator>JimDon</dc:creator>
    <dc:date>2020-10-29T09:26:28Z</dc:date>
    <item>
      <title>CF51JM not reliable at full PLL speed</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/CF51JM-not-reliable-at-full-PLL-speed/m-p/177473#M7040</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am working on some prototypes of a new product,&amp;nbsp; and am getting wierd lockups and fail-to-start issues when the PLL is set to 48mhz (for a bus speed of 24).&amp;nbsp; This clock speed is required for USB to work,&amp;nbsp; so its important to determine the issue.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have tried 8 mhz and 12 mhz crystals,&amp;nbsp; and the problem is essentially unchanged.&amp;nbsp; Sometimes the CPU locks up very soon after powerup,&amp;nbsp; sometimes it will run for a while.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using CW6.3 with ProcessorExpert.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If I reduce the clock,&amp;nbsp; the symptom goes away (not sure if its truly solved,&amp;nbsp; as testing is preliminary), but this product needs USB to be functional.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there some errata on this?&amp;nbsp; Does it sound familiar to anyone?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Bob&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Oct 2011 21:50:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/CF51JM-not-reliable-at-full-PLL-speed/m-p/177473#M7040</guid>
      <dc:creator>TurboBob</dc:creator>
      <dc:date>2011-10-26T21:50:30Z</dc:date>
    </item>
    <item>
      <title>Re: CF51JM not reliable at full PLL speed</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/CF51JM-not-reliable-at-full-PLL-speed/m-p/177474#M7041</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;FLL mode works fine to full speed (alas no USB though)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;anyone had this issue?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Oct 2011 03:14:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/CF51JM-not-reliable-at-full-PLL-speed/m-p/177474#M7041</guid>
      <dc:creator>TurboBob</dc:creator>
      <dc:date>2011-10-27T03:14:00Z</dc:date>
    </item>
    <item>
      <title>Re: CF51JM not reliable at full PLL speed</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/CF51JM-not-reliable-at-full-PLL-speed/m-p/177475#M7042</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is your clock switching code following the flow charts in Chapter 7 of the Reference Manual. I think Flowchart 7.10 may apply.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Can you program an output pin to some signal related to the clock (one of the timers generating a square wave), so you can monitor any frequency excursions with an oscilloscope?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Have you checked your power supplies and bypassing? The higher frequency operation may be drawing more current.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Tom&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Oct 2011 05:29:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/CF51JM-not-reliable-at-full-PLL-speed/m-p/177475#M7042</guid>
      <dc:creator>TomE</dc:creator>
      <dc:date>2011-10-27T05:29:54Z</dc:date>
    </item>
    <item>
      <title>Re: CF51JM not reliable at full PLL speed</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/CF51JM-not-reliable-at-full-PLL-speed/m-p/177476#M7043</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I was looking at that.&amp;nbsp; The supply bypassing was a little light,&amp;nbsp; so I tacked in a .1 ceramic and a 22uf tantalum with no change in the condition.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;When running full speed from the FLL,&amp;nbsp; both internal and external,&amp;nbsp; everything runs fine.&amp;nbsp; But looking at clock stability and stuff like that makes some sense.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using Processor Expert with Codewarrior 6.3,&amp;nbsp; I have not double checked the clock switching sequence,&amp;nbsp; but all the other PLL equipped chips I have used in a bunch of other projects have been fine&amp;nbsp; (HC08AP, HCS08AW, HCS08JM).&amp;nbsp; It may be time to recheck the stuff I'm sure about though.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This is my first project with the CF,&amp;nbsp; I like the part,&amp;nbsp; but am getting worried.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for the suggestions,&amp;nbsp;&amp;nbsp; keep them coming.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Bob Bailey&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Oct 2011 11:42:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/CF51JM-not-reliable-at-full-PLL-speed/m-p/177476#M7043</guid>
      <dc:creator>TurboBob</dc:creator>
      <dc:date>2011-10-27T11:42:58Z</dc:date>
    </item>
    <item>
      <title>Re: CF51JM not reliable at full PLL speed</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/CF51JM-not-reliable-at-full-PLL-speed/m-p/177477#M7044</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Well FWIW, I use that part at 48Mhz with no issues.&lt;/P&gt;&lt;P&gt;The clock fail is to detect manufacuring issues.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;PRE&gt;/* * Enable the 12Mhz xtal oscillator and use the PLL * to crank it up to 48MHz. */void InitCLOCK12MHZ(void){ long counter = 0; // See chapter 7 of MCF51JMRM.pdf  // to completely understand this. // First start the 12 MHz XTAL oscillator up. // Set BDIV=0 RANGE=1,HGO=1,EREFS=1,ERCLKEN=1 MCGC2 = 0x36;    // Wait for the osc to start up. while(MCGSC_OSCINIT == 0 &amp;amp;&amp;amp; counter++ &amp;lt; 10000)   ; if(counter &amp;gt; 10000) {  OSCILLATOR_Fail = 1;  return; } // Select the external ref clock (the 12 MHz oscillator). // set RDIV to divide by 8 - 12/8 = 1.5 MHz to feed the PLL // CLKS=10 RDIV=3 See 7.3.1 // Also, enable the internal 32k ref clock so RTC can use it. MCGC1 = 0x98 | MCGC1_IRCLKEN_MASK ;  // Wait for bit 3 to set and bit 2 to reset to indicate // external reference is selected. while((MCGSC &amp;amp; 0xC) != 0x8)  ;  // Select the PLL with a x32 multiplier to give 48MHz // PLLS=1  VDIV=8 (x32) 1.5x32=48 See Table  7.3.6 MCGC3 = 0x48;  // Wait for the PLL to be selected while(MCGSC_PLLST == 0 )  ;  // Wait for the PLL to lock. while(MCGSC_LOCK == 0)  ;  // Clear bits 6 &amp;amp; 7 to 0 to select the PLL output as the CPU clock. MCGC1 &amp;amp;= ~0xC0;  }&lt;/PRE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Oct 2020 09:26:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/CF51JM-not-reliable-at-full-PLL-speed/m-p/177477#M7044</guid>
      <dc:creator>JimDon</dc:creator>
      <dc:date>2020-10-29T09:26:28Z</dc:date>
    </item>
    <item>
      <title>Re: CF51JM not reliable at full PLL speed</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/CF51JM-not-reliable-at-full-PLL-speed/m-p/177478#M7045</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the reply.&amp;nbsp; When I said this is my first experience with the CF,&amp;nbsp; I meant "ColdFire".&amp;nbsp; But,&amp;nbsp; this is my first PLL issue also...&amp;nbsp; &lt;IMG alt=":smileyhappy:" class="emoticon emoticon-smileyhappy" id="smileyhappy" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-happy.gif" title="Smiley Happy" /&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;When Processor Expert inits the clock,&amp;nbsp; it generates the following code.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;PRE&gt;  /*  System clock initialization */  if (*(unsigned char*)0x03FF != 0xFF) { /* Test if the device trim value is stored on the specified address */    MCGTRM = *(unsigned char*)0x03FF;  /* Initialize MCGTRM register from a non volatile memory */    MCGSC = *(unsigned char*)0x03FE;   /* Initialize MCGSC register from a non volatile memory */  }  /* MCGC2: BDIV=0,RANGE=1,HGO=1,LP=0,EREFS=1,ERCLKEN=1,EREFSTEN=0 */  setReg8(MCGC2, 0x36);                /* Set MCGC2 register */   while(!MCGSC_OSCINIT) {              /* Wait until external reference is stable */  }  /* MCGC3: DIV32=1 */  setReg8Bits(MCGC3, 0x10);               /* MCGC1: CLKS=2,RDIV=3,IREFS=0,IRCLKEN=1,IREFSTEN=0 */  setReg8(MCGC1, 0x9A);                /* Set MCGC1 register */   while(MCGSC_IREFST) {                /* Wait until external reference is selected */  }  /* MCGC3: LOLIE=1,PLLS=0,CME=0,DIV32=1,VDIV=8 */  setReg8(MCGC3, 0x98);                /* Set MCGC3 register */   /* MCGC4: ??=0,??=0,DMX32=0,??=0,??=0,??=0,DRST_DRS=0 */  setReg8(MCGC4, 0x00);                /* Set MCGC4 register */   while((MCGSC &amp;amp; 0x0C) != 0x08) {      /* Wait until external clock is selected as a bus clock reference */  }  /* MCGC2: BDIV=0,RANGE=1,HGO=1,LP=1,EREFS=1,ERCLKEN=1,EREFSTEN=0 */  setReg8(MCGC2, 0x3E);                /* Set MCGC2 register */   /* MCGC1: CLKS=2,RDIV=3,IREFS=0,IRCLKEN=1,IREFSTEN=0 */  setReg8(MCGC1, 0x9A);                /* Set MCGC1 register */   /* MCGC3: LOLIE=1,PLLS=0,CME=0,DIV32=0,VDIV=8 */  setReg8(MCGC3, 0x88);                /* Set MCGC3 register */   /* MCGC3: LOLIE=1,PLLS=1,CME=0,DIV32=0,VDIV=8 */  setReg8(MCGC3, 0xC8);                /* Set MCGC3 register */   while(!MCGSC_PLLST) {                /* Wait until PLL is selected */  }  /* MCGC2: LP=0 */  clrReg8Bits(MCGC2, 0x08);               while(!MCGSC_LOCK) {                 /* Wait until PLL is locked */  }  /* MCGC1: CLKS=0,RDIV=3,IREFS=0,IRCLKEN=1,IREFSTEN=0 */  setReg8(MCGC1, 0x1A);                /* Set MCGC1 register */   while((MCGSC &amp;amp; 0x0C) != 0x0C) {      /* Wait until PLL clock is selected as a bus clock reference */  }  /* MCGC3: CME=1 */  setReg8Bits(MCGC3, 0x20);            /* Enable Clock monitor */  &lt;/PRE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I think part of my "Lost in Space" issue may be that I had no vector for the loss of lock interrupt (the interrupt was enabled).&amp;nbsp; So I will handle that next time the unit is on the bench.&amp;nbsp; But that does not answer why it lost lock (assuming thats whats happening).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The investigation continues.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Bob&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Oct 2020 09:26:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/CF51JM-not-reliable-at-full-PLL-speed/m-p/177478#M7045</guid>
      <dc:creator>TurboBob</dc:creator>
      <dc:date>2020-10-29T09:26:30Z</dc:date>
    </item>
    <item>
      <title>Re: CF51JM not reliable at full PLL speed</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/CF51JM-not-reliable-at-full-PLL-speed/m-p/177479#M7046</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;well,&amp;nbsp; I put in a vector for the loss of lock,&amp;nbsp; and thats not where its going.&amp;nbsp; I have seen it wind up in the unhandled interrupt handler,&amp;nbsp; and it also jump out into space (PC was really high) once.&amp;nbsp; Its not very repeatable.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Trying to determine how to see the interrupt source on this part.&amp;nbsp; Some days I wish I had put in the HCS08....&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;So,&amp;nbsp; even though the symptom occurrs when running the PLL fast,&amp;nbsp; its not a lock failure thats causing this (or so it seems)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Bob&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Oct 2011 23:21:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/CF51JM-not-reliable-at-full-PLL-speed/m-p/177479#M7046</guid>
      <dc:creator>TurboBob</dc:creator>
      <dc:date>2011-10-27T23:21:28Z</dc:date>
    </item>
    <item>
      <title>Re: CF51JM not reliable at full PLL speed</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/CF51JM-not-reliable-at-full-PLL-speed/m-p/177480#M7047</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Spent a bunch of time on this,&amp;nbsp; with the symptom being intermittant.&amp;nbsp; But always there.&amp;nbsp; I loaded the software into my JM demo board and it happens there also.&amp;nbsp; So no layout / circuit issues.&amp;nbsp;&amp;nbsp; After multiple software iterations trying to track down stuff,&amp;nbsp; the symptom seemed to be getting worse,&amp;nbsp; yet the software was getting simpler.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Then,&amp;nbsp; when the software would refuse to run in 48 mhz PLL mode,&amp;nbsp; I swapped in a fresh MCU,&amp;nbsp; and its been running solid for over 24 hours in PLL mode.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The software does use the flash to save data,&amp;nbsp; and a save happens every time the software is reloaded,&amp;nbsp; as well as periodically.&amp;nbsp; So perhaps I'm breaking something with the flash routines.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I checked,&amp;nbsp; and I'm initializing the flash properly (just the FCDIV I think).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm using the AN3942 routines with a bugfix posted by Peg on the forum.&amp;nbsp; The fixed code is pasted below.&amp;nbsp; Perhaps the fix is wrong and I need to use the released code?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;PRE&gt;/*******************************************************************************/.if(MCU == MCF51_JM_QE_CN_AC)_Burst_Prog:               move.l  d0,d4               move.l  a1,a3               move.l  a0,d2               move.l  #(SpSubBurstEnd),a1               move.l  #(SpSubBurst),a6               bsr     DoOnStack                        move.l  a0,a1               moveq   #(mFSTAT_FACCERR+mFSTAT_FPVIOL),d0//;fix               move.b  #(mFSTAT_FCCF + mFSTAT_FCBEF),d0               move.b  d0,FSTAT               jsr     (A1)               rts.endif&lt;/PRE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Note the fix.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Does anyone have some feedback on this?&amp;nbsp; Are there better routines for this?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks!!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Bob&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Oct 2020 09:26:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/CF51JM-not-reliable-at-full-PLL-speed/m-p/177480#M7047</guid>
      <dc:creator>TurboBob</dc:creator>
      <dc:date>2020-10-29T09:26:32Z</dc:date>
    </item>
    <item>
      <title>Re: CF51JM not reliable at full PLL speed</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/CF51JM-not-reliable-at-full-PLL-speed/m-p/177481#M7048</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Well,&amp;nbsp; I removed the ASM flash routines and put in Flash.c and Flash.h,&amp;nbsp; which I believe are from the CF version of the badgeboard.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The new routines don't use burst mode,&amp;nbsp; but regardless,&amp;nbsp; the symptoms have subsided.&amp;nbsp; I did have to replace the CPU.&amp;nbsp; The flash array must have gotten worn out or something.&amp;nbsp; ( I saw this on several CPUs,&amp;nbsp; so it was not a defective part IMO)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I don't have any further infomation/answers&amp;nbsp; but it looks like things are working properly now.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;There is an SR in the system,&amp;nbsp; as my local FAE is working with me to see if a root cause can be determined.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Just wanted to update anyone watching the thread.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Bob&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 Nov 2011 07:08:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/CF51JM-not-reliable-at-full-PLL-speed/m-p/177481#M7048</guid>
      <dc:creator>TurboBob</dc:creator>
      <dc:date>2011-11-04T07:08:49Z</dc:date>
    </item>
    <item>
      <title>Re: CF51JM not reliable at full PLL speed</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/CF51JM-not-reliable-at-full-PLL-speed/m-p/177482#M7049</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;JimDon:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Do you write to flash in your application,&amp;nbsp; and is your application 5-volt?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Just some more thoughts.&amp;nbsp; This still bugs me.&amp;nbsp; (I'm putting a serial EEPROM on the next board layout,&amp;nbsp; anyone have some bit-bang'ed I2C code to share?)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Bob&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Jan 2012 15:36:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/CF51JM-not-reliable-at-full-PLL-speed/m-p/177482#M7049</guid>
      <dc:creator>TurboBob</dc:creator>
      <dc:date>2012-01-17T15:36:56Z</dc:date>
    </item>
    <item>
      <title>Re: CF51JM not reliable at full PLL speed</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/CF51JM-not-reliable-at-full-PLL-speed/m-p/177483#M7050</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Google finds some code in Linux distributions:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="http://comments.gmane.org/gmane.linux.uclinux.devel/5634" rel="nofollow" target="_blank"&gt;http://comments.gmane.org/gmane.linux.uclinux.devel/5634&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Tom&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Jan 2012 07:54:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/CF51JM-not-reliable-at-full-PLL-speed/m-p/177483#M7050</guid>
      <dc:creator>TomE</dc:creator>
      <dc:date>2012-01-18T07:54:22Z</dc:date>
    </item>
  </channel>
</rss>