<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MCF5445x with LTIB - static linking in ColdFire/68K Microcontrollers and Processors</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5445x-with-LTIB-static-linking/m-p/177057#M6973</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using LTIB (m54455_20071214-ltib-final.iso) and the target is MCF5445x.&amp;nbsp; Currently have an eval board that has a flash filing system complete with stdc/stdc++ shared objects.&amp;nbsp; I was looking into the options of creating a statically linked executable, so I put "-static" on the link line.&amp;nbsp; When attempting to run on the target I get illegal instruction.&amp;nbsp; If I remove "-static" it works ok.&amp;nbsp; I tried helloWorld and that didn't work either.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Anybody tried something similar?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 30 Apr 2009 14:57:46 GMT</pubDate>
    <dc:creator>DJP</dc:creator>
    <dc:date>2009-04-30T14:57:46Z</dc:date>
    <item>
      <title>MCF5445x with LTIB - static linking</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5445x-with-LTIB-static-linking/m-p/177057#M6973</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using LTIB (m54455_20071214-ltib-final.iso) and the target is MCF5445x.&amp;nbsp; Currently have an eval board that has a flash filing system complete with stdc/stdc++ shared objects.&amp;nbsp; I was looking into the options of creating a statically linked executable, so I put "-static" on the link line.&amp;nbsp; When attempting to run on the target I get illegal instruction.&amp;nbsp; If I remove "-static" it works ok.&amp;nbsp; I tried helloWorld and that didn't work either.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Anybody tried something similar?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 Apr 2009 14:57:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5445x-with-LTIB-static-linking/m-p/177057#M6973</guid>
      <dc:creator>DJP</dc:creator>
      <dc:date>2009-04-30T14:57:46Z</dc:date>
    </item>
    <item>
      <title>Re: MCF5445x with LTIB - static linking</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5445x-with-LTIB-static-linking/m-p/177058#M6974</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;This looks like&amp;nbsp;a toolchain issue reported to codesourcery with -static&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Here's the&amp;nbsp;report to CodeSourcery:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;A href="http://www.codesourcery.com/archives/coldfire-gnu-discuss/msg00620.html" rel="nofollow" target="_blank"&gt;http://www.codesourcery.com/archives/coldfire-gnu-discuss/msg00620.html&lt;/A&gt;&lt;BR /&gt;Here is the the gcc bug on gcc's bugzilla:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;A href="http://gcc.gnu.org/bugzilla/show_bug.cgi?id=36047" rel="nofollow" target="_blank"&gt;http://gcc.gnu.org/bugzilla/show_bug.cgi?id=36047&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 May 2009 03:32:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5445x-with-LTIB-static-linking/m-p/177058#M6974</guid>
      <dc:creator>fsl_linux_spt</dc:creator>
      <dc:date>2009-05-06T03:32:38Z</dc:date>
    </item>
    <item>
      <title>Re: MCF5445x with LTIB - static linking</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5445x-with-LTIB-static-linking/m-p/177059#M6975</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;thanks for that, very helpful!&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 May 2009 14:13:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5445x-with-LTIB-static-linking/m-p/177059#M6975</guid>
      <dc:creator>DJP</dc:creator>
      <dc:date>2009-05-06T14:13:11Z</dc:date>
    </item>
  </channel>
</rss>