<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: n00b Question about AN Port, GPIO and reading 8 bit words in ColdFire/68K Microcontrollers and Processors</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/n00b-Question-about-AN-Port-GPIO-and-reading-8-bit-words/m-p/176609#M6927</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;When you were saying "seven bit ports" you must have meant "eight-bit ports."&lt;/P&gt;&lt;P&gt;Yes, you can read a byte through one 8-bit port and the other byte through the other 8-bit port. You have to make sure the 16-bit word is stable while you are sampling it (the two 8-bit reads cannot be simultaneous.)&lt;/P&gt;&lt;P&gt;Otherwise, it's ok.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 17 Feb 2010 21:56:41 GMT</pubDate>
    <dc:creator>scifi</dc:creator>
    <dc:date>2010-02-17T21:56:41Z</dc:date>
    <item>
      <title>n00b Question about AN Port, GPIO and reading 8 bit words</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/n00b-Question-about-AN-Port-GPIO-and-reading-8-bit-words/m-p/176608#M6926</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;ok so i've been working with MCF52235EVB for some time now. i now want to build my own MCF52235 PCB to do some stuff. one of the things I need to do is read 16bit parallel words. so i thought i could use one port to read 8 bits MSB and another port to read 8 bits LSB.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;i read through the reference manual and see that analog port (PAN[0:7]) and the interrupt port (PGP[0:7]) are two seven bit ports. so i can set these two ports to be GPIO and digital inputs and read in the words.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;is this the right way to do this? any obvious mistakes?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Feb 2010 21:11:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/n00b-Question-about-AN-Port-GPIO-and-reading-8-bit-words/m-p/176608#M6926</guid>
      <dc:creator>jab</dc:creator>
      <dc:date>2010-02-17T21:11:17Z</dc:date>
    </item>
    <item>
      <title>Re: n00b Question about AN Port, GPIO and reading 8 bit words</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/n00b-Question-about-AN-Port-GPIO-and-reading-8-bit-words/m-p/176609#M6927</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;When you were saying "seven bit ports" you must have meant "eight-bit ports."&lt;/P&gt;&lt;P&gt;Yes, you can read a byte through one 8-bit port and the other byte through the other 8-bit port. You have to make sure the 16-bit word is stable while you are sampling it (the two 8-bit reads cannot be simultaneous.)&lt;/P&gt;&lt;P&gt;Otherwise, it's ok.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Feb 2010 21:56:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/n00b-Question-about-AN-Port-GPIO-and-reading-8-bit-words/m-p/176609#M6927</guid>
      <dc:creator>scifi</dc:creator>
      <dc:date>2010-02-17T21:56:41Z</dc:date>
    </item>
    <item>
      <title>Re: n00b Question about AN Port, GPIO and reading 8 bit words</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/n00b-Question-about-AN-Port-GPIO-and-reading-8-bit-words/m-p/176610#M6928</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;eight bits yes, thanks &lt;IMG alt=":smileyhappy:" class="emoticon emoticon-smileyhappy" id="smileyhappy" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-happy.gif" title="Smiley Happy" /&gt; .&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Feb 2010 15:01:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/n00b-Question-about-AN-Port-GPIO-and-reading-8-bit-words/m-p/176610#M6928</guid>
      <dc:creator>jab</dc:creator>
      <dc:date>2010-02-18T15:01:14Z</dc:date>
    </item>
  </channel>
</rss>