<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>ColdFire/68K Microcontrollers and ProcessorsのトピックRe: Digital  2 wire 4-20mA conversion to voltage modulated signal</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Digital-2-wire-4-20mA-conversion-to-voltage-modulated-signal/m-p/173341#M6583</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Surely with the correct resistor values you should be able to do it on a normal digital IO pin?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 11 Oct 2011 18:37:09 GMT</pubDate>
    <dc:creator>FridgeFreezer</dc:creator>
    <dc:date>2011-10-11T18:37:09Z</dc:date>
    <item>
      <title>Digital  2 wire 4-20mA conversion to voltage modulated signal</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Digital-2-wire-4-20mA-conversion-to-voltage-modulated-signal/m-p/173340#M6582</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I need to use a digital single axis accelerometer with capacity to go up to a few hundred g's.&amp;nbsp; The only decent ones I've been able to get hold of are the ADXL180's from ADI.&amp;nbsp; However my project is using the MCF51JM128 so I need to find a way to interface with the device as it uses a 2 wire digital 4-20mA interface.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Now from what I've read I can use a precision resistor and sample the voltage across the resistor through the ADC but then I must do a bunch of programming to convert that into something useful.&amp;nbsp; I don't mind doing the work but I want to know if there is a better solution then bit banging a comms interface.&amp;nbsp; Are there any IC's out there that convert it to a standard interface like SCI/SPI/I2C?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in Advance&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Dave Wright&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Oct 2011 22:26:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Digital-2-wire-4-20mA-conversion-to-voltage-modulated-signal/m-p/173340#M6582</guid>
      <dc:creator>Dave_W</dc:creator>
      <dc:date>2011-10-10T22:26:49Z</dc:date>
    </item>
    <item>
      <title>Re: Digital  2 wire 4-20mA conversion to voltage modulated signal</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Digital-2-wire-4-20mA-conversion-to-voltage-modulated-signal/m-p/173341#M6583</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Surely with the correct resistor values you should be able to do it on a normal digital IO pin?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Oct 2011 18:37:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Digital-2-wire-4-20mA-conversion-to-voltage-modulated-signal/m-p/173341#M6583</guid>
      <dc:creator>FridgeFreezer</dc:creator>
      <dc:date>2011-10-11T18:37:09Z</dc:date>
    </item>
  </channel>
</rss>