<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Using DDR2 memory with coldfire 54450 processor in ColdFire/68K Microcontrollers and Processors</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Using-DDR2-memory-with-coldfire-54450-processor/m-p/173003#M6553</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;I would like to use DDR2 memory with the MCF54450 processor which has an in built DDR memory controller.&amp;nbsp; The 5445x datasheet specifies that the 54450 and 51 devices can only run up to a maximum of 240MHz, giving a bus clock maximum of 120MHz.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;DDR2 memory requires a bus clock maximum period of 8nS, meaning the bus frequency needs to be 125MHz.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Can someone please confirm that these figures are correct and if so, what effect does it have on the memory if it is slightly underclocked ?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;If underclocking the memory is a problem, does anyone have any ideas whether slightly overclocking the coldfire to 250MHz to get the correct bus clock is a bad idea ?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thank you in advance,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Paul H&lt;/SPAN&gt;&lt;BR /&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 15 Jul 2008 18:38:26 GMT</pubDate>
    <dc:creator>PaulHodgskin</dc:creator>
    <dc:date>2008-07-15T18:38:26Z</dc:date>
    <item>
      <title>Using DDR2 memory with coldfire 54450 processor</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Using-DDR2-memory-with-coldfire-54450-processor/m-p/173003#M6553</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;I would like to use DDR2 memory with the MCF54450 processor which has an in built DDR memory controller.&amp;nbsp; The 5445x datasheet specifies that the 54450 and 51 devices can only run up to a maximum of 240MHz, giving a bus clock maximum of 120MHz.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;DDR2 memory requires a bus clock maximum period of 8nS, meaning the bus frequency needs to be 125MHz.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Can someone please confirm that these figures are correct and if so, what effect does it have on the memory if it is slightly underclocked ?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;If underclocking the memory is a problem, does anyone have any ideas whether slightly overclocking the coldfire to 250MHz to get the correct bus clock is a bad idea ?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thank you in advance,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Paul H&lt;/SPAN&gt;&lt;BR /&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 Jul 2008 18:38:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Using-DDR2-memory-with-coldfire-54450-processor/m-p/173003#M6553</guid>
      <dc:creator>PaulHodgskin</dc:creator>
      <dc:date>2008-07-15T18:38:26Z</dc:date>
    </item>
    <item>
      <title>Re: Using DDR2 memory with coldfire 54450 processor</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Using-DDR2-memory-with-coldfire-54450-processor/m-p/173004#M6554</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hi Paul&lt;/DIV&gt;&lt;DIV&gt;&lt;DIV&gt;Some experts believe 120MHz will not lead to bad functioning ....&lt;/DIV&gt;I´ve heard people using clock of 75MHz (150MHz controller)&amp;nbsp;to clock DDR2 and it is works fine ...&lt;/DIV&gt;&lt;DIV&gt;However I´m a very begining 54451 "observer" :smileyhappy:&lt;/DIV&gt;&lt;DIV&gt;Ricardo Raupp&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 02 Aug 2008 06:16:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Using-DDR2-memory-with-coldfire-54450-processor/m-p/173004#M6554</guid>
      <dc:creator>Ricardo_RauppV</dc:creator>
      <dc:date>2008-08-02T06:16:06Z</dc:date>
    </item>
  </channel>
</rss>