<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: problem with general purpose timer in ColdFire/68K Microcontrollers and Processors</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/problem-with-general-purpose-timer/m-p/129105#M652</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;Thanks for the aid but already to be used PIT. The problem is that I need to use a GPT and not that I am forming bad.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;DIV&gt;I want to timer each 1mseg to a frequency of 60MHz &lt;SPAN&gt;&lt;FONT color="#000000"&gt;M52233demo&lt;/FONT&gt;&lt;/SPAN&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&lt;/SPAN&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&lt;FONT color="#000000"&gt;Thanks&lt;/FONT&gt;&lt;/SPAN&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 02 Apr 2007 17:17:28 GMT</pubDate>
    <dc:creator>VeronicaFNX</dc:creator>
    <dc:date>2007-04-02T17:17:28Z</dc:date>
    <item>
      <title>problem with general purpose timer</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/problem-with-general-purpose-timer/m-p/129103#M650</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hello, I have a problem with the GPT (general Purpose to timer).&lt;/DIV&gt;&lt;DIV&gt;I want to put&amp;nbsp;a timer each 1 mseg and I do this,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;void GPTimers_inicializa(void)&lt;BR /&gt;{&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;MCF_GPT_GPTIOS = 0x01;&amp;nbsp;&amp;nbsp;&amp;nbsp;//Habilita los 4 GPT como output compare&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;MCF_GPT_GPTSCR1 = MCF_GPT_GPTSCR1_GPTEN;&amp;nbsp;//habilita cualquier&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;MCF_GPT_GPTIE = MCF_GPT_GPTIE_CI(0x01);&amp;nbsp;&amp;nbsp;//habilita la interrupcion del GPT0&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;MCF_GPT_GPTSCR2 =MCF_GPT_GPTSCR2_PR(0x00);&amp;nbsp;//Prescaler, 30MHz&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;MCF_GPT_GPTFLG1 = 0x00;&amp;nbsp;//limpia los chanel flags&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;MCF_GPT_GPTFLG2 = 0x00;&amp;nbsp;//limpiar flags&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;MCF_GPT_GPTC0 = MCF_GPT_GPTC0_CCNT(0x7530);&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;MCF_GPT_GPTC1 = 0;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;MCF_GPT_GPTC2 = 0;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;MCF_GPT_GPTC3 = 0;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;MCF_INTC0_ICR44 = MCF_INTC_ICR_IL(0x7) | MCF_INTC_ICR_IP(0x7);&amp;nbsp;//GPT0&lt;BR /&gt;&amp;nbsp;&amp;nbsp;MCF_INTC0_IMRH &amp;amp;= ~MCF_INTC_IMRH_MASK44;&lt;BR /&gt;}&lt;/DIV&gt;&lt;DIV&gt;&lt;BR /&gt;int main()&lt;BR /&gt;{&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&amp;nbsp;Leds_Init();&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;GPTimers_inicializa();&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;while(1);&amp;nbsp;// Idle&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;return 0;&lt;BR /&gt;}&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;and also initialize the interrupt vectors. That I am making bad? or, that I need to do? Thanks&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Apr 2007 15:07:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/problem-with-general-purpose-timer/m-p/129103#M650</guid>
      <dc:creator>VeronicaFNX</dc:creator>
      <dc:date>2007-04-02T15:07:10Z</dc:date>
    </item>
    <item>
      <title>Re: problem with general purpose timer</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/problem-with-general-purpose-timer/m-p/129104#M651</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hi&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I am not sure if the GPT is better for your application than a Programmable Interrupt Timer - it seems like you just want to generate an interrupt every 1ms so&amp;nbsp;a PIT would be easier. Of course, you may be using a part with no PIT.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I haven't used GPT, but I have included below code that will set up PITs and ISRs for them. If you need to use a GPT, then it shouldn't be too difficult to adapt this. My code is for mcf5282, but I know it also works on mcf52235.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;When I looked at you code, I noticed that your set the interrupt level and priority to 7 - this level is non-maskable. Unless your ISR happens to need an NMI, a lower level may be better.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I also noticed that you haven't set a vector for the ISR, is this hardcoded in your vectors? If not, you must set the correct&amp;nbsp;vector. I have included source for a C function that will both set the vector and the interrupt mask. (all code samples belowe are aimed at GCC, but should be portable to CW).&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;First, timer initialisation, adapt this for GPT:&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN class="msg_source_code"&gt;&lt;SPAN class="text_smallest"&gt;Code:&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;PRE&gt;/* FUNCTION: PIT_Timer_Init() * * Initialise and enable a Programmable Interval Timer * * PARAM1: PIT - can be 0, 1, 2 or 3 * * PARAM2: Prescaler value - sets the tick frequency to *     (system clock/2) divided by 2^PCSR * * PARAM3: Modulo counter - sets the mumber of ticks per interrupt * * PARAM4: Interrupt handler * * RETURNS: none */voidPIT_Timer_Init(uint8 timer, uint8 PCSR, uint16 PMR, void (*handler)(void)){ // At 64MHz: // PCSR = 5 gives a tick per uS // PMR = 10000 gives an interrupt every 10ms if (timer &amp;lt; 4) {  uint8 ipl = MCF5282_INTC_ICR_IL(TIMER_NETWORK_LEVEL)     | MCF5282_INTC_ICR_IP(timer);  MCF5282_PIT_PCSR(timer) = 0;  // Set up interrupt handler  mcf5282_interrupt_init(timer + 55, ipl, handler);  // Set modulo count  // (= number of ticks per interrupt)  MCF5282_PIT_PMR(timer) = PMR;  // Tick frequency = (system clock/2) divided by 2^PCSR  MCF5282_PIT_PCSR(timer)  = (uint16)(MCF5282_PIT_PCSR_PRE(PCSR));  // Create and enable 'set and forget' timer  MCF5282_PIT_PCSR(timer) |= MCF5282_PIT_PCSR_OVW         | MCF5282_PIT_PCSR_PIE         | MCF5282_PIT_PCSR_PIF         | MCF5282_PIT_PCSR_RLD         | MCF5282_PIT_PCSR_EN; }}/* FUNCTION: PIT_Timer_Stop() * * Disable timer interrupts for the specified PIT * * PARAM1: PIT - can be 0, 1, 2 or 3 * * RETURNS: none */voidPIT_Timer_Stop(uint8 timer){ if (timer &amp;lt; 4)  MCF5282_PIT_PCSR(timer) &amp;amp;= ~( MCF5282_PIT_PCSR_PIE | MCF5282_PIT_PCSR_EN );}&lt;/PRE&gt;&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;Second, set up the interrupt vector and enable the interrupt in the interrupt controller:&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN class="msg_source_code"&gt;&lt;SPAN class="text_smallest"&gt;Code:&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;PRE&gt;/* FUNCTION: mcf5282_interrupt_init() * * Initialise an interrupt handler for an interrupt source * for INTC0. If the handler is a NULL pointer, then mask * this interrupt. * * PARAM1: Interrupt source (1..62) * * PARAM2: Interrupt level and priority * * PARAM3: Interrupt handler * * RETURNS: none */voidmcf5282_interrupt_init(uint8 source, uint8 ipl, void (*handler)(void)){ // Only for user defined vectors in INTC0 if ((source &amp;gt; 0) &amp;amp;&amp;amp; (source &amp;lt; 63)) {  // Interrupts should be disabled to avoid vector problems  // and to ensure that a spurious interrupt exception can't  // be generated.  uint8 sysint = asm_set_ipl(7);  if (handler)  {   // Set interrupt priority level   MCF5282_INTC0_ICR(source) = (ipl &amp;amp; 0x3F);   // Set vector   mcf5xxx_set_handler(source+64, (ADDRESS)handler);   // Clear mask for this handler   if (source &amp;lt; 32)    MCF5282_INTC0_IMRL &amp;amp;= ~(MCF5282_INTC_IMRL_INT(source)          | MCF5282_INTC_IMRL_MASKALL);   else   {    MCF5282_INTC0_IMRL &amp;amp;= ~(MCF5282_INTC_IMRL_MASKALL);    MCF5282_INTC0_IMRH &amp;amp;= ~(MCF5282_INTC_IMRH_INT(source));   }  }  else  {   // Set vector   mcf5xxx_set_handler(source+64, (ADDRESS)handler);   // Set mask for this handler   if (source &amp;lt; 32)   {    MCF5282_INTC0_IMRL |= MCF5282_INTC_IMRL_INT(source);   }   else   {    MCF5282_INTC0_IMRH |= MCF5282_INTC_IMRH_INT(source);   }  }  // As you were...  asm_set_ipl(sysint); }}/********************************************************************/&lt;/PRE&gt;&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;In case you need it, this is the assembler for the function that masks interrupts in the SR, used while the interrupt vectors and masks are being modified:&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN class="msg_source_code"&gt;&lt;SPAN class="text_smallest"&gt;Code:&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;PRE&gt;/********************************************************************//* * This routines changes the IPL to the value passed into the routine. * It also returns the old IPL value back. * Calling convention from C: *   old_ipl = asm_set_ipl(new_ipl); * For the Diab Data C compiler, it passes return value thru D0. * Note that only the least significant three bits of the passed * value are used. */asm_set_ipl:_asm_set_ipl:    link    A6,#-8    movem.l D6-D7,(SP)    move.w  SR,D7       /* current sr    */    move.l  D7,D0       /* prepare return value  */    andi.l  #0x0700,D0  /* mask out IPL  */    lsr.l   #8,D0       /* IPL   */    move.l  8(A6),D6    /* get argument  */    andi.l  #0x07,D6        /* least significant three bits  */    lsl.l   #8,D6       /* move over to make mask    */    andi.l  #0x0000F8FF,D7  /* zero out current IPL  */    or.l    D6,D7           /* place new IPL in sr   */    move.w  D7,SR    movem.l (SP),D6-D7    lea     8(SP),SP    unlk    A6    rts&lt;/PRE&gt;&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;And the interrupt handler (note that __attribute__((interrupt_handler)) is GCC specific, you need to change for CW):&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;SPAN class="msg_source_code"&gt;&lt;SPAN class="text_smallest"&gt;Code:&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;PRE&gt;/******************************************************************** * FUNCTION: hz_timer_isr() * * PIT2 interrupt handler, set to be called at 1 second intervals * * PARAMS: none * * RETURNS: none * * Used for updating rate counters for bit rates, etc. */__attribute__((interrupt_handler))voidhz_timer_isr(void){ // Do something...  // Clear interrupt at CSR MCF5282_PIT_PCSR(HZ_TIMER) |= MCF5282_PIT_PCSR_PIF;}&lt;/PRE&gt;&lt;DIV&gt;&lt;BR /&gt;&amp;nbsp;And finally, put this call somewhere to set up a timer (this is to create a timer that is called at 1 second intervals on a mcf5282 running at 64MHz, change the values to get a 1ms timer):&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;SPAN class="msg_source_code"&gt;&lt;SPAN class="text_smallest"&gt;Code:&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;PRE&gt; // We are assuming that sys_clk is 64MHz // so PCSR = 11 gives 15625 ticks per second. PIT_Timer_Init(HZ_TIMER, 11, 15625, hz_timer_isr);&lt;/PRE&gt;&lt;DIV&gt;&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Cheers,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Paul.&lt;BR /&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Apr 2007 16:58:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/problem-with-general-purpose-timer/m-p/129104#M651</guid>
      <dc:creator>mccPaul</dc:creator>
      <dc:date>2007-04-02T16:58:37Z</dc:date>
    </item>
    <item>
      <title>Re: problem with general purpose timer</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/problem-with-general-purpose-timer/m-p/129105#M652</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;Thanks for the aid but already to be used PIT. The problem is that I need to use a GPT and not that I am forming bad.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;DIV&gt;I want to timer each 1mseg to a frequency of 60MHz &lt;SPAN&gt;&lt;FONT color="#000000"&gt;M52233demo&lt;/FONT&gt;&lt;/SPAN&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&lt;/SPAN&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&lt;FONT color="#000000"&gt;Thanks&lt;/FONT&gt;&lt;/SPAN&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Apr 2007 17:17:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/problem-with-general-purpose-timer/m-p/129105#M652</guid>
      <dc:creator>VeronicaFNX</dc:creator>
      <dc:date>2007-04-02T17:17:28Z</dc:date>
    </item>
    <item>
      <title>Re: problem with general purpose timer</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/problem-with-general-purpose-timer/m-p/129106#M653</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hi&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;OK, so I have modified the code above to use GPT0 as it it was a PIT, see below. You will have you chaneg the references from MCF5282_GPTA to the equivalent MCF_GPT #defines because I have written this for the 5282 which has 2 GPTs (GPTA and GPTB) so the registers are slightly different.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I have just tested this and it works on my 5282. I noticed one error in your code - when you want to clear the flags, you must write a 1, not a 0. These lines are wrong:&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;MCF_GPT_GPTFLG1 = 0x00;&amp;nbsp;//limpia los chanel flags&lt;BR /&gt;&amp;nbsp;MCF_GPT_GPTFLG2 = 0x00;&amp;nbsp;//limpiar flags&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;See section 23.6.12 in the reference guide. I also noticed a problem in the refernce guide with the pre-scaler. In table 23-14 it shows divisors from 1 to 64, in section 23.7.1 it says you can use 1 or 16. I don't know which is correct for 5223x. For 5282 all divisors are shown in both places in the refernce guide.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Maybe you will have to use prescaler divisor of 16 with count of 0x753 to get 1ms at 60MHz CPU clock.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Configure GPT:&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN class="msg_source_code"&gt;&lt;SPAN class="text_smallest"&gt;Code:&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;PRE&gt;/* FUNCTION: GPTA_Timer_Init() * * Initialise and enable General Purpose Timer A0 to work like * a PIT. * * PARAM2: Prescaler value - sets the tick frequency to *     (system clock/2) divided by 2^PCSR * * PARAM3: Modulo counter - sets the mumber of ticks per interrupt * * PARAM4: Interrupt handler * * RETURNS: none */voidGPTA_Timer_Init(uint8 PCSR, uint16 PMR, void (*handler)(void)){ // At 64MHz: // PCSR = 5 gives a tick per uS // PMR = 1000 gives an interrupt every 1ms uint8 ipl = MCF5282_INTC_ICR_IL(2)    | MCF5282_INTC_ICR_IP(0); // Disable timer A MCF5282_GPTA_GPTSCR1 = 0; // Set up interrupt handler mcf5282_interrupt_init(44, ipl, handler); // Set modulo count // (= number of ticks per interrupt) MCF5282_GPTA_GPTC0 = PMR; // Tick frequency = (system clock/2) divided by 2^PCSR MCF5282_GPTA_GPTSCR2  = (uint16)(MCF5282_GPT_GPTSCR2_PR(PCSR)); MCF5282_GPTA_GPTIOS = MCF5282_GPT_GPTIOS_IOS0; MCF5282_GPTA_GPTIE = MCF5282_GPT_GPTIE_C0I; MCF5282_GPTA_GPTFLG1 = MCF5282_GPT_GPTFLG1_C0F; MCF5282_GPTA_GPTFLG2 = MCF5282_GPT_GPTFLG2_TOF | MCF5282_GPT_GPTFLG2_C0F; // Enable timer A MCF5282_GPTA_GPTSCR1 = MCF5282_GPT_GPTSCR1_GPTEN;}&lt;/PRE&gt;&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;ISR:&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN class="msg_source_code"&gt;&lt;SPAN class="text_smallest"&gt;Code:&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;PRE&gt;/******************************************************************** * FUNCTION: gpt_timer_isr() * * GPTA0 interrupt handler, set to be called at 1ms intervals * * PARAMS: none * * RETURNS: none */__attribute__((interrupt_handler))voidgpt_timer_isr(void){ // Clear interrupt MCF5282_GPTA_GPTFLG1 = MCF5282_GPT_GPTFLG1_C0F;}&lt;/PRE&gt;&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;Configure it like this:&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN class="msg_source_code"&gt;&lt;SPAN class="text_smallest"&gt;Code:&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;PRE&gt;GPTA_Timer_Init(5, 10000, gpt_timer_isr);&lt;/PRE&gt;&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;Cheers,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Paul.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Apr 2007 18:38:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/problem-with-general-purpose-timer/m-p/129106#M653</guid>
      <dc:creator>mccPaul</dc:creator>
      <dc:date>2007-04-02T18:38:10Z</dc:date>
    </item>
  </channel>
</rss>