<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Connecting LCD to M5213 in ColdFire/68K Microcontrollers and Processors</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Connecting-LCD-to-M5213/m-p/128970#M637</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi,&lt;BR /&gt;&lt;BR /&gt;You could use a level translator such as the ST2378E from STM wich is bidirectional and 15KV ESD protected.&lt;BR /&gt;&lt;BR /&gt;Emmanuel&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 08 Sep 2006 13:17:38 GMT</pubDate>
    <dc:creator>Nouchi</dc:creator>
    <dc:date>2006-09-08T13:17:38Z</dc:date>
    <item>
      <title>Connecting LCD to M5213</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Connecting-LCD-to-M5213/m-p/128967#M634</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hi,&lt;/DIV&gt;&lt;DIV&gt;I am new to Coldfire and now having project to connect M5213 to LCD display (44780 compatible).&amp;nbsp; Is there any sample/application note I can look at?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Thanks.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;M. Ludwig&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 02 Sep 2006 02:44:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Connecting-LCD-to-M5213/m-p/128967#M634</guid>
      <dc:creator>MLudwig</dc:creator>
      <dc:date>2006-09-02T02:44:39Z</dc:date>
    </item>
    <item>
      <title>Re: Connecting LCD to M5213</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Connecting-LCD-to-M5213/m-p/128968#M635</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;I have the same problem. I´m using a M5213EVB board and want to connect a HD44780 compatible LCD. It would be nice if Freescale (or someone else) could provide an application note for the Coldfire, like the AN2940 for the HC08 processor.&amp;nbsp;I´m primarly writing in C and using CodeWarrior.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Thanx.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;/Dan&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 Sep 2006 18:01:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Connecting-LCD-to-M5213/m-p/128968#M635</guid>
      <dc:creator>Lotus</dc:creator>
      <dc:date>2006-09-04T18:01:47Z</dc:date>
    </item>
    <item>
      <title>Re: Connecting LCD to M5213</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Connecting-LCD-to-M5213/m-p/128969#M636</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;OK, I've some info about how to do this. We can actually use shift register to convert serial bits coming from one of the GPIO to 8-bit data used for data, another pin to control the EN input, and one to control R/W*.&lt;BR /&gt;But I still doubt if connecting this 5V TTL register (and the LCD controller) to 3V level inputs on M5213 will work.&lt;BR /&gt;&lt;BR /&gt;Any thought?&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 08 Sep 2006 12:31:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Connecting-LCD-to-M5213/m-p/128969#M636</guid>
      <dc:creator>MLudwig</dc:creator>
      <dc:date>2006-09-08T12:31:26Z</dc:date>
    </item>
    <item>
      <title>Re: Connecting LCD to M5213</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Connecting-LCD-to-M5213/m-p/128970#M637</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi,&lt;BR /&gt;&lt;BR /&gt;You could use a level translator such as the ST2378E from STM wich is bidirectional and 15KV ESD protected.&lt;BR /&gt;&lt;BR /&gt;Emmanuel&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 08 Sep 2006 13:17:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Connecting-LCD-to-M5213/m-p/128970#M637</guid>
      <dc:creator>Nouchi</dc:creator>
      <dc:date>2006-09-08T13:17:38Z</dc:date>
    </item>
  </channel>
</rss>