<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: uClinux and dBug in ColdFire/68K Microcontrollers and Processors</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/uClinux-and-dBug/m-p/168875#M6076</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;i have a same problem, you can tell me if you are fix this problem, if yes how?&lt;/P&gt;&lt;P&gt;thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 20 Feb 2012 23:12:35 GMT</pubDate>
    <dc:creator>slime_samir</dc:creator>
    <dc:date>2012-02-20T23:12:35Z</dc:date>
    <item>
      <title>uClinux and dBug</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/uClinux-and-dBug/m-p/168873#M6074</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;&amp;nbsp;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm following the AN3408 in order to install a uClinux on the MCF5329EVB.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have built the uClinux kernel and I have to download it to the target board with dBug.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The problem is that I can't set an IP address with dBug. I execute the command "set" to set the IP addresses and it looks like it works (when I execute "show" I can see the new IP values displayed). But when I make a ping from my PC (server) to the target board IP address, it doesn't work. Neither the command "dn" to download the kernel. It looks like I can't configure the IP addresses with dBug with the command set.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I've followed the AN3408 steps. All the settings show me right. But then it doesn't work.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;My dBug version is v4b.1a.1d.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Can you help me please? Any idea?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Best regards&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks&lt;/SPAN&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 30 Nov 2007 20:38:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/uClinux-and-dBug/m-p/168873#M6074</guid>
      <dc:creator>jesortsan</dc:creator>
      <dc:date>2007-11-30T20:38:41Z</dc:date>
    </item>
    <item>
      <title>Re: uClinux and dBug</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/uClinux-and-dBug/m-p/168874#M6075</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi&lt;BR /&gt;&lt;BR /&gt;The dBUG monitor doesn't respond to 'ping'. It's not multi-threaded, so it's just sitting there at the command prompt and can't handle any ping packets which turn up.&lt;BR /&gt;&lt;BR /&gt;Downloading via TFTP should work OK, however. Here are some ideas to check:&lt;BR /&gt;&lt;BR /&gt;(1) Is there a TFTP server running on your server? If you're using something like a Linux box, TFTP is usually disabled by default because it's a security hole.&lt;BR /&gt;&lt;BR /&gt;(2) The TFTP server is very restrictive in where it looks for the file to download. You need to make sure that it's in a place where the TFTP server can see it.&lt;BR /&gt;&lt;BR /&gt;(3) You could be getting hosed by a Firewall blocking attempts at TFTP connection to the server.&lt;BR /&gt;&lt;BR /&gt;Stick with it, because it does work OK when you get it configured correctly.&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;Hope this helps, and good luck&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;Simon&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 30 Nov 2007 22:07:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/uClinux-and-dBug/m-p/168874#M6075</guid>
      <dc:creator>SimonMarsden_de</dc:creator>
      <dc:date>2007-11-30T22:07:37Z</dc:date>
    </item>
    <item>
      <title>Re: uClinux and dBug</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/uClinux-and-dBug/m-p/168875#M6076</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;i have a same problem, you can tell me if you are fix this problem, if yes how?&lt;/P&gt;&lt;P&gt;thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 20 Feb 2012 23:12:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/uClinux-and-dBug/m-p/168875#M6076</guid>
      <dc:creator>slime_samir</dc:creator>
      <dc:date>2012-02-20T23:12:35Z</dc:date>
    </item>
  </channel>
</rss>